Press Releases
RS Components introduces high-reliability DC/DC converters targeting medical applications
Series of 2W and 3.5W DC/DC converters offer excellent value and are approved for use in medical equipment
UK, 21 June 2018:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), a global multi-channel distributor, has announced availability of a new range of DC/DC converters that target use in medical applications. Offering high reliability and excellent value, the TIM 2 and TIM 3.5 series are manufactured by Traco Power and feature 2W and 3.5W DC/DC converters, respectively.
Importantly for medical applications, the converters provide reinforced isolation of up to 5000V AC (RMS). Also, offering a low leakage current of less than 2μA, the converters are suited to use in insulating electrical equipment within the BF classification for patient applied parts.
The converters are approved to IEC/EN/ES60601-1 3rd edition for 250V AC 2xMOPP up to an altitude of 5000m, and an ISO14971 risk management file is available. Further approvals include compliance with the latest EMC requirements IEC 60601-1-2 4th edition for medical equipment.
Available in compact DIP-16 or SMD-16 packages, a wide range of series models are available with output voltages of 3.3, 5.0, 9.0, 12, 15, 24, ±12 and ±15V DC. Devices in the series offer input voltage ranges of 4.5-12V, 9.0-18V, 18-36V and 36-75V DC.
Delivering high efficiencies, the converters also offer operation at environmental temperatures from –40 up to 95°C and up to 90°C for the TIM 3.5 series. Both series provide shock, vibration and thermal shock resistance, according to MIL-STD-810F.
The Traco Power TIM 2 and TIM 3.5 series of DC/DC converters are supplied with a 5-year product warranty and are shipping now in the EMEA and Asia Pacific regions.
-Ends-
About RS Components
RS Components and Allied Electronics & Automation are the trading brands of Electrocomponents plc, a global multi-channel distributor. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2018 had revenues of £1.71bn.
For more information, please visit the website at www.rs-online.com.
Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com
+44 (0) 7795 400 651
PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000
Further information is available via these links:
Twitter:
@RSComponents
@alliedelec
@designsparkRS
RS Components on Linkedin:
http://www.linkedin.com/company/rs-components
Other Relevant Links:
Electrocomponents plc:
www.electrocomponents.com
RS Components:
www.rs-online.com
DesignSpark:
www.designspark.com