Getting Started
One of the most common method of using a rocker switch is on a light switch, but they are in quite a few other devices and applications as well including surge protectors and appliances. It is possible to change existing switches and turn them into rocker switchers.
These sorts of switches are advantageous to many types of applications because they have a relatively small profile and they require actual manual manipulation in order to activate. Because of the nature of the rocker switch, they work well with appliances, tools, lights, and more. Large rocker switches that are easy to manipulate are helpful for those who do not have fine motor control, as they would have to do if the device had a toggle switch instead.
The rocker switch received its name because of the way in which it works. The user will rock the switch in one direction or the other, which will open or close the circuit. These sorts of switches will generally have an up and down motion, but a side-to-side motion is possible as well, depending on the device and the location of the switch. In the case of a surge protector, they have a back and forth motion since they are on the floor, but the general conceit is the same. They simply rock back and forth.
What Differentiates a Rocker Switch from Another Switch?
Rocker switches have an on and an off position, and they break the electrical circuit to interrupt the current just as other switches do. The rocker switches are very simple though, when compared with other types of switches. The thing that makes the switches unique those is the rocker property of the actuator. You do not have to turn a knob, and it is even simpler to operate even than a toggle switch, which is very similar. Simply rocking the switch back and forth will open or close the circuit.
- Solidworks is one of the most popular parametric-based modelling tools on the market. Solidworks is developed by Dassault Systèmes.
- Top Solid is a fully integrated CAD/CAM software that enables users to design and manufacture their parts using a common software platform.
- Pro/Engineer from PTC was one of the first CAD systems to offer parametric, feature-based, associative solid modelling.
- Solid Edge is a software tool that offers full parametric based modelling, along with links to PLM (Product Lifecycle Management) software.
- SketchUp is the leading free-to-market 3D modelling tool. Previously developed by Google, the tool is now published by Trimble.
- Parasolid is a geometric modelling kernel owned by Siemens PLM Software. It provides the core functionality for many of the parametric-based modelling tools on the market today.
- CATIA is a multi-platform CAD/CAM software suite from Dassault Systèmes. A high-end professional tool, CATIA is the cornerstone of the Dassault Systemes product lifecycle management software suite.
- TurboCAD was originally developed as a low cost alternative to AutoCAD in the 2D drafting market. Now in the 19th version, it continues to offer low cost access to 3D modelling.
- DesignSpark Mechanical is our very own FREE 3D software. Using direct modelling techniques it is not only easy to learn but also easy to use saving you thousands and pounds and valuable design time.
- SpaceClaim is the leading direct-modelling tool on the market, offering very intuitive modelling combined with powerful professional features, making it a real alternative to more traditional parametric-based tools.
Product spotlights
Motion Sensor
An electronic device capable of converting the movements it senses into electrical signals.
Rocker Switch
One of the most common method of using a rocker switch is on a light switch, but they are in quite a few other devices and applications as well including surge protectors and appliances.
Strain Gauge
Stretching a strip of conductive metal will not only make it longer and thinner, it will result in an increase in electrical resistance from one end of the strip to another.
Screw Extractors
Screws have significant advantages over nails in certain applications.