A Complete Guide to MOSFET Transistors

Learn everything you need to know about MOSFETs in our complete guide and discover leading brands and products.

Primary Types of Transistor

There are two primary types of transistors. The first is the Bipolar Junction Transistor (BJT) and the second is the Field Effect Transistor (FET). MOSFETs are a type of FET. BJTs are usually used for electrical currents of under one amp, while MOSFETs are typically used for higher-current applications.

Users can choose between MOSFETs featuring depletion or enhancement modes. The depletion mode operates in a similar way to the closed switch, with current flowing when the on voltage is applied. If a negative voltage is applied, then the current will stop. On the flip side, enhancement mode MOSFETs are the most commonly used type for modern-day applications.

What is a MOSFET Transistor?

The Metal Oxide Semiconductor Field Effect Transistor (MOSFET) is a commonly used semiconductor in digital and analogue circuits and is also a useful power device. As the original compact transistor, it is suitable for a wide variety of electrical applications.

It has been argued that many of the 21st century’s technological developments wouldn’t have been possible without the MOSFET. It is more widely used than the BJT as it requires minimal current for load-current control. The level of conductivity can be increased from the ‘normally off’ state when the MOSFET is set to enhancement mode. Voltage transmitted via the gate can minimise conductivity from the ‘normally on’ state. The process of miniaturising MOSFETs is relatively simple and they can be effectively scaled down for compact applications.

Additional advantages of the MOSFET include rapid switching (particularly in relation to digital signals), minimal power consumption, and high-density capacity which makes them ideally suited to large-scale integration.

The MOSFET is a core component of the integrated circuit and it can be designed and fabricated in a single chip due to its compact size. It features four terminals, these being the Source (S), Gate (G), Drain (D), and Body (B). The body is typically connected to the source terminal so that the MOSFET functions as a field-effect transistor.

How Do MOSFETs Work and What Do They Do?

MOSFET

MOSFETs feature three pins - Source, Gate and Drain. They effectively control the electrical current flowing between the Source and Drain contacts, with voltage being applied via the Gate. You can prompt the appearance or disappearance of an electrical channel by altering the electrical voltage. This enables the electrical device to be switched on or off. The use of a semiconductor allows for the separation of different impurity varieties. This means that charges of different signs can be effectively isolated, and barriers can be created, preventing the flow of charge from one region to the next.

The transfer of current from the Gate to the Source terminals will result in current flowing from the Drain to the Source pins. The Drain-source resistance will ideally be very high when there is no current flowing and low when the current is transmitted. However, you should be aware that MOSFETs complete with microcontrollers may require 10-15 Gate Source potential difference for the lowest level of Drain source resistance with the microcontroller operating on 5v or 3.3v.

The MOSFET Gate source pins have a capacitance that prevents rapid switching between states. High current will be necessary for a rapid change between voltage on internal capacitance. It must prompt an automatic switch between the change (source) and discharge (sink). A change in voltage applied to the Gate will result in a simultaneous switch in resistance from the Drain to the Source. The levels of voltage will correspond directly with the levels of resistance. Power MOSFETs are purpose-made for applications involving the generation of high power levels.

Shop MOSFET Transistors

Browse Our Quality Range of MOSFET Transistors:

Each
£1.16
Each (In a Pack of 2)
£4.57
Each (On a Reel of 3000)
£0.213
Each (In a Pack of 10)
£0.617
Each
£2.21

Different Types of MOSFET Transistors

PMOS Logic

As previously mentioned, the integration of a MOSFET allows for high levels of circuit efficiency when compared with BJTs. P-channel MOSFETs can be used with PMOS logic to implement digital circuitry and logic gates.

NMOS Logic

NMOS logic is similar to PMOS logic with the exception that N-channel MOSFETs are applied to logic gates and related digital circuitry. As a general rule, N-channel MOSFETs can be smaller than P-channel MOSFETs which makes them more attractive in certain situations. However, NMOS logic constantly consumes power whereas PMOS logic does not.

CMOS Logic

Complementary metal-oxide-semiconductor (CMOS) logic is a technology used to produce integrated circuits. Such circuits are featured across a range of electrical components and are known to generate electrical power. Both P and N-channel MOSFETs are used in conjunction with connected gates and drains in order to reduce power consumption and excess heat generation.

Depletion Mode MOSFET Devices

Depletion mode MOSFET devices are among the less common types of MOSFETs. They have a low channel resistance, with the channel being considered as ‘ON’. When set to the no-power state these switches will conduct in accordance with their design. The channel resistance will be linear, with low distortion across the signal amplitude range.

MISFETs

All MOSFETs are MISFETs (Metal Insulator Semiconductor Field Effect Transistors) but not all MISFETs are MOSFETs. The gate dialectic insulator featured in this type of component is silicon dioxide in a MOSFET, however, alternative materials can be used. The gate dialectic is positioned underneath the gate electrode and above the MISFET channel.

Floating-Gate MOSFETs (FGMOS)

The floating-gate MOSFET features an electronically isolated gate. This has the effect of generating a floating node in DC together with a range of secondary gate inputs situated above the floating gate. Among various other uses, the FGMOS is typically used as a floating-gate memory cell.

Power MOSFETs

The structure of the power MOSFET is vertical, rather than planar. This allows the transistor to maintain high blocking voltage and high current simultaneously. The transistor voltage rating corresponds directly to the doping and thickness of the N-epitaxial layer, with the current rating being a result of the channel width. There is also a direct link between the component area and level of current that can be sustained by this type of device. The power MOSFET allows for low gate drive functionality, rapid switching speed, and advanced paralleling capabilities.

DMOS

These double-diffused metal oxide semiconductors come in lateral and vertical varieties. The majority of power MOSFETs are constructed using this kind of technology.

MOS Capacitors

This type of capacitator has the MOSFET structure, with the MOS capacitator being flanked by dual P-N junctions. It is typically used as a memory chip storage capacitator and support for the charge-coupled device (CCD) in image sensor technology.

TFT

The thin-film transistor (TFT) is a unique type of MOSFET. Creating this variety involves the deposition of thin semiconductor films, combined with a dialectic layer and metallic contacts over a supporting substrate. A range of semiconductor materials may be used, with silicone being a common variety. They can be made to be completely transparent and are used in the manufacture of video display panels.

Bipolar-MOS Transistors

The BiCMOS is an integrated circuit featuring BJT and CMOS transistors on a single chip. The insulated-gate bipolar transistor (IGBT) has similar functionality to the MOSFET and bipolar junction transistor (BJT).

MOS Sensors

A range of MOS sensors has been developed to accurately measure physical, chemical, biological, and environmental variables. Examples include the open-gate FET (OGFET), ion-sensitive field-effect transistor (ISFET), gas sensor FET, charge flow transistor (CFT), and enzyme-modified FET. Commonly used sensors used for digital imaging include the couple-charged device (CCD) and active-pixel sensor (CMOS sensor).

Multi-Gate Field Effect Transistors

The dual-gate MOSFET has a tetrode configuration, with the level of current being controlled by the two gates. It is typically used for small-signal devices in radio frequency applications that call for the reduction of gain loss associated with the Miller effect. This effect occurs when separate transistors are replaced in a cascode configuration.

RHBD

It is quite common for the enclosed-layout transistor (ELT) to be used to create a radiation hardened by design (RHBD) device. The gate of the MOSFET typically surrounds the drain, which is situated close to the centre of the ELT. The source of the MOSFET surrounds the gate in this instance. The H-gate is another type of MOSFET which ensures minimal radiation leakage.

MOSFET Applications and Uses

MOSFET

As previously mentioned, the MOSFET is a device used to switch or amplify electrical signals. This is achieved through alteration of the conductivity in relation to the level of the applied voltage.

The MOSFET is the most common transistor in digital circuits, with the potential for millions being integrated into a memory chip or microprocessor. MOSFET transistors are also commonly included as voltage-controlled circuit switches. It is thought that the development of technologies such as the pocket calculator and digital wristwatch wouldn’t have been possible without the MOSFET.

MOS Integrated Circuits

The MOSFET is the most popular type of transistor and is essential for the electrical operation of integrated circuit (IC) chips. They do not require the same series of steps as bipolar transistors for P-N junction isolation on a chip. However, they do allow for relatively easy separation.

CMOS Circuits

A complementary metal-oxide-semiconductor is a form of technology used to develop integrated circuits. Such technology is used in the manufacture of integrated circuit (IC) chips such as microprocessors, microcontrollers, memory chips and other digital logic circuits. It is also a primary component in the development of analogue circuits including image sensors, data converters, RF circuits, and integrated transmitters for digital communication.

The key characteristics of CMOS devices include high noise immunity and minimal static power consumption. Such devices produce minimal excess heat when compared with alternative forms of logic such as the NMOS logic or transistor-transistor logic. Such characteristics allow for the integration of high-density chip logic functions.

Analogue Switches

The benefits of MOSFETs for digital circuit integration far outweigh those for analogue integration. The transistor behaviour is different in each instance. Digital circuits can be switched fully on or off for the majority of the time. The level of speed and charge are the two primary factors which have a bearing on the switching process. Functionality must be ensured in the transition region of the analogue circuit in the event that minor V changes can alter the output (drain) current.

MOSFETs are still integrated across a variety of analogue circuits because of the associated advantages. Such advantages include reliability, zero gate current, and high and adjustable output impedance. There is also the potential for changing the characteristics and performance of analogue circuits through adjustments to the MOSFET size. MOSFETs are also a preferred option for switches due to the gate current (zero) and drain-source offset voltage (zero).

Power Electronics

MOSFETs are used across a broad range of power electronics. They are integrated for reverse battery protection, switching power between alternate sources, and the powering down of unrequired loads. The key features of compact MOSFETs include the small footprint, high current, and integrated ESD protection. The development of MOS technology is also widely regarded as one of the main contributing factors to the integration of network bandwidth in telecommunication networks.

MOS Memory

The development of the MOSFET allowed for the convenient use of MOS transistors for memory cell storage. MOS technology is one of the key components of DRAM (dynamic-access random memory). It offers higher levels of performance, consumes minimal power, and is relatively affordable when compared with magnetic core memory.

MOSFET Sensors

MOSFET sensors, otherwise referred to as MOS sensors, are commonly used in the measurement of physical, chemical, biological, and environmental parameters. They are also integrated within microelectromechanical systems, primarily because they allow for interaction and the processing of elements such as chemicals, light, and movement. MOS technology also has image sensing applications, being suitable for integration in charge-coupled devices and active-pixel sensors.

Quantum Physics

The quantum field-effect transistor (QFET) and quantum-well field effect transistor (QWFET) are both types of MOSFET which make use of quantum tunnelling to increase the speed of transistor operation. This is achieved by eliminating the area of electron conduction which results in the significant slowing of carriers. The operation of such quantum devices relies on the process of rapid thermal processing (RTP), using extremely fine layers of building materials.

MOSFET by Mount Types

Learn more and explore the different MOSFET mount types below.

Panel Mounted MOSFETs

Panel Mounted MOSFETs

There is a wide variety of MOSFETs that can be mounted onto metal plates or heat sinks with screws. These enhancement MOSFETs allow for fast and reliable switching at high currents.

PCB Mounted MOSFETs

PCB Mounted MOSFETs

The design of the MOSFET with PCB mounting is such that the wrong fuse can’t be fitted. This form of mounting also features a tab, which prevents accidental misuse. Fuse protection is assured, and the circuits are protected against overcurrent conditions. The N-channel MOSFET is one such example, featuring a surface mount and straight lead. This MOSFET is available in tape and reel varieties. It allows for fast switching.

Surface Mounted MOSFETs

Surface Mounted MOSFETs

There is a great selection of MOSFETs complete with surface mounts that allow for quick and convenient PCB assembly. These compact MOSFETs are inexpensive and reliable. The N-channel ON Semiconductor MOSFET is one such example, effectively minimising on-state resistance and ensuring the reliability of switching.

Through Hole Mounted MOSFETs

Through Hole Mounted MOSFETs

MOSFETs with through-hole mounts feature component leads, inserted into holes and securely attached to printed circuit boards (PCBs). They offer relatively strong mechanical bonds when compared to the surface-mounted variety. However, these MOSFETs are preferred for large and heavy components such as semiconductors.

What MOSFET Should I Buy?

It is essential that you select the appropriate N-channel or P-channel MOSFET for your purposes. Each of these MOSFETs functions as an electrical switch. The regular power application features a MOSFET which is connected to the ground, with the lead hooked up to the rail voltage. This is considered to be a low-side switch and requires the fitting of an N-channel MOSFET due to the levels of voltage that must be transmitted in order to switch the device on and off. The P-channel variety should be used when there is a high side switch connected to the bus and load resistor connected to the ground.

The MOSFET voltage must be taken into account. This should exceed both the rail and bus voltage to ensure sufficient protection and prevent MOSFET failure. The current rating should be of the maximum capacity for the load in all instances. Other factors that should be taken into consideration include the technology impact, thermal requirements, and switching performance. The gate parameters must also correspond with the driver circuitry. In short, the appropriate selection will depend on the application of the MOSFET.

FAQs

Popular Brands

microchip mosfet

Microchip

Explore the full range of Microchip MOSFETs, including a selection of products best suited to varying applications.

View Range

fairchild semiconductor mosfet

Fairchild

Fairchild Semiconductor offers a wide range of high-quality MOSFETs. Browse the range and shop online with RS.

View Range

texas instruments mosfet

Texas Instruments

Browse MOSFETs from Texas Instruments and discover the most suitable product for your requirements with RS.

View Range

infineon mosfet

Infineon

RS offers an extensive range of Infineon MOSFETs, giving you the freedom to select the most suitable product.

View Range

Lorna Little

Lorna is an SEO Content Specialist at RS, where she creates search-led content focused on topics including industrial innovation, engineering, maintenance, and procurement. After studying Creative & Professional Writing at Canterbury Christ Church University, she built her career in SEO and content marketing across both agency and in-house environments, helping readers navigate technical subjects through informative, user-focused content. Outside of work, Lorna enjoys reading, travelling, and making memories with her family.

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy