Condition monitoring can keep specialist equipment in operation for longer
According to research by RS and the Institution of Mechanical Engineers, downtime is the biggest challenge facing maintenance engineers. Given that an average of nearly 20 hours per week is spent on unscheduled maintenance, at an average cost of over £100,000, it is also a major challenge for the organisations they work for.
The same report also found that the biggest drivers of unscheduled downtime are ageing assets and mechanical failure, but there are ways to address these issues. Condition monitoring, for instance, uses sensors, oil analysis and the tracking of lubrication levels to detect faults before they become apparent and avoid unscheduled outages. The data generated also improves preventative maintenance so that it is based on the actual performance of components in service.
RS Maintenance Solutions can help take the complexity out of the process of condition monitoring. Here’s an example showing how.
The challenge
Producing some of the world’s finest instant coffee is all about spin – a spinning cone column (SCC) to be precise. It’s at the heart of the process, and each SCC is specifically built for the factory in which it is installed.
The machine is so specialised that, if it is damaged beyond repair, it can take up to 26 weeks to manufacture, deliver and install a replacement. There’s therefore no room for error if you want to keep the coffee flowing.
The SCC uses steam stripping to extract and recover coffee aromas in a natural way, so that they can be used to enhance the instant coffee. The problem is that product can build up in the column, causing it to spin unevenly.
Unbalanced rotation can cause significant damage to the machine. If the cone becomes damaged, it takes several days to remove and, if a replacement is needed, it has to be specially manufactured in Australia.
While the factory waits, production will be cut to a third of normal output. So, when the Maintenance Solutions team from RS advised a leading coffee manufacturer to install condition monitoring equipment on the SCC at its factory, the company took the advice seriously.
The solution
The RS Maintenance Solutions team had already demonstrated that condition monitoring could save downtime and money by assessing vibration in different parts of a plant. Although the team kept a spare SCC on site, they were keen to avoid breakdowns.
Now the system detects any imbalance in the cone’s rotation, so that it can be stopped for cleaning − a relatively quick process which causes only minimum disruption to the factory’s 24-hour production.
The outcome
Regular cleaning, prompted by condition monitoring, allows the plant to run for longer between cleans, increasing overall productivity. It has been so successful in increasing the asset’s performance that the manufacturer has awarded a contract to install similar equipment on all SCCs at their factories worldwide.
As the Technical Lead from RS Maintenance Solutions who oversaw the installation at the company’s factor in Bremen, Germany, explains, “It makes perfect sense: when we see a vibration level, we can automatically trigger a cleaning cycle. Cleaning takes just 45 minutes which means the rest of the plant can keep working. And it’s a lot less disruptive than a 26-week outage.
“The same issues affect this equipment wherever it is installed around the world. We have provided a global solution to what is a global problem. In this case the return on investment was less than one week.”
For more information about RS Maintenance Solutions, click here