• Published 21 Nov 2024
    • Last Modified 21 Nov 2024
  • 5 min

Understanding Electrical Symbols

Learn how to read and understand the different types of component symbols in electric schematics with this guide.

electrical symbols

Electrical circuit diagram symbols may seem cryptic at first, but they are easily understandable, once you know what you’re looking at. With these basic graphic symbols in this guide, you can map out many electric circuit diagrams. Although, there are other advanced symbol categories, too.

Importance of Electrical Symbols

Industry standard electrical component symbols are vital for sharing knowledge about applications of electric and electronic systems:

  • Clarity: Electrical symbols allow electric engineers to clearly show electricians what they want wired, and how.
  • Safety: A circuit diagram with clear electrical symbols can reveal safety hazards to those who know what to look for.
  • Common Language: Electrical symbols transcend written languages, allowing electricians all over the world to understand each other’s work.
  • Troubleshooting: When problems arise in electric circuits, the interconnection wiring diagram is provided for the first thing to look at. With clear, simple to understand electrical schematic symbols, electricians can quickly figure out what they’re looking at and begin diagnosing the problem.
  • Business: By using standard electrical symbols for their industry components, merchants can clearly describe what they sell.

Reading Electrical Symbols

Electrical circuit symbols are simple graphics and follow a common logic, but they can be a lot to take in for the new user. Keep the following tips in mind when reading electrical schematic diagram symbols:

  • Symbols joined with a dot indicate an electric connection between components.
  • Plus and Minus symbols indicate a specific direction of charge (DC only).
  • A backwards, rotated S-symbol (a wave symbol) indicates AC current.
  • An arrow parallel to wire direction indicates current direction.
  • A diagonal arrow superimposed on a symbol indicates adjustability.
  • A single capital letter in a circle indicates an electrical properties measuring instrument.
  • Triangles, as in diode symbols, point in the default current direction.

Electrical Symbols

Electrical circuit symbols represent all the components involved in distributing electrical power. This includes powering motors, lights, heaters, and speakers. Making this happen involves wires, power sources, switches, relays, inductors, and grounding working together, and these all require detailed, accurate circuit diagrams to ensure the system works properly. 

What are the common electrical symbols used in industry? The sections below outline the most basic electrical components symbols.

Wire Symbols

As the connectors transmitting electric energy between all electric devices, wires are the most basic of electronic components. This wire symbol section also includes fuse symbols.

wire symbol

Wire: A straight, featureless line implies a wire connecting one device to another.

connected wire symbol

Connected Wires: The solid junctions represent wire connections.

unconnected wire symbol

Unconnected Wires: One wire jumping over another indicates the wires aren’t connected.

fuse symbol

Fuse: Fuses protect circuits and components from the hazards and damage of overly high currents. The fuse symbol shows the expendable filament between the wiring junctions.

Source Symbols

Source and cell symbols represent any device initiating electric discharge through a circuit, be that through controlled voltage or current.

single cell battery symbol

Single-Cell Battery: A pair of straight lines of different lengths represents one battery cell, which outputs a constant voltage. Positive (+) is the side with the longer line.

multi cell battery symbol

Multi-Cell Battery: Multiple pairs of lines indicate multiple cells.

voltage source symbol

Voltage Source: A constant voltage source other than a battery, with the plus and minus indicating the discharge direction.

controlled voltage source symbol

Controlled Voltage Source: The diamond shape indicates that the voltage can be varied.

ac voltage source symbol

AC Voltage Source: A voltage source using alternating current.

current source symbol

Current Source: A constant current source, with the arrow indicating the current direction.

controlled current source symbol

Controlled Current Source: The diamond shape indicates that the current can be varied.

Ground Symbols

An indispensable part of circuit safety, ground symbols depict a safe current termination.

earth ground symbol

Earth Ground: When the ground point is the literal ground, the three diminishing lines represent the circuit voltage discharging to its zero-potential reference point.

chassis ground symbol

Chassis Ground: This represents the circuit grounded to a nearby metal frame, which should in turn be grounded to earth.

digital and analogue grounds symbol

Digital and Analogue Grounds: Used in electronic circuits, these grounds help keep digital and analogue circuits separate and smooth out noise.

Switch and Relay Symbols

Relay and switch symbols indicate devices that direct current.

spst toggle switch symbol

SPST Toggle Switch: Single pole single throw flows current when closed.

spdt toggle switch symbol

SPDT Toggle Switch: Single pole double throw always flows current to one of two selectable wires.

n.o push button symbol

N.O. Push Button: A normally open button that flows current only when pushed down.

n.c push button symbol

N.C. Push Button: A normally closed button that blocks current only when pushed down.

dip switch symbol

DIP Switch: A dual in-line package of switches.

spst relay symbol

SPST Relay: Single pole single throw flows current only when the electromagnet closes the relay.

spdt relay symbol

SPDT Relay: Single pole single throw always flows current to one of two selectable wires as the electromagnet directs.

Inductor Symbols

Inductors are coils of wire that store electric energy in a magnetic field when current flows through them.

inductor symbol

Inductor: Represents the basic coil of wire for basic inductors.

iron core inductor symbol

Iron Core Inductor: The dual straight lines represent a solid piece of iron the coil wraps around to increase inductance.

variable inductor symbol

Variable Inductor: An inductor with a variable magnetic field.

Electromechanical Symbols

Electric motors and electromechanical devices convert electric energy into mechanical energy or sound, light, or heat energy.

motor symbol

Motor: Converts electric energy to rotational kinetic energy.

Speaker: Makes a speaker oscillate to create soundwaves.

buzzer symbol

Buzzer: Activates an electric buzzer to produce a sound.

bell symbol

Bell: Activates a mechanism for ringing a physical bell.

lamp symbol

Lamp: Represents a lamp or light bulb, which illuminates as it receives current.

heater symbol

Heater: An electric device that gives off heat.

Using Electrical Symbols

With this beginner’s knowledge of electrical symbols, you can create circuit diagrams tailored to your application. Consider using computer-aided design (CAD) software programs with electrical symbols libraries to help quickly place symbols and map out circuits.

Graphic symbols only describe the function of each part, though. These various components interact with each other differently (though in predictable ways) depending on the electrical circuit. Always ensure trained professionals review any drafted schematics before wiring anything.

RS has product lines covering all these categories of electric and electronic parts. Browse them today to plan your circuits.

Related Articles

Related links