Comparing Raspberry Pi vs Arduino - A Guide

Find out all you need to know about development tools Raspberry Pi vs Arduino.

Communication & Wireless Development Tools Banner

If you're working on a new project or designing a new product, development tools are a great way to test out your ideas. Raspberry Pi is a range of single-board computers used for computing and programming projects, while Arduino is an open-source electronics platform based on microcontroller boards and software.

Both are popular development tools, but they offer different capabilities and applications. This guide compares Raspberry Pi vs Arduino, exploring their features, programming languages, advantages and drawbacks to help you choose the most suitable option for your project.

What are Raspberry Pi and Arduino?

Raspberry Pi and Arduino are two of the most commonly used development tools, offering accessible ways to learn programming, test ideas and develop electronic projects. However, they differ in their design, capabilities and intended applications. While Raspberry Pi computers are designed to perform a variety of computing tasks, Arduino boards are commonly used to control electronic components and interact with sensors.

Raspberry Pi

Developed by Raspberry Pi, Raspberry Pi computers are a range of compact, low-cost single-board computers designed to make computing and programming more accessible. Since the launch of the original Raspberry Pi in 2012, several generations and models have been released, offering different processing capabilities, memory configurations and connectivity options.

Raspberry Pi computers are designed to be easily accessible and versatile. Many models can connect to monitors, keyboards and other peripherals, allowing users to perform tasks similar to those of a desktop computer. Their compact design makes them suitable for a range of computing and electronics projects, from developing Internet of Things (IoT) systems to connecting compatible sensors and other electronic components.

Arduino

Arduino combines programmable hardware with software to create an open-source electronics platform designed to help users test and develop electronic systems. Many Arduino boards are based on microcontrollers that can read inputs from sensors and control outputs such as LEDs, motors and alarms.

By reading an input and using programmed instructions to determine an output, Arduino boards can perform a range of automated tasks. For example, an Arduino board can activate an alarm when an object comes close to a sensor or, with additional components, control the movement of a robot.

There are several models of Arduino boards available to suit a range of user requirements, making them an accessible option for anyone starting out in electronics and programming.

What Languages Do Raspberry Pi and Arduino Use?

Raspberry Pi and Arduino support different programming languages and development environments, allowing users to write and run code for a range of electronic projects. The languages available depend on the hardware and software being used.

Raspberry Pi

Raspberry Pi computers typically run a Linux-based operating system, such as Raspberry Pi OS, which was previously known as Raspbian. Raspberry Pi OS is available in different versions, including desktop and Lite editions, depending on whether users require a graphical interface or a command-line environment.

Raspberry Pi supports a variety of programming languages, including Python, C and C++. Python is particularly popular for beginners due to its straightforward syntax and wide range of libraries. Users can also choose from different programming environments and install additional software to suit their project requirements.

Arduino

The Arduino Integrated Development Environment (IDE) is one of the main software tools used to program Arduino boards. Arduino programs, known as sketches, are generally written in C++ using Arduino libraries and functions. These sketches are commonly saved as .ino files before being compiled and uploaded to a compatible board.

The Arduino IDE also supports additional libraries, allowing users to extend the functionality of their projects. Depending on the board, other programming languages and development environments may also be supported.

Single Board Computers as Development Tools

Electronic development boards and kits provide hardware platforms that can be used alongside software to test, prototype and evaluate electronic designs. They allow users to experiment with different functions and develop projects without needing to manufacture a custom printed circuit board during the initial stages of development. These tools can include microcontroller development boards, single-board computers and FPGA development tools, each offering different capabilities depending on the requirements of the project.

Single-board computers contain the main components of a computer on a single circuit board, including a processor, memory and input/output interfaces. They can be connected to peripherals and other electronic components, making them suitable for developing software, testing ideas and evaluating electronic systems.

Depending on the type of development tool, users can experiment with new computing projects, prototype ideas or evaluate existing designs. Some development platforms support open-source software, allowing users to access, modify and redistribute code under the terms of its licence. Others use a combination of open-source and proprietary software or hardware designs.

Single-board computers and microcontroller development boards offer different capabilities, making it important to select the appropriate tool for the requirements of each project.

Raspberry Pi vs Arduino

When comparing Raspberry Pi vs Arduino, there are several key differences to consider, including processing capabilities, power requirements, functionality and cost. While both are popular development tools, each offers different advantages depending on the type of project.

Raspberry Pi Advantages and Drawbacks

One of the main advantages of Raspberry Pi computers is their processing capability. Many models can run multiple applications, making them suitable for projects that require more complex computing functions, network connectivity or data processing. They can also connect to a range of peripherals, including monitors, keyboards and external storage devices.

However, Raspberry Pi computers generally require more power than basic Arduino microcontroller boards. Models running a general-purpose operating system also take time to boot and may be less suitable for tasks requiring precise, predictable response times without additional hardware or software.

Arduino Advantages and Drawbacks

Arduino microcontroller boards are particularly useful for projects involving sensors, electronic components and automated control. Many models have relatively low power requirements and can run programmed tasks without needing a general-purpose operating system. This makes them suitable for embedded applications and projects that require direct interaction with hardware.

However, many Arduino microcontroller boards have less processing power and memory than Raspberry Pi computers. This can limit their suitability for applications involving complex data processing, graphical interfaces or running multiple demanding applications.

Both platforms are available in a range of models and price points, so the most suitable option will depend on the processing requirements, available power supply and intended application.

Comparing the Tools

Raspberry Pi and Arduino offer different features and capabilities depending on the requirements of your project. The table below compares their key characteristics, including processing power, connectivity and typical applications.

Feature
Raspberry Pi computers
Arduino microcontroller boards
Hardware typeSingle-board computer built around a processor-based system-on-chip (SoC)Development board built around a microcontroller
Processing capabilitiesGenerally higher processing power, suitable for running multiple applications and more demanding computing tasksTypically designed for dedicated control tasks, with processing capabilities varying by model
Operating systemTypically runs a Linux-based operating system, such as Raspberry Pi OSMost run programs directly on the microcontroller without a general-purpose operating system
Memory and storageTypically includes RAM and uses microSD or other supported storage for the operating system and filesTypically uses on-chip RAM and non-volatile memory for programs and data
Power requirementsGenerally higher power consumption, with supply requirements varying by model and connected peripheralsOften lower power consumption, with supply requirements varying by board and connected components
ConnectivityModel-dependent USB, Ethernet, Wi-Fi, Bluetooth and GPIO interfacesModel-dependent digital and analogue I/O, serial communication interfaces and wireless connectivity
Real-time controlGeneral-purpose operating systems do not normally guarantee precise response times without additional measuresCan provide predictable timing for suitable control tasks, depending on hardware, software and system requirements
Typical applicationsSoftware development, web servers, IoT gateways and data processingSensor monitoring, robotics, embedded systems and electronic control
CostVaries by model, memory capacity and required accessoriesVaries by board, processing capabilities and additional hardware

Choosing Raspberry Pi and Arduino for Development

Choosing between Raspberry Pi and Arduino depends on the requirements of your project, including processing power, connectivity, power consumption and the type of tasks you want to perform.

If you're looking to develop more complex projects involving data processing, networking or multiple applications, a Raspberry Pi computer may be the better option. Its computing capabilities make it suitable for projects such as web servers, IoT gateways and software development.

Alternatively, Arduino microcontroller boards are well suited to projects involving sensors, electronic components and automated control. They are particularly useful for applications that require dedicated hardware control or relatively low power consumption.

Both platforms offer a range of development options for beginners and experienced users. The most suitable choice will depend on your project's specific requirements and the capabilities of the individual board. Explore our range of microcontroller development tools to find a suitable option for your project.

FAQs

Lorna Little

Lorna is an SEO Content Specialist at RS, where she creates search-led content focused on topics including industrial innovation, engineering, maintenance, and procurement. After studying Creative & Professional Writing at Canterbury Christ Church University, she built her career in SEO and content marketing across both agency and in-house environments, helping readers navigate technical subjects through informative, user-focused content. Outside of work, Lorna enjoys reading, travelling, and making memories with her family.

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy