What is an SDS Drill: Everything You Need to Know

Our guide explains how SDS drills work, what they do, and their most common uses.

Blue and black SDS drills

SDS drills, also known as chisel or hammer drills, are a powerful type of hammer tool best suited to heavy-duty drilling applications. These specialist power tools can be used to drill through materials such as steel, brick, masonry, and concrete, making them handy tools for a range of tasks.

These tools combine the hammer action of a standard hammer drill with the rotary motion of regular drills, making them highly beneficial, effective power tools.

How Do SDS Drills Work?

SDS drills feature a slotted drive system, meaning that the chuck is designed to fit specialist SDS drill bits. These have slots or indentations at the end of their shanks, ensuring a seamless fit into the chuck.

When in operation, the hammer action thrusts the bit forwards. Crucially, the bit’s slots also feature a pair of sprung ball bearings. These bearings are housed in the slots on the bit and act as a sort of safety mechanism, ensuring the bit stays fitted in the chuck. The indentations also help to permit the back and forth hammer action.

The hammer motion is driven by a piston, which fires the bit forward before pulling it back again in a concentrated motion. SDS drills need to have a high level of strength to perform heavy-duty drilling applications, and the smooth action of the ball bearings in the bit help to boost the drill’s strength while also working to reduce friction levels.

How Do You Use an SDS Drill Safely?

A worker using an SDS drill to drill into a concrete wall on a construction site

As is the case when using power tools of any kind, you must ensure that you are fully aware of the relevant safety guidelines before operating the device. It is essential that you ensure both the drill and the bit/s are in good working order – perform a visual inspection before use and if in doubt, do not use the part. You should also make sure to use the correct bit for the task and ensure it is securely fitted into the chuck prior to operation.

Consideration should also be taken with regards to the environment and drilling location, as well as the material you will be drilling. Not only will this help to inform the best type of bit for the task, but it will also determine any additional safety precautions you may need to take.

Lastly, never operate a drill without the correct PPE. Personal protective equipment is essential for keeping you safe while you work, and the importance of this should not be overlooked. The PPE you need when operating a drill includes:

SDS Drill Maintenance Tips

All power tools need semi-regular maintenance to perform optimally and prolong their working life. The following tips should help you keep your tool in good working order:

  • Always follow the manufacturer’s guidelines for usage and maintenance and be sure to familiarise yourself with any warning signs the drill might have
  • Replace any damaged drill bits as soon as possible as using them could end up damaging the drill itself
  • Remove any debris from the end of the bit after use
  • Wipe the end of the bit before fitting into the chuck to ensure a secure hold and to prevent any dirt or dust from causing issues with the mechanism
  • You may find it beneficial to grease the bit shank before fitting into the chuck to help prevent jamming. Take care not to over-grease though, as this could also be problematic

Types of SDS Drills

Multiple different types of SDS drills are available, each with their own advantages and most suitable applications. Although these drills can be categorised in several different ways, one of the simplest is to determine whether the drill is a corded or cordless model.

The two different types are explained below:

A yellow and black cordless SDS drill

Cordless SDS Drills

Cordless drills are often preferred due to the increased mobility and flexibility that they offer. Instead of being tethered by a cable and constrained by the proximity of a plug socket (or the length of an extension lead), you can use a cordless drill virtually anywhere. However, cordless drills run on batteries, which means you need to keep an eye on your battery power and may need to pause work to allow the battery to recharge.

A blue and black corded SDS drill

Corded SDS Drills

On the other hand, corded power tools take their power from mains electricity, avoiding the time taken to recharge batteries. This also means that they need to be connected to an outlet to work, which may be problematic in certain situations. However, the key advantage of using a corded drill is that the majority of corded drills are more powerful than their cordless counterparts. Additionally, they will usually offer greater torque, too.

SDS Drills by Brand

In addition to corded and cordless models, another way to distinguish the different types of SDS drills is by brand. When shopping for a drill, quality and durability should come across all else, and selecting the best model for your requirements is essential.

Browse a selection of leading brands below and click through to shop with RS.

SDS Drill vs Hammer Drill

SDS drills and hammer drills both use a hammering action to drill into hard materials, however, they are designed for different applications.

SDS drills are built for heavy-duty masonry work and use a specialised chuck system that delivers greater impact energy, making them ideal for drilling into concrete, brick, and stone.

Hammer drills, on the other hand, are better suited to lighter drilling tasks and occasional masonry work. They use a standard chuck and are commonly used for general DIY applications involving wood, metal, and softer materials.

SDS Drill
Hammer Drill
Designed for heavy-duty drilling into concrete, brick, stone, and masonryBetter suited to lighter materials and occasional masonry work
Uses an SDS chuck system that allows drill bits to slot securely into placeUses a standard keyed or keyless chuck
Uses a piston-based hammer mechanism for higher impact energyUses a mechanical hammer action created by internal discs or gears
Compatible with SDS Plus or SDS Max drill bitsCompatible with standard straight-shank drill bits
Many models include a hammer-only or rotation-stop mode for chisellingTypically designed for drilling rather than chiselling
Commonly used for construction, renovation, and heavy-duty masonry workCommonly used for DIY, woodworking, metal drilling, and light masonry tasks

SDS Drill Bits

An SDS drill bit

Good quality bits are essential for achieving the best results in drilling applications. A wide variety of different options is available, so you must select the most suitable rotary hammer drill bit for the task at hand. You must consider the size of the bit – not only whether its diameter will fit the drill chuck, but also whether it is the right length for the required task.

Additionally, the material which the bit is made from should also play a role in your selection. Most SDS drill bits are manufactured from steel, often with various coatings and finishes applied. Popular options include carbide tipped (designed to maintain a sharper cutting edge for longer) and chrome-nickel molybdenum steel.

One final consideration to take into account when choosing a drill bit should be the brand. Many leading brands are available, offering top-quality SDS bits, but ultimately, your personal preference will depend on which manufacturer’s products you select.

Top Tip!

If you will be using standard drill bits with an SDS drill, you must ensure that the hammer action is disabled before use. This will avoid damaging the bit and will also help to keep you safe while operating the drill.

Browse SDS Drill Bits

Shop From Our Selection of SDS Drill Bits

Each
£11.78
  • RS Stock No. 349-9346
  • Mfr. Part No. 2608833789
Each
£4.85
  • RS Stock No. 349-9368
  • Mfr. Part No. 2608833807
Each
£7.11
  • RS Stock No. 231-1165
  • Mfr. Part No. 2608900239
Each
£115.26
  • RS Stock No. 188-7126
  • Mfr. Part No. D-00066
Each
£3.16
Each
£43.94
Each
£7.77
Each
£5.46

FAQs

RS Technical Team

The RS Technical Team provides expert technical reviews, ensuring articles are accurate, up to date, and aligned with industry best practices. With expertise spanning engineering, manufacturing, automation, maintenance, safety, and industrial products, the team plays a vital role in delivering content that readers can trust.

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy