- Published 7 Sept 2026
- Last Modified 13 Oct 2026
- 6 min
A Complete Guide to Fibre Optic Cables

What are They?
Offering significantly improved performance in terms of both bandwidth and data carrying than traditional metal conductor alternatives, this type of cable is an advanced type of network cable.
What is Optical Fibre?
Fibre optic technology is an effective cabled-based communication system. It is reliable, versatile, and widely used in many applications and industries.
This type of cabling is used to transfer information via pulses of light, which pass along one or more transparent plastic or glass pipes. In some cases, this can be more than several hundred pipes. Each of these strands is a little wider than an average hair and is normally surrounded by a further layer of cladding which is also in plastic or glass but constructed at a different density to the main inner strand.
A sheath made up of several layers of insulated casing is also wrapped around the cladded fibres. This usually comprises of a protective wrapper, known as a buffer tube, followed by a final outer jacket designed to protect the entire multi-stranded cable.
Uses
Optic cables are commonly found in a variety of applications such as the internet and broadband, phone lines, networking, and telecommunications. Additional uses in the home and workplace include lighting and interior decor.
They can save space compared to bulkier traditional cabling. This ability has also made it popular for many safety and lighting features in vehicles. Optical fibre technologies are widely used in many other demanding professional fields too, including in medical applications, for detailed mechanical inspections, and as sensors for monitoring and controlling the flow of various sorts of electrical currents, sounds and chemicals.
Uses in Internet and Networking
Fibre optic internet cable is increasingly popular. This is due to the higher speeds and bandwidth it can provide compared to standard ethernet or Wi-Fi signals delivered via coaxial or even copper wire from street-level exchanges. This means that fibre networking is a far better choice where high speeds are advantageous or for particularly intensive data transfer needs. Much of this is also true for phone lines.
Fibre optic bandwidth is usually significantly higher than a typical ethernet connection. It is also safe to use in high-voltage locations, and in areas where flammable gases or other harsh chemicals or weather conditions are likely to be a factor. This can be another important factor in choosing these cables for broadband delivery and telecoms as opposed to standard ethernet.
Uses in Lighting
LED lighting is also a common application of this technology in domestic and commercial environments. Fibre optics can transmit data in a clean and versatile manner across a wide spectrum of colours and patterns. This means that it is widely used in decorative lighting applications, accent lights, and feature lamps.
Far less electricity is also used by fibre optic LED lighting compared to standard bulb options, which makes it both environmentally friendly and economical. You can buy fibre optic lighting cables that are safe to use in a wide variety of applications and environments. They do not carry electrical current and are largely resistant to general wear, damage and degradation.
How Do They Work?
In understanding how optical fibres work and how data is sent through these cables, it is important to note that there are multiple components involved in its construction. All are required to ensure successful installation. The glass strands themselves are absolutely central to the system, but there is also a number of other key parts that play a role in effective data transfer.
Diagram
This handy diagram clearly illustrates the different components that make up a fibre optic cable. The fibre itself is comprised of a core and cladding.
As explained below, these have different refractive indexes to aid the travel of light along the cable. A protective coating, jacket or strength members will then encompass the core and cladding. This is then surrounded by an armoured outer jacket which forms the visible part of the cable. This may be IP-rated for water-blocking purposes.

How Does It Work?
This second diagram shows the basic principle of the technology and how it works.
Light enters at one end of the cable and travels through the highly refractive core, bouncing off the cladding which has a low refractive index for this exact reason. Once a beam reaches the end, it is dispersed at an approximately 60° angle and emitted to the target.

Advantages
Fibre optic cabling has several major characteristics which provide a strong advantage compared to traditional copper conductor cables.
Key advantages include:
- Distance - because of their low signal power loss rate, they are able to carry optical signals over far longer distances than older types of cabling. With the ideal combination of network setup, materials, and wavelength, some single fibre optics are effective at carrying signals over hundreds of kilometres. In comparison, standard copper cables have a limitation of 328-feet for good quality transfer distance.
- Bandwidth and data transfer - copper data cables offer quite limited bandwidth in comparison.
- Speed - these cables enjoy a significant speed advantage compared to other data transfer modes because they use light pulses as the primary information conveyance source. In this regard, it typically outstrips the expected performance of even high-grade copper cables such as Cat5 and Cat6.
Types
There are multiple fibre optic cable types, and it is important to understand the differences between each one. Each has distinct advantages and will be suited to varying environments, applications, or industries.
Some of the main types are explored below:

Glass
In terms of bend and flex, glass optical fibre is more delicate than its plastic counterparts. This also means that it is more susceptible to damage - especially if it has to loop tightly or be moved continually over its run length. It cannot be cut, repaired, or spliced, which means that it is not suitable for applications where high levels of flexibility are needed.
Despite this, they are sturdy and durable in terms of both mechanical strength and overall resistance to chemicals, moisture, fluctuating temperatures, and extreme environments. This makes it well-suited to longer-distance applications where cables are often submerged or buried. Due to the many different fittings, adapters, and configurations available, it is also noted for its versatility.
This type is regularly used in challenging and longer-distance applications. It often costs more to purchase and install than more economical plastic variations, which also boast greater flexibility and ease of use for most non-specialised applications.
Single-Mode Cables
Single-mode and multimode optical fibres are varying cable configuration types. They deliver different potential performance levels at distance.
Single-mode fibre optic cables are comprised of one glass fibre strand with a fairly slim core diameter. Far less internal reflection is involved as light rays pass through it, therefore reducing attenuation and allowing for far higher speed data transfer over longer distances. This configuration is typically used for long-distance signal transmission.
Multimode Cables
Conversely, multimode cables feature larger cores that guide many modes simultaneously. Multimode fibre cabling significantly increases reflection. This results in higher attenuation and dispersion rates, therefore increasing bandwidth delivery over short distances. Applications needing large data volumes sent over shorter runs (such as communication data in or between a small localised area) typically utilise multimode fibre optic cabling.
Multimode fibre, also known as multi-core, is available in various specifications. Common everyday networking fibre optic cable configurations include two-core options, eight-core varieties, and even twenty-four-core fibre optic cable. Essentially, the bandwidth potential and the ability to cope with higher data throughput over shorter distances is determined by the number of cores the cable carries.