• Published 5 Aug 2024
    • Last Modified 22 Aug 2024
  • 5 min

Ohms Law Calculator

Use our Ohm’s Law calculators to accurately calculate Ohm’s Law and determine the Voltage, resistance, or current value you require for your installation.

Our Ohm’s Law calculators enable you to easily obtain unknown values in the Ohm’s Law equations simply by providing any two known values. In resistive circuits, this allows you to determine the relationship between power, resistance, current, and Voltage.

Simply enter any two known values into the respective tool, be it for resistance or power, below, press "calculate", and Ohm's Law will determine the remaining value.

Ohms Law Calculator formula explained

In this formula for Ohm’s Law:

V = I * R

V = Voltage, measured in Volts (V)

I = Current, measured in Amps (A)

R = Resistance, measured in Ohms (Ω)

As Ohm’s Law states that V = I * R, for a given constant Voltage, higher resistance entails a lower flow of current. The reverse is equally true as well. The higher the current flow, the lower the resistance for the constant Voltage. This is represented visually by the Ohm’s Law triangle you can see at the top of the calculator.

Ohms Law Power calculator formula explained

Our second Ohm’s Law calculator utilises the equation:

P = V * I

Whereby:

P = Power, measured in Watts (W)

V = Voltage, measured in Volts (V)

I = Current, measured in Amps (A)

You can use our calculator above to work out the remaining value depending on the two known values, employing the Ohm’s Law formulas.

Ohm’s Law describes the connection between resistance, current, and Voltage simply by stating that the current flowing through a conductor is directly proportional to potential difference between two points. In many materials, this holds true at a variety of currents and Voltages.

Essentially, Ohm’s Law states that the Voltage difference between two points, the electric current flowing between those points, and the resistance along the current path are all related and proportional. The Voltage difference across the terminals of a two-terminal device such as a fixed resistor directly affects the current passing across the device.

No matter whether the current or driving Voltage is time-varying (AC) or constant (DC), Ohm's Law applies to circuits that contain only resistive elements - so no inductors or capacitors. We can express it using several equations as outlined above and depicted in the Ohm’s Law triangle.

Disclaimer: The information provided by this digital calculator is intended for general guidance purposes only. While we strive for accuracy, we advise users to consult the manufacturer's technical specification sheets for detailed and precise information. We cannot guarantee the completeness or reliability of the data presented here. For specific applications and critical decisions, always refer to the official technical documentation provided by the manufacturer.

Browse some of our key product ranges and related content below.

Chassis mount fixed resistor

Fixed Resistors

Fixed resistors have a set, unchangeable resistance value. They are the most common resistor type and are also among the most-used electronic components.

Potentiometer

Variable Resistors

Allowing the amount of resistance to be changed, variable resistors are vital in a circuit. Their value can be adjusted from virtually zero Ohms to a set, determined value.

Electrical wiring

A Guide to Cables

In this guide, we will navigate through the various types of cables, their applications, regulations, and safety considerations.

Related links

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy