- Published 22 Oct 2025
- Last Modified 22 Oct 2025
- 6 min
Quantum Computing vs Climate Change
Quantum computing revolutionises climate action, simulating complex systems for a sustainable future.

Quantum computing has the power to achieve chemistry breakthroughs that not only allow industry to operate more sustainably but also present real solutions to the climate crisis.
What is Quantum Computing and Why Does it Matter to Climate Change?
Quantum computing operates at a vastly more powerful and complex level than classical computing. It uses principles of quantum mechanics such as superposition and entanglement to process information, giving it the ability to simulate complex systems in order to solve complex problems.
Because of its power, theoretically, many real-world problems can be solved using quantum computing algorithms compared to traditional computing power, including solutions to combat climate change.
Experts already surmise the theoretical applications of quantum computing for sustainable practices. Challenges such as reducing the emissions from fertiliser and cement production, to producing more sustainable batteries and more efficient solar panels.
Quantum computing can also be applied directly to the challenge of accurate climate modelling and mitigation strategies for extreme weather events.
Potential Use Cases in Industrial Sustainability
Industry accounts for 25% of carbon dioxide emissions. Innovation in this area to reduce emissions and climate change acceleration is urgently needed.
By applying quantum computing to sustainability goals, it’s possible to achieve the vast computational requirements that stand between theory and innovative design.
Here are just some of the breakthroughs that could present a significant impact on sustainability:
New Battery Chemistries
There are a number of sustainability issues linked to traditional batteries. They rely on mining rare earth elements, such as lithium, cobalt, and nickel, the extraction of which is energy-intensive and environmentally destructive.
The development of new battery chemistries from more abundant sources, such as sodium or aluminium, for example, could be the answer.
However, it requires extensive research into and modelling of molecular interactions. This is where quantum computing could assist. Quantum simulation of these interactions could lead to the discovery of safer, more sustainable battery chemistries, lessening adverse effects on the climate.
Improving Solar Panels and Grid Distribution
Breakthroughs in solar panel development lie with something called singlet fission, a process where the dynamics of photon molecule absorption create an excited state. This excited state causes the photon to split into two triplet states. Normally, solar cells have a supposed limit of 33% efficiency. However, this is a state of concentrated energy that can ultimately double the electrons that can generate current, making the process more efficient.
Quantum computing can also be applied to the various challenges of efficient renewable energy distribution. The power of quantum algorithms is such that it can integrate real-time consumption rates and weather patterns to make decisions about power storage and distribution. Applying this to a grid would make the use of renewable energy more efficient and ensure a more dependable supply.
Enhancing Green Hydrogen Production
Combining quantum optimisation and digital twin approaches allowed one company to propose a method for improving the efficiency of green hydrogen production. The quantum digital twin replicated the operations of a green hydrogen production factory and used these inputs to focus on optimising the electrolysis process, which breaks the chemical bond in water to extract the hydrogen.
The water-splitting process has historically been quite expensive; however, results from the test showed a 5% increase in hydrogen production and a 5% revenue increase.
Enzyme Modelling for Greener Fertiliser Production
The production of fertiliser contributes to 2% of global C02 emissions. Contributing to this are the temperatures needed to produce fertiliser traditionally. This method combines nitrogen with hydrogen at high pressures and temperatures, around 400 degrees, producing the ammonia needed for fertiliser.
However, we know that microbes produce ammonia through chemical reactions at much lower temperatures using enzymes.
The crucial area for development using quantum computing is our understanding of nitrogenase, a bacterial enzyme that converts nitrogen into ammonia. How nitrogenase works is incredibly complex. However, quantum computing’s ability to understand and simulate nitrogenase reactions and model them could pave the way for more energy-efficient fertiliser production.
Climate Modelling and Prediction
Current climate forecasting models, which must contend with the complexity of atmospheric patterns, ocean current dynamics, and radiation transport, could be greatly enhanced by the power and simulation capabilities that quantum computing could offer.
The potential power to predict catastrophic weather events, the likelihood of which is increasing with climate change, would be transformative globally and more significant for the most vulnerable communities amid the climate crisis.
The technology could allow for improved preparation and mitigation strategies as well as provide an incentive for policymakers to push for more stringent rules around emissions and greater investment in renewables and climate initiatives, such as reforestation.
Offsetting the Impact of Quantum Computing
Quantum computing is, itself, a challenge to sustainability. The main demands it makes of the environment come from its high energy and cooling requirements, even when not actively in use.
The need for constant, high levels of power is needed to enable its precise controls. These also need power to protect them from interference such as vibrations, electromagnetic fields, and temperature changes.
The temperatures needed to protect the quantum states the computer works in are close to absolute zero, powered by helium, of which there is a rare supply.
However, quantum computing’s ability to accelerate our understanding of, and response to, climate change is seen by many as a far greater contribution to alleviating humanity’s current crises, and these results would offset the current impact on the environment.
Using Quantum Computing to Improve Environmental Reporting Accuracy
Quantum computing also holds the key to improving our understanding of just how impactful our behaviours are on the environment.
Currently, the volume of environmental data - everything from correct carbon emission readings to individual community behaviours relating to sustainability - is far too unwieldy to give an accurate picture.
Quantum computing algorithms offer a way to integrate all of this data (in a way that traditional systems can’t), identifying and bringing to light minute patterns and processes that lead to a greater climate burden.
This understanding would allow us to improve ESG reporting standards for the industry and improve guidance and regulation for those in the worst offending areas. Improved ESG reporting may also be used as a vehicle for obtaining greater financial investment in the industry, which demonstrates greater sustainability levels through a more accurate framework.
What’s Next for Quantum Computing?
Since last year alone, there has been a 183% increase in investment in quantum computing, up $355,644,534 in 2024 to $1,007,497,500 in 2025.
According to McKinsey’s report, The Year of Quantum, Japan made a large, single-year public funding announcement of $7.4 billion in 2025, while the UK's primary commitment is £2.5 billion (approximately $3.1 billion), which is spread over 10 years (2024-2034)
While the focus may not always or primarily be climate-focused, huge Silicon Valley names, IBM, Google, and META, as well as dedicated chemistry firms, are exploring the possibilities of quantum computing applications.
The timeline for these breakthroughs, however, is something that’s much debated, with many insinuating we’ll have to wait possibly a decade or more to see the results of this investment.
The AI, data, and robotics partnership is fundamentally transforming industry. By mastering multimodal AI for quality control and predictive maintenance, manufacturers can gain a crucial competitive edge, which 92% of executives now view as essential for success.
Related Articles
Related links
- Quantum Computing vs Cryptocurrency: The Race for Post-Quantum Security
- The gradual impact of ESG
- Comparing Carbon Credits vs Renewable Energy Certificates
- How to Make Single-use Devices More Sustainable
- The Race for Quantum Computing Supremacy
- Quantum Filter Solutions: Low, High & Band Pass
- Driving smarter, more sustainable waste practices
- Supply Chain Decarbonisation Solutions for Industry