As organisations come under more pressure to reduce carbon emissions and improve their sustainability credentials, procurement must now demonstrate how it can play its part. This means looking internally but also at the wider supply chain.
Environmental, social and governance (ESG) issues are now front of mind for procurement professionals, as the pressure to reduce carbon emissions from the supply chain and ensure businesses operate responsibly continues to grow.
The 2025 Indirect Procurement Report, produced by RS and the Chartered Institute of Procurement & Supply (CIPS), finds almost two-thirds (64%) of respondents say ESG is now an important part of their company strategy – up from 52 per cent a year ago – and just 11 per cent feel this is unimportant, down from 21 per cent in 2023.
This emphasis is reflected in procurement’s own focus; more than half (53%) now have a sustainable and ethical procurement policy – up from 26 per cent in 2023 – and just under half (48%) have a strategy to reduce their carbon footprint.
Helen Alder, Head of Knowledge & Learning Development at CIPS, says the growing prominence of ESG is due to a combination of the wider pressure on businesses to improve their sustainability credentials and an increasing emphasis on reporting emissions through legislation such as the EU’s Corporate Sustainability Reporting Directive.
“This is starting to apply not just to organisations that investors have to put a value on,” she points out. “I think it’s going to become a social norm that all organisations of a certain size have some kind of carbon rating on them, and they will thrive or not because of that.”
Holding carbon to account
The main areas of focus for organisations when it comes to reducing carbon footprint are waste recycling, used by 72 per cent, energy management (58%), reduced energy usage (56%) and cutting down on plastic packaging (54%). But Alder points out that, while these can have an impact, the biggest potential for positive improvements is likely to come from within the wider supply chain.