A Complete Guide to Sensor Connectors and Cables

A guide to sensor connectors and sensor and actuator cables, discussing their uses, working, and the different types.

Reviewed by Mithun Subbaroybhat, Technical Support Engineer (January 2022)

What are Sensor Connectors?

Sensor connectors are electrical interfaces used to connect sensors and actuators to cables, junction boxes and control equipment. They provide detachable connections for transmitting power, electrical signals or communication data. Common industrial designs include M8 and M12 circular connectors, available with different contact configurations, coding options and environmental protection ratings.

What Do Sensor Connectors Do?

Alongside sensor and actuator cables, sensor connectors feature technology which enables them to integrate into industrial automation processes and systems seamlessly. In short, these connectors are used to join the corresponding cables and components with the switches, sensors, and equipment which make up the industrial automation process. All of these separate components are then joined together to work as one automated unit, helping to increase productivity and minimise downtime.

Sensor connectors and cables are suitable for use with a wide range of switches, sensors and transducers. They provide electrical connections that allow power and signals to pass between compatible devices and equipment.

Different sensor connectors are best suited to various applications and can be installed in diverse environments. As such, selecting the appropriate connector depends on the requirements of the connected equipment and its operating environment.

Technician connecting a circular electrical connector to industrial equipment alongside multiple cables.

Sensor Connectors and Components

Sensor connectors consist of several components that work together to provide a secure electrical connection between sensors, cables and control equipment. The design and materials used can vary depending on the connector type and its intended application.

The main components of a typical sensor connector include:

  • Contacts: Metal pins or sockets that establish electrical connections, allowing power and signals to pass between compatible devices.
  • Housing: The outer casing that protects the internal components and provides mechanical support.
  • Insulator: A non-conductive component that separates the electrical contacts and helps prevent short circuits.
  • Seals: Components that help protect against dust and moisture, depending on the connector's design and ingress protection rating.
  • Coupling mechanism: A feature, such as a threaded locking system, that secures the connector to its mating component.

Sensor connectors are commonly used alongside sensor and actuator cables, which contain the electrical conductors that carry power and signals between connected devices. Together, these components provide a connection suitable for the requirements of the sensor and its operating environment.

In addition to their physical characteristics, sensor connector assemblies may need to support specific communication interfaces or meet safety requirements, depending on their intended application.

IO-Link

IO-Link is a standardised, point-to-point communication technology used in industrial automation. It enables compatible sensors and actuators to exchange data with an IO-Link master, which can connect to higher-level industrial Ethernet or fieldbus networks.

ATEX

ATEX refers to European regulations covering equipment and protective systems intended for use in potentially explosive atmospheres. Sensor connectors used in these environments must be suitable for the relevant hazardous-area classification and installation requirements.

Types of Sensor Connectors

There are multiple types of sensor connectors, each suitable for different uses and applications. They are available in various sizes, materials and contact configurations, making it important to select a connector that is compatible with the sensor, cable and equipment being used.

Sensor connectors can be classified by their intended application, such as oxygen, pressure, speed or temperature sensing, or by their physical connection type, such as M8 and M12 connectors.

Sensor Connector Features

Different sensor connectors offer various features depending on their design and intended application. The table below outlines some common sensor connector types, their technical characteristics and typical uses.

Connector type
Technical characteristics
Typical applications
O2 sensor connectorsAutomotive-specific contact arrangements and housings, with temperature resistance depending on the designConnecting oxygen sensors in vehicle exhaust systems
Pressure sensor connectorsAvailable with different contact configurations, electrical interfaces and environmental protection ratingsIndustrial pressure sensors and transmitters
Speed sensor connectorsApplication-specific electrical connections, with vibration and environmental resistance depending on the designAutomotive wheel-speed sensors and industrial speed monitoring
Temperature sensor connectorsConnection requirements vary depending on whether the device uses a thermocouple, RTD or temperature transmitterIndustrial temperature measurement and monitoring
M8 connectors8 mm nominal threaded coupling interface, available in different contact configurationsCompact industrial sensors and actuators
M12 connectors12 mm nominal threaded coupling interface, available in multiple contact configurations and coding optionsIndustrial sensors, actuators and communication systems

M8 and M12 refer to the physical connector interface, while oxygen, pressure, speed and temperature connectors are categorised by their application. These categories can overlap, as some pressure and temperature sensors may use M8 or M12 connections.

Sensor and Actuator Cable Connection Types

Both male and female connection types are available, alongside a wide range of different sizes and materials used in the manufacturing process. Some connector types have varying numbers of pins, making them suitable for different cables and components. As explored above, each distinct type of sensor connector has unique benefits and advantages. Still, it is also important to consider the connection type when choosing sensor connectors for your application.

3-pin connectors feature three distinct pins for connection to specific cables and components. They can be used with various cable assemblies for a range of sensing tasks.

4-pin connectors are ideal for a range of uses and applications. Suitable for use with a variety of electronic sensor types, 4-pin connectors can vary in size and gender.

5-pin connectors are characterised by their five pins, typically housed in a protective outer casing. They are suitable for a range of devices and applications including cable assemblies and distribution units.

Sensor Connector Applications

Sensor connectors are used across a wide range of industries and applications, providing electrical connections between sensors, actuators and control equipment. They are particularly common in industrial process control and automation environments, where reliable connections are important for monitoring equipment and maintaining efficient operations.

Some common applications of sensor connectors include:

  • Industrial automation: Connecting proximity sensors, photoelectric sensors and other sensing devices to control systems used in automated production lines.
  • Manufacturing: Connecting sensors used to monitor machinery, detect objects and track equipment position or movement.
  • Food and beverage processing: Connecting sensors used to monitor temperature, pressure and other process conditions. Suitable connectors may offer protection against moisture and cleaning chemicals.
  • Automotive: Connecting oxygen, pressure and speed sensors to vehicle electrical and electronic control systems.

The most suitable sensor connector depends on the requirements of the application, including the type of sensor, electrical connection, operating conditions and environmental protection needed.

Explore our range of electrical power and industrial cables to find suitable cabling for your application, or browse our full selection of cables and wires at RS.

Popular Brands

RS PRO Sensor Connector

RS PRO

Browse the full range of products available from RS PRO, our in-house brand, and discover the best sensor connector for your task.

Shop RS PRO

R2192460-01

Omron

Shop the full selection of Omron sensor connectors and choose the most suitable product for your application.

Shop Omron

FAQs

Lorna Little

Lorna is an SEO Content Specialist at RS, where she creates search-led content focused on topics including industrial innovation, engineering, maintenance, and procurement. After studying Creative & Professional Writing at Canterbury Christ Church University, she built her career in SEO and content marketing across both agency and in-house environments, helping readers navigate technical subjects through informative, user-focused content. Outside of work, Lorna enjoys reading, travelling, and making memories with her family.

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy