- Published 21 Feb 2025
- Last Modified 21 Feb 2025
- 7 min
Pressure Washer Guide
Pressure washers are essential tools for tackling tough cleaning jobs around your business or home. This guide explores what they are, the different types and how to use them.
Reviewed by Stephen Bettles (Technical Support Engineer, January 2025)
Pressure washers are highly effective tools that simplify and expedite various cleaning tasks. Whether you're tackling grime on your patio, driveway, or car, a pressure washer can help you achieve a spotless finish efficiently. In this comprehensive guide, we'll delve into what a pressure washer is, explore the different types available, and offer tips on selecting the best one for your specific needs.
What is a Pressure Washer?
A pressure washer is a dynamic cleaning device that employs high-pressure water to dislodge dirt, grime, and other unwanted substances from various surfaces. They are widely used for cleaning and maintenance in both commercial and residential settings to clean driveways, patios, vehicles, and even buildings.
How Does a Pressure Washer Work?
A pressure washer operates by pressurising water and expelling it at high velocity through a nozzle. Water is typically drawn from a source such as a garden hose and then channelled through a motorised pump. The pump significantly boosts the water pressure, which is quantified in pounds per square inch (PSI). The source can also be rainwater, or other containers like a bucket or water butt to supply a pressure washer.
What Does PSI Stand for in Pressure Washers?
PSI stands for pounds per square inch, a unit of pressure measurement. In the context of pressure washers, PSI denotes the force with which water is expelled from the nozzle. A higher PSI translates to greater cleaning power, enabling you to tackle stubborn dirt and stains more effectively.
When selecting a pressure washer, consider key factors such as PSI, flow rate, nozzle types, and additional features like adjustable pressure settings or detergent injection.
Types of Pressure Washers
Pressure washers come in various types to cater to different cleaning needs and applications. Here are some of the most common types of pressure washer:
Commercial Pressure Washers
If you require a pressure washer for commercial use, you'll need a machine designed to withstand intensive usage and deliver superior performance. Commercial pressure washers are built to handle large-scale cleaning tasks such as washing vehicles, industrial equipment, or extensive outdoor surfaces. These machines are equipped with powerful motors and high-pressure pumps to tackle even the most challenging grime and dirt.
Electric Pressure Washers
Electric pressure washers are perfect for light-duty use, offering a pressure range of around 1300–2000 PSI, meaning they’re a great choice for homeowners for cleaning cars, patios and outdoor furniture. They are powered by electricity, which means their mobility is restricted as they need to be connected to a power source, but they are typically lighter, quieter and cheaper than petrol pressure washers.
Petrol Pressure Washers
Petrol pressure washers are designed for heavy-duty use, making them a perfect choice for professionals for larger cleaning projects. Powered by petrol, these pressure washers typically offer a higher pressure range of 2000-4000 PSI, which allows them to wash industrial equipment and remove paint. As they don't require an electrical outlet, petrol pressure washers are portable and provide greater versatility for outdoor tasks. But often, they are heavier, noisier, and need more upkeep, such as frequent fuel and oil changes, meaning they’re not the most convenient choice for occasional use.
Diesel Pressure Washers
Like petrol powered pressure washers, diesel powered washers are also used for heavy-duty and professional use. These machines are typically more expensive than their petrol counterpart, however they are more powerful and fuel efficient. With this power difference compared to petrol pressure washers, they are also a lot louder and heavier due to the size of their engines, making it harder to manoeuvre them.
Battery Powered Washers
Battery powered pressure washers are compact, less powerful washers compared to your standard pressure washer. Due to the lower pressure, these are much less likely to cause any damage, making them a great option for cleaning things such as cars, bicycles, tools, patios and windows. Due to their size, and being cordless, these washers are great for home and on-the-go use.
Pressure Washer Parts
Pressure washers usually have interchangeable parts and accessories for various job requirements. Below are some examples of the most common parts you can interchange:
- Nozzles: Depending on the task, different nozzles can be used, such as a smaller jet for tough dirt or grime or a wider angle for general cleaning. Typical spraying patterns include 0°, 15°, 25° and 40°.
- Hoses: You can replace the hose of a pressure washer, depending on the flexibility, durability or length of hose needed.
- Pumps: Different types of pumps include axial, triplex and wobble with each one offering different durability and pressure levels.
- Filters: There are water inlet filters and air filters. Filters can be replaced or upgraded if they are clogged or damaged.
- Detergent compartment: Some pressure washers include detergent or soap tanks, and these can be replaceable depending on the pressure washer’s design.
From hose extensions to nozzles, RS carries an assortment of pressure washer parts for various applications.
What is the Best Pressure Washer?
Selecting the best pressure washer for your needs involves considering several important factors. One of the most crucial aspects is the cost. Pressure washers can vary significantly in price depending on their features, power, and brand.
However, it's important to note that the cost of a pressure washer is not the only factor to consider. You should also evaluate the PSI, flow rate, nozzle types, and any additional features that are important to you.
How to Use a Pressure Washer Safely
Wondering how to use a pressure washer? Using a pressure washer safely is paramount to avoid damage to surfaces and injury to yourself or others. Here are some essential safety tips to keep in mind:
Read the Manual: Before using your pressure washer, thoroughly read the manufacturer's manual. This will provide you with important information about the machine's operation, maintenance, and safety precautions.
Wear Protective Gear: Always wear appropriate protective gear, including safety goggles, gloves, and sturdy footwear. This will help protect you from high-pressure water jets and any debris that may be dislodged during cleaning.
Check the Area: Before you start cleaning, inspect the area for any potential hazards such as loose debris, electrical outlets, or delicate surfaces that could be damaged by high-pressure water.
Maintain a Safe Distance: When using the pressure washer, maintain a safe distance from the surface you are cleaning. This will help prevent damage to the surface and reduce the risk of injury.
Use the Right Nozzle: Select the appropriate nozzle for the task at hand. Different nozzles offer varying spray patterns and pressure levels, so choose one that matches your cleaning needs without causing damage to the surface.
Test on a Small Area: Before cleaning a large area, test the pressure washer on a small, inconspicuous spot to ensure it doesn't cause any damage or unwanted effects.
Follow Maintenance Guidelines: Regularly maintain your pressure washer according to the manufacturer's recommendations. This includes checking hoses and connections, cleaning filters, and storing the machine properly when not in use.
Browse the extensive selection of cleaning equipment that RS has to offer including pressure washers and pressure washer parts, for a range of different applications.
Related Articles
Related links
- Pressure Washers
- SIP 8981 Hot Water Pressure Washer, 230V 120bar 39600L/h
- Karcher HDS 6/12 C Hot Water Pressure Washer, 240V 120bar 560L/h
- SIP PH480/150 Hot Water Pressure Washer, 230V 140bar 480L/h
- SIP PH540/150 Hot Water Pressure Washer, 230V 150bar 540L/h
- Karcher HDS 7/10-4 M Hot Water Pressure Washer, 240V 100bar 700L/h
- Bosch Pressure Washers
- Karcher 2.642-301.0 Pressure Washer Hose for K Series Pressure washers