- Lorna Little
- Published 8 Sept 2026
- Last Modified 6 Nov 2026
- 5 min
What is a Cable Rod?
This guide provides a comprehensive overview of cable rods, including their uses and accessories, to help you choose the right cable rod for your needs.

Cable rods, also known as cable pulling rods or cable installation rods, are long, flexible rods that are used to run cables and wires through ducts or conduits. They are typically made of fibreglass or composite materials, which makes them lightweight, strong, and durable.
Cable rods come in various lengths and diameters to suit different installation requirements. Cable rods are an essential tool for many businesses, particularly those in the construction and utility industries, as they make it easier to install and maintain electrical systems.
If you’re in the market for cable rods, you may be wondering what they are, what they’re used for, how they work, and the different types available. This guide aims to answer those questions and provide you with a comprehensive understanding of cable rods.
What are Cable Rods Used for?
Cable rods are used in a variety of industries and applications, including:
- Electrical installations: Cable rods are used to run electrical cables and wires through conduits and ducts during the construction or maintenance of electrical systems
- Telecommunications: Cable rods are used to install or repair cables and wires for phone, internet, and TV services
- Plumbing: Cable rods are used to run pipes and cables through tight spaces in buildings, such as under floors or behind walls
- Automotive repair: Cable rods are used to thread wires through tight spaces in car engines during repairs or maintenance
Cable Rod Sets

Cable rod sets are kits that include several cable rods and accessories, such as hooks, attachments, and carrying cases. They are designed to provide everything you need to install or repair cables and wires in a convenient package. Cable rod sets come in assorted sizes and configurations to suit different installation requirements.
Some cable rod sets are designed for specific applications, such as telecommunications or automotive repair, while others are more versatile and suitable for a range of applications. When choosing a cable rod set, it’s important to consider the length and diameter of the cable rods, as well as the accessories included. Some cable rod sets also come with additional features, such as glow-in-the-dark or threaded rods, to provide added functionality.
Cable Rod Accessories
In addition to cable rods themselves, there are various accessories available that can enhance the functionality and ease of use of cable rods. Here are some common cable rod accessories:
Cable Rod Gliders
Cable rod gliders feature a whisk-shaped head attachment that is designed to join the head of the cable. They’re designed to reduce friction and abrasion between the cable and the conduit or duct, making it easier to pull the cable through without damaging the connector.
Cable Rod Hook and End Rings
Cable rod hook and end rings are versatile accessories that can be attached to the end of a cable rod to help grip the cable or wire during installation or repair. The hook or ring can be used to attach the cable to the cable rod, providing a secure grip for pulling or pushing and guiding the cable. They can also be used to retrieve cables from tight spaces and difficult-to-access areas.
Cable Rod Magnet Heads
Cable rod magnet heads are attachments that can be added to the end of a cable rod to help retrieve cables and connectors. They are advantageous as the magnet can retrieve components without the need to manually fix the attachment, aiding in both speed and ease of use.
Cable Rod Grippers
Cable rod grippers are a type of cable grip that attaches to the end of the cable and provides a secure grip for pulling. The compression-style gripper enables the accessory to fit various cable sizes to accommodate different cable diameters and installation requirements.
Cable Rod Inspection Beams
Cable rod inspection beams are accessories that can be attached to the end of a cable rod to provide additional visibility during cable installation or repair. The inspection beam typically consists of a bright LED torch light that can illuminate the inside of the conduit or duct, making it easier to see and work with the cable.

Lorna is an SEO Content Specialist at RS, where she creates search-led content focused on topics including industrial innovation, engineering, maintenance, and procurement. After studying Creative & Professional Writing at Canterbury Christ Church University, she built her career in SEO and content marketing across both agency and in-house environments, helping readers navigate technical subjects through informative, user-focused content. Outside of work, Lorna enjoys reading, travelling, and making memories with her family.