Press Releases


RS Components launches IP67 industrial digital multimeter

Fluke 87V upgrade offers 4m drop resistance, electrical noise shielding and enhanced battery life

London, UK, 18 December 2019:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel provider of industrial and electronic products and solutions, has introduced the new Fluke 87V MAX true-RMS digital multimeter (DMM), designed for use by maintenance engineers in the most demanding industrial environments. An enhanced version of the popular Fluke 87V DMM, the 87V MAX comes with an IP67 rated casing, doubled battery life, and all the features required to efficiently troubleshoot almost any electrical problem in, for example, motor drives, plant automation, power distribution and electromechanical equipment.

The industrial-strength casing of the Fluke 87V MAX is designed and tested to withstand drops up to 4 metres in its holster. Waterproofing and dustproofing to IP67 standards and an extended operating temperature range from –15° to +55°C (down to –40°C for up to 20 minutes) and up to 95% humidity make the 87V MAX more than equal to extreme environmental conditions.

All the advanced features of the 87V are incorporated into the 87V MAX, including voltage measurement up to 1000V AC or DC, current measurement up to 10A (or 20A for 30 seconds), and true-RMS AC voltage and current readings to accurately measure non-linear signals. The capacitance measurement range is 10,000μF and the frequency range is 200kHz. Other features include resistance, continuity and diode test, and a relative mode to remove test lead resistance from low-ohm measurements.

The 87V MAX true-RMS digital multimeter provides the resolution and accuracy to efficiently troubleshoot motor drives, plant automation, power distribution, and electromechanical equipment even in loud, high-energy, and high-altitude locations. It includes a unique function for accurately measuring noisy signals at the variable frequency drive and at the motor terminals: special shielding blocks high frequency, high-energy noise generated by large drive systems. It correctly measures pulse-width modulated motor drive signals.

The Fluke 87V MAX industrial multimeter is safety rated to CAT III 1000V and CAT IV 600V. It is available now from RS in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components is a trading brand of Electrocomponents plc. We offer more than 500,000 industrial and electronic products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

We support customers across the product life cycle, whether via innovation and technical support at the design phase, improving time to market and productivity at the build phase, or reducing purchasing costs and optimising inventory in the maintenance phase. We offer our customers tailored product and service propositions that are essential for the successful operation of their businesses and help them save time and money.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2019 reported revenue of £1.88 billion. Electrocomponents has seven operating brands: RS Components, Allied Electronics & Automation, RS PRO, OKdo, DesignSpark, IESA and Monition.

For more information, please visit the website at https://uk.rs-online.com/web/

Editorial Contact:
Aakriti Kaushik
PR Manager – Northern Europe
RS Components
aakriti.kaushik@rs-components.com

PR Agency Contact:
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0) 1225 470000



Further information is available via these links:

Twitter: @RSComponents; @designsparkRS

Linkedin: www.linkedin.com/company/rs-components

RS Components

www.rs-online.com

DesignSpark

www.rs-online.com/designspark

Electrocomponents plc

www.electrocomponents.com