Press Releases


RS Components introduces new Fluke tester to simplify testing and measurement of industrial control valves

Fluke 710 provides technicians with simple and easy method to measure control valve data and make maintenance decisions

London, UK, 24 January 2019:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel distributor, has announced availability of the Fluke™ 710 mA Loop Valve Tester, which is an easy-to-use tool that greatly simplifies the testing of control valves, enabling the quick measurement of critical valve readings using a simple two-wire connection.

Traditionally, complex equipment has been used for control valve testing, but use of these complicated devices has meant extensive training for users, as well as removal of the control valve under test, and potentially one or two hours of bench testing. However, the Fluke 710 offers built-in test procedures and a highly intuitive interface including valve status indicators.

Importantly, the device provides quick checks of control valves while they are in place in a system. It sources the 4-20mA current loop signal and causes the smart control valve to move, while simultaneously interrogating the HART communication protocol data to collect critical diagnostic information about the valve’s position and status. Therefore, the tester enables technicians to make fast and confident decisions on whether maintenance, and potentially system downtime, is required or not.

The built-in pre-configured valve-test routines offered by the Fluke 710 include: manually changing the mA signal and viewing the HART position and pressure variable information; full range ramping of the signal while recording the position or applied pressures, in terms of percentage from 0 to 100 to 0%; evaluating the valve’s response to changes in the mA input; speed tests to determine how fast the valve can open or close; and bump and partial stroke tests to test valves over a portion of their range.

Measurements and other test results are recorded and stored in the Fluke 710’s memory, where they can be uploaded to the Fluke ValveTrack™ analysis software, which is included with the tester. This enables technicians to plot logged valve tests taken in the field, as well as the ability to compare previous uploaded tests to recent tests.

The Fluke 710 tester is now shipping from RS in the EMEA and Asia Pacific regions. The datasheet is available here.

-Ends-

About RS Components

RS Components, Allied Electronics & Automation and IESA Ltd are the trading brands of Electrocomponents plc, a global multi-channel distributor. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2018 had revenues of £1.71bn.

For more information, please visit the website at https://uk.rs-online.com

Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000

Further information is available via these links:

Twitter: @RSComponents; @designsparkRS

Linkedin: www.linkedin.com/company/rs-components

RS Components

www.rs-online.com

DesignSpark

www.rs-online.com/designspark

Electrocomponents plc

www.electrocomponents.com