Press Releases


RS Components now stocking new series of high-efficiency fans and controllers from ebm-papst

New fan controllers deliver temperature-sensitive fan speed control

London, UK, 17 May 2018:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has announced the availability of new energy-efficient fan controllers together with the 4300N series of fans from ebm-papst, one of the world’s leading makers of high-efficiency fans and motor products.

The latest fan controller solutions are low-cost, credit-card-sized devices. The DCP controllers offer optimised power consumption by providing temperature-sensitive speed control for four-wire PWM controlled compact fans at 12, 24 and 48V DC. The EC range offers temperature control for compatible fans fitted with energy-saving motors.

Both ranges offer a choice of pre-set temperature profiles and are supplied with a 2m temperature sensor lead, enabling a set of alarm functions such as over-temperature, fan and sensor failure, all without the need for an additional power supply to operate them. This latest generation also includes the brand new Configurable Generic Controller (CGC), which is suitable for both DC and EC fans and enables customers to adapt temperature profiles, making them ideal for use as a development kit.

Also available from RS is the 4300N series of DC axial fans, which offers high airflow (up to 285m³/h) with low operating noise and high efficiency. The 119 x 119 x 32mm series features improvements such as specially formed discharge vanes and innovative winglets on the blade tips to improve the aerodynamic efficiency and prevent turbulence that can cause noise. More specialised versions are also available that offer speed signal output, PWM input, moisture protection, IP68 protection and external temperature sensor. This enables the fans to target a range of industries and applications including computing and telecommunications, drives, automation, solar inverters, as well as automation and a wide selection of other industrial applications.

The ebm-papst 4300N series of DC axial fans and fan controllers are now shipping in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components and Allied Electronics & Automation are the trading brands of Electrocomponents plc, the global distributor for engineers. We offer more than 500,000 industrial and electronic products, sourced from 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we trade through multiple channels and ship around 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2017 had revenues of £1.51bn.

For more information, please visit the website at www.rs-online.com.

Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com
+44 (0) 7795 400 651

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000



Further information is available via these links:

Twitter: 
@RSComponents     
@alliedelec   
@designsparkRS


RS Components on Linkedin:  
http://www.linkedin.com/company/rs-components


Other Relevant Links:

Electrocomponents plc: 
www.electrocomponents.com

RS Components: 
www.rs-online.com

DesignSpark
www.designspark.com