Press Releases


RS Components announces availability of compact and high-performance industrial Ethernet interface from Hirose

New ix Industrial range sets new standard for robustness, performance and miniaturisation in Ethernet for Industrial Internet of Things applications

London, UK, 16 January 2018:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has announced availability of the ix IndustrialÔ range from Hirose, which sets a higher standard for Ethernet interfaces and responds to future challenges posed by Industry 4.0 and the IIoT (Industrial Internet of Things).

There has been recognition that device interfaces and system cables need to be smaller, more powerful and even more robust. Hirose has developed this new technology to deliver this robust miniature Ethernet interface, which has the potential to replace the conventional RJ45 connection. The units have been designed particularly for use in a variety of fields and applications including security systems, factory automation such as machinery and robotics, communications and data networks, and various transportation applications.

The units take up 70% less space than the standard RJ45 and enable parallel 11mm-pitch mounting, which is ideal for daisy-chaining applications and offers space-saving cabling for applications with miniaturised requirements. The devices are also much safer because the two snap-in metal hooks ensure that the receptacle and connector are more securely connected. Robustness is provided via the use of five through-hole shield contacts, which offer maximum stability on the PCB, increasing locking strength and providing durable cable connection of the plug. The robust structure also supports strong resistance to vibration and shock, enabling 5000 mating cycles.

The range is designed to provide Cat 6A performance for up to 10 Gbps Ethernet data transmission and is standardised to IEC/PAS61076-3-124. Data transmission is safe, even in EMC-critical applications, due to the continuous 360° shield design, which guarantees high immunity from interference.

The Hirose ix Industrial range of Ethernet interface connectors is now shipping from RS in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components and Allied Electronics & Automation are the trading brands of Electrocomponents plc, the global distributor for engineers. We offer more than 500,000 industrial and electronic products, sourced from 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we trade through multiple channels and ship around 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2017 had revenues of £1.51bn.

For more information, please visit the website at www.rs-online.com.

Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com
+44 (0) 7795 400 651

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000



Further information is available via these links:

Twitter: 
@RSComponents     
@alliedelec   
@designsparkRS


RS Components on Linkedin:  
http://www.linkedin.com/company/rs-components


Other Relevant Links:

Electrocomponents plc: 
www.electrocomponents.com

RS Components: 
www.rs-online.com

DesignSpark
www.designspark.com