• Published 21 Nov 2025
    • Last Modified 21 Nov 2025
  • 10 min

Battery Storage For Renewable Energy

Battery storage systems reduce utility costs and protect business performance against electricity blackouts. Discover how they work and the right approach to selecting the right system for your company.

Large battery storage containers beside wind turbines storing renewable energy at a modern wind farm.

Battery energy storage systems allow businesses to store electricity they generate as well as electricity from the Grid. They can then use this to reduce energy bills at peak times. The technology also helps businesses stay operational during power outages.

For companies wanting to deploy battery energy systems, there is a wide range of hardware and software options available. The best solution for businesses is one that matches their energy profile, site setup, and future commercial needs.

In this article, discover the benefits battery energy storage systems deliver. You'll also find out how to choose and implement the right solution for your business. Professor Jacopo Torriti, a Professor of Energy Economics and Policy at the University of Reading, also provides insights into battery use with renewable energy.

What are Battery Storage Systems?

A battery energy storage system is a type of technology that stores electricity for later use. This can be energy from the National Grid or renewable energy you generate yourself.

Benefits of Battery Storage Systems

1. Cost Savings for Commercial Users

Battery storage systems can significantly reduce the cost of energy for businesses. For example, a factory could fully charge its batteries with off-peak electricity or from solar and wind power it generates. It can then use that electricity instead of expensive peak power from the Grid.

Prof. Torriti elaborates, discussing who can best benefit from battery use, as well as how businesses can wisely invest in the energy that makes good use of it:

“When solar panels heat up, they create electricity through inverters, during the day, then the batteries allow you to store anything you're not using during the day. 

For instance, a commercial premises might extend later into the day. They would be carrying on using a bit of the battery from the solar panel used earlier, even if we didn't see much sun that day. But that makes sense if you have activities which are not too energy-intensive and that're spread throughout the day.“

The potential cost savings are significant. Utility companies charge peak rates when many businesses are using the most electricity, typically from 7 am to 7 pm. A report by energy service provider Joulen found that firms with solar and battery storage could achieve a 60% saving by avoiding reliance on peak-rate electricity.

Solar power became increasingly popular with businesses in the 2010s. Adoption surged with the availability of more affordable equipment and installation, as well as government incentives.

Today, battery costs are falling quickly. This makes investing in the technology more affordable, reducing payback periods to between four and eight years. Businesses can shorten that time further by selling excess capacity back to the Grid, creating an additional revenue stream.

A handful of vendors are seeking to remove upfront costs for businesses. Some suppliers will now provide storage systems at no cost with a power purchase agreement (PPA). Firms can expect to reduce energy bills by 50% although they will need to sign a 20-to-30-year agreement with the supplier in order to lease the technology.

2. Business Continuity and Grid Resilience

Although power outages in the UK are relatively rare, they do happen. Many companies already have diesel power generators in place for such incidents. The problem is that, when companies need them, issues such as pre-start preheating and fuel filter clogging can delay startup.

Manufacturers, cold storage warehouses, and data centres need a more reliable fallback. This is where battery storage offers a solution. They can respond to fluctuations in the power supply almost instantly.

They offer other benefits, too. Senior engineering managers benefit from fewer halts in production and greater operational certainty. Maintenance leads find they need less servicing and eliminate fuel storage and handling issues. 

The use of battery power also reduces demand on the Grid, enhancing its stability. In fact, the Grid works with battery storage companies to provide backup in case of failure.

The system works as evidenced in 2019 when two power plants went offline, but in seconds, firms including Upside Energy and Limejump plugged the gap.

Prof. Torriti also explains how batteries can help prevent taking energy from the grid, especially when prices are high:

“Batteries make sense when you have something that is close to a residential user or a commercial use, combined with a solar panel. That's where you have very short paybacks, particularly when electricity prices from the grid are high. You would then get a better return on your money when you invest in this type of technology.”

3. Hitting Corporate and Company Carbon Targets

By generating and storing their own electricity, firms cut their reliance on fossil fuel power. 

Battery storage systems appeal to companies under pressure to cut carbon dioxide emissions. Many procurement leads see this form of sustainable technology as a way to meet Scope 2 emissions targets.

In the UK, batteries contributed to a 4% drop in power sector emissions between January and August 2024. Modo Energy reported that this prevented 950,000 tonnes of carbon emissions during this period.

Prof. Torriti explains that corporations and businesses are turning towards renewable energy like solar more and more nowadays:

“If you're a business and you're going to invest [in a specific type of clean energy], it can be difficult to pick a winner. If you have a business facility, installation, or a plant, and you want to look at the local level to invest in a renewable source for your own energy needs, I’d say solar photovoltaics (PV). 

Their ‘learning curves’, as we call them, their costs have been decreasing immensely, which means that the payback periods, the returns of investment are reducing significantly, and they make more and more sense. 

This is why we see them without the need for any feed-in tariffs, or without the need for any incentives, whether it's from the local government or the government more centrally. 

We see PV visually more and more with businesses. There are space issues, they cover quite a bit, but you're going to basically reduce your bills. You’re going to reduce your bills if, say, during the day you’re using energy and you’re taking energy from PV, especially when you combine it with a battery, that makes even more economic sense.”

Battery storage is expected to become the norm for managing renewable energy and Grid energy in the coming years. Technological advances such as increased power storage capacity and falling prices will accelerate this adoption. 

Perhaps the most important benefit battery storage offers is its potential impact on industry attitudes towards renewable power, transforming what is currently an intermittent source of power into a source of on-demand electricity.

Choosing the Right Battery Storage System

While the benefits of battery energy storage systems are clear, companies should be careful when choosing a solution.

Prof. Torriti discusses the type of battery systems available for renewable energy:

“We're quite limited at the moment, in terms of the type of batteries and the type of storage that can be combined with distributed energy resources or renewables at a local level. There's clearly a range in the market, but the type of batteries that dominate the market and that make economic sense all tend to be lithium-based.”

1. Battery Chemistry

Most systems today are lithium-ion, of which there are two variants:

  • NMC (Nickel Manganese Cobalt): NMC batteries charge and discharge quickly, so they're better if you need high power over a short period
  • LFP (Lithium Iron Phosphate): LFP batteries have a higher cycle life and are safer. They constitute around 60% of UK systems

If you need power for more than six hours, flow batteries are a suitable solution. Unlike lithium-ion batteries, flow batteries discharge over longer periods, meaning they can maintain a steady output over an extended use period.

Prof. Torriti provides more insight into general battery power:

“Lithium batteries have a dispatch time typically around 4 hours, which was true until maybe a couple of years ago. Now, they can dispatch for 6, in some cases 8 hours. But what that means, particularly for commercial purposes or industrial end users, there is a limit. 

There's only so much you can do with a battery that allows you to stock up for 4 to 8 hours. This depends on the industry, but some industrial processes require power ratings which are really high, like furnaces. 

These are typically, mostly not electricity-based, so there's only so much you can store around a certain industrial process.”

Manufacturers are currently developing alternatives like solid-state storage and sodium-ion batteries. They promise higher energy density, longer operating lifespans, and faster charging.

2. System Size and Demand Profile

Companies need a system that will cover Grid outages at peak production time. This provides assurance that production won’t grind to a halt. There are other benefits too, like peak shaving.

Peak shaving is switching to the power in your batteries to replace some or all electricity usage from the Grid. This can result in significant savings during peak hours by reducing your outside energy consumption.

3. Site System Integration

System integration is important because battery storage systems need to work with existing equipment. 

For companies with their own solar PV and/or wind power generators, compatibility is particularly important to make sure that surplus energy can be captured and deployed.

Software also plays a major role. The right energy management system can do a lot more than just balance charging and discharging. For example, it can connect to a building management system to reduce Grid electricity used for heating and cooling. 

For companies with EV chargers on site, the software can smooth out charging demand and save money on peak tariffs.

4. Lifecycle Cost and Efficiency

Upfront cost is an important consideration, but companies need to factor in costs relating to performance and lifespan, as well.

Some batteries deliver more usable energy for every unit you put in. This would be handy for cold store warehouses, for example, which could store electricity to power chillers at peak times. 

Others hold their capacity for longer before they need replacing. This would be useful for businesses such as hotels with spas, laundries, and other facilities because of their daily use and long cycle runs.

Other factors to think about are the warranty and disposal. Companies should consider how many years of reliable use a system will provide them with, as well as how suppliers handle equipment and the end of life, since the UK and EU now require a recycling plan.

Software support is important, too. This is essential to confirming how long a vendor will support a company’s energy management software, as there is a risk that the batteries may outlast the system that controls them. 

Tips for Implementing Your Battery Storage

Before implementing a battery storage system, it’s important to get a clear picture of energy use levels and energy peaks. Involving suppliers as early as possible provides useful guidance on hardware, software, sizing, safety, and connection to the Grid.

Once a system is installed and operational, staff need training on how to use and maintain it. Regular checking will confirm that it’s working as expected. Suppliers can provide additional support if there are performance issues.

Financing a battery storage system also requires careful consideration. Comparing the cost of different systems over their lifetime will give companies a clear picture of the true cost of ownership and likely return on investment.

When considering which businesses would benefit from investing in battery storage for renewable energy, Prof. Torriti explained:

“A combination of battery and solar panels makes sense for a lot of not-too-energy-intensive, commercial use, spread across the day. Whereas when you're dealing with, say, an industrial plant, and I'm taking the example of a furnace, you have intense energy needs for a limited amount of time. Those kinds of batteries are not going to help you a lot.”

Professor Jacopo Toritti

Professor Jacopo Torriti is a Professor of Energy Economics and Policy at the University of Reading. He is the Flexibility Theme Lead of the Energy Demand Research Centre (EDRC), serves as a member of the Panel of Technical Experts of the Department for Energy Security and Net Zero, DSO Performance panel, and the Strategic Advisory Team on Energy and Decarbonisation for the Engineering and Physical Sciences Research Council (EPSRC).

Prof. Torriti has authored several books, including ‘Appraising the Economics of Smart Meters’ (2020), ‘Energy Fables’ (2019), and ‘Peak Energy Demand and Demand Side Response’ (2015).

Related Articles

Related links