Recently searched
      • Published 17 Jan 2023
      • Last Modified 25 Jan 2024
    • 7 min

    A Complete Guide to Zener Diodes

    Our guide is designed to help you understand what Zener diodes are, their characteristics, and how they work.

    What is a Zener Diode?

    Zener diodes are silicone-based discrete semiconductor devices which allow current to flow bidirectionally - either reverse or forward. Diodes are comprised of a heavily-doped P-N silicone junction, which is intended to conduct in the reverse direction once a particular voltage threshold has been met.

    Zener diodes have a set reverse breakdown voltage. When this is reached, they start to conduct current and continue to operate unceasingly in the reverse bias direction without incurring damage. One of the main benefits of Zener diodes is that a varying range of voltages will still maintain a constant voltage drop across the diode. As a result, Zener diodes can be used for voltage regulation applications.

    Zener Diode Characteristics

    Zener Diodes

    Zener diodes operate similarly to conventional diodes when in the forward-bias mode. They have a bias turn-on voltage of between 0.3 and 0.7V. When connected in the reverse mode, there is a small leakage current flow in most applications. As the reverse voltage increases to the set breakdown voltage, there will be current flowing through the diode. When the current increases to a maximum (determined by the resistors in series), it will then stabilise and remain constant over a wide range of applied voltage.

    Irrespective of the current value flowing through the diode, the voltage remains almost constant. This is also the case with large current changes, providing that the diode current stays between the maximum current and the breakdown current.

    A Zener diode’s strong self-control is highly useful when it comes to regulating and stabilising variations in load or supply against a voltage source. This makes it a key characteristic as it enables the diode to be used in a variety of voltage regulator applications.

    Zener Diode Specifications

    Some specifications will vary between individual Zener diodes. These include power dissipation, nominal working voltage, and maximum reverse current. Additional commonplace specifications include:

    • Zener Voltage – this relates to the reverse breakdown voltage. This ranges from 2.4V up to 200V, depending on the specific diode
    • Current (maximum) – the maximum current at the rated Zener voltage. This can range from 200uA to 200A
    • Current (minimum) - the minimum current required at the Zener voltage for the diode to break down. This is typically between 5mA and 10mA
    • Power Rating – the maximum power dissipation rating of the diode, including both the current flowing through the diode and the voltage across it. Standard values include 400mW, 500mW, 1W, and 5W. With surface-mounted diodes, typical values are 200mW, 350mW, 500mW, and 1W
    • Voltage Tolerance – typically ±5%
    • Temperature Stability – the most stable diodes are usually approximately 5V
    • Zener Resistance – the resistance exhibited by the diode

    Zener Diode Applications

    Zener diodes are used for a range of applications, including:

    • Voltage regulation
    • Voltage reference
    • Surge suppression
    • Switching applications
    • Clipper circuits

    It is possible to use a Zener diode to create a stabilised low-ripple output voltage under variable load current conditions. When a suitable current limiting resistor is used to pass a minor current from a voltage source through the diode, sufficient current will be conducted to maintain the required voltage drop. As the load value is altered, the average voltage output also changes. However, the addition of a Zener diode can produce an even voltage output.

    With that being said, it should also be noted that Zener diodes may occasionally produce electrical noise on the DC supply as they work to steady the voltage. This is fine in the majority of applications, but adding a high value decoupling capacitor to the output of the diode can rectify the problem by providing extra smoothing.

    As Zener diodes can operate in the reverse bias condition, they can be used in voltage regulator circuits to sustain constant DC voltage output. This constant voltage can be maintained despite any variations in voltage input or load current changes.

    This voltage regulator circuit comprises a current limiting resistor which is connected in series with the input voltage. The diode and the load should then be connected in parallel. The stabilised voltage output and the diode’s breakdown voltage will always be the same.

    Idea Lightbulb

    Zener Diode Uses and Working Applications

    Zener diodes are also used in modern applications such as smartphones and Android devices. Many such uses involve Bluetooth technology. On average, a standard Bluetooth device needs around 3V for operation. In this application, a Zener diode would be used to provide the required 3V to the Bluetooth-enabled device.

    How Does a Zener Diode Work?

    The principle behind the operation of a Zener diode is determined by the cause of the diode’s breakdown in the reverse bias condition. There are typically two types – Zener and avalanche.

    Zener Breakdown

    A Zener breakdown happens with a reverse bias voltage between 2V and 8V. The intensity of the electric field is enough to apply force to the valence electrons, separating them from the nuclei – even at this low voltage. This process forms mobile electron-hole pairs, therefore increasing current flow.

    Zener breakdowns typically occur for highly-doped diodes with a large electric field and low breakdown voltage. More energy is gained by the valence electrons as temperature increases, therefore requiring less outward voltage. This also means that Zener breakdown voltage reduces alongside temperature.

    Avalanche Breakdown

    Voltage breakdown also happens in the reverse bias condition, at a minimum of 8V, for light-doped diodes that have a large breakdown voltage. Electrons flowing through the diode collide with electrons in the covalent bond, disrupting it. The velocity of the electrons increases as the voltage also increases, meaning that the covalent bonds can be disrupted more easily. It should also be noted that avalanche breakdown voltage rises alongside temperature.

    What is the Zener Diode Symbol?

    The images portray the standard Zener diode symbol used within a circuit diagram.

    This symbol shows how the presence of a Zener diode would be noted in a circuit diagram. Similarly, if you see this symbol in a circuit diagram, it means that a Zener diode is present at that point in the circuit.

    This diagram then builds on the above, showing more information about the Zener diode. The top line of the diagram shows the diode symbol plus the positive and negative as it relates to the anode and cathode. The bottom line of the diagram shows the same, except with a simplified version of a realistic diode as opposed to the Zener diode symbol.

    FAQs

    Can You Connect Multiple Zener Diodes in Series?

    It is possible to connect multiple Zener diodes in series and this is usually done to achieve a particular Zener voltage. However, if you are using multiple diodes, you must also monitor the Zener current and ensure the maximum is not exceeded. This is because the maximum allowable Zener current becomes equal to the lowest diode connected in the series. This also means that in a scenario where two Zener diodes are connected in series, one will not exhibit the stated Zener current or voltage if the diodes do not have the same Zener current specifications.

    What is the Difference Between a Zener Diode vs a Diode?

    A diode is a semiconductor device which conducts in a single direction (unidirectional). Zener diodes are also semiconductor devices, but the key difference is that they conduct in both a forward and reverse bias condition. Another important difference between the two types is doping intensity. Conventional diodes are typically moderately doped, whereas Zener diodes are doped more highly to enable sharper breakdown voltage.

    Related Guides

    Related links