RS Components

0£0.00
The next generation of Raspberry Pi is here with the Raspberry Pi4, available from RS Components in the 2GB and 4GB versions. This is the most powerful Pi board to date and is now a complete desktop computer; it can power 2 independent 4K screens simultaneously, and has 3 times the processing power and 4 times the multimedia performance of its predecessors allowing users to surf, stream films, edit images and even create apps in ultra high definition.

New Raspberry Pi4 Model

Processor Broadcom BCM2711, quad-core Cortex-A72 (ARM v8) 64-bit SoC @1.5GHz
Memory 2GB and 4GB models (1GB model available at okdo.com)
Connectivity 2.4 GHz and 5.0 GHz IEEE 802.11b/g/n/ac wireless LAN, Bluetooth 5.0, BLE. Gigabit Ethernet, 2 x USB 3.0 ports and 2 x USB 2.0 ports
Access Standard 40-pin GPIO (backwards-compatible)
Video and Sound 2 xmirco HDMI ports (up to 4Kp60 supported)2-lane MIPI DSI Display port2-lane MIPI CSI camera port4-pole stereo audio and composite video port
Multimedia H.265 (4Kp60 decode), H.264 (1080p60 decode, 1080p30 encode), OpenGL ES, 3.0 graphics
We now have stock for both the Raspberry Pi 4 4GB and the 2GB. If you are purchasing for personal use, please visit one our approved resellers or okdo.com (owned by Electrocomponents Group).

Check out RS's authorised resellers and Okdo (owned by Electrocomponents Group), for personal use only

OKdo is a unique global tech company owned by Electrocomponents Group. Solely focusing on SBC and IoT, OKdo works with some of the best technology companies on the planet to bring people the latest products, innovations and services, wherever they are on their SBC and IoT journey.

The below companies are selected by RS Components as authorised resellers for Raspberry Pi products. Consumer customers, without VAT numbers, are requested to purchase via the below listed resellers.

We remind you that once following the links below, your order will be managed by the reseller autonomously and independently from RS.

RS has no responsibility for any dealings you may have with these resellers, and any purchase you make will be governed by the terms and conditions of sale of the relevent reseller.

Accessories for Raspberry Pi4 Model

Raspberry Pi 3 Model B+

Processor Broadcom BCM2837B0, Cortex-A53 64-Bit SoC @ 1.4GHz
Memory 1GB LPDDR2 SDRAM
Connectivity 2.4GHz and 5GHz IEEE 802.11.b/g/n/ac wireless LAN, Bluetooth 4.2, BLE Gigabit Ethernet over USB 2.0 (maximum throughput 300Mbps) 4 × USB 2.0 ports
Access Extended 40-pin GPIO header
Video and Sound 1 × full size HDMI MIPI DSI display port MIPI CSI camera port 4 pole stereo output and composite video port
Multimedia H.264, MPEG-4 decode (1080p30); H.264 encode (1080p30); OpenGL ES 1.1, 2.0 graphics

Raspberry Pi 3 Model B+ and Accessories

Setting up your new Raspberry Pi 3 Model B+ is as easy as Pi...

Once you’ve received your new Raspberry Pi it’s easy to connect it up and get started. Watch Pete Wood, from DesignSpark, show you how to connect your board up and start running NOOBS, the new out-of-the-box software from the Raspberry Pi Foundation.