Press Releases
RS Components introduces series of leading-edge cordless battery-powered torque tools from Norbar
Available from RS, the new EvoTorque Battery Tool (EBT) is perfect for safety critical and heavy industrial applications where traceability is paramount.
London, UK, 27 September 2019:

The EvoTorque® Battery Tool (EBT) series has been specifically designed to deliver improved performance and data traceability in safety-critical and heavy industrial operations. Equipped with a high-powered and maintenance-free brushless motor, the series is ideal for applications where mains-supplied electric or pneumatic power is unavailable, or in environments where the presence of cables may constitute a safety risk.
In addition to outstanding performance, it also offers excellent thermal durability
minimising any overheating problems, which can commonly occur with battery-operated tools. For many applications, the number of tightening cycles performed by a hand tool before it overheats is more critical specification than the number of cycles provided by the battery.
A key feature of the EBT is its transducer control, rather than being current controlled, which enables it to deliver a precise torque to within an accuracy of ±3%. In addition, the EBT units integrate the maker’s ‘intelligent joint sensing’ technology, which continually measures the joint being tightened and will use dynamic braking to avoid torque over-shoot.
Two-way communication with the EBT is available either wirelessly via Bluetooth or via USB cable: as well as being able to download up to 3000 time/date-stamped readings or even stream live data from the tool, users can also upload information such as tightening sequences. In addition, all the tools come with a free copy of Norbar’s EvoLog PC software to manage the data; alternatively, data can also be output in CSV format. Importantly, and especially for safety critical applications in fields such as railway infrastructure, the tool can also be used with mobile phones and tablets, thereby enabling the recording of torque tightening data that is linked to GPS coordinates.
The EBT cordless torque tool family offers three torque ranges with maximum outputs of 1350, 2700 and 4000Nm, with a single- and a two-speed device in each torque class. All the tools come in a hard case with two batteries and a three-bay rapid charger, which can fully charge cold batteries in 45 minutes. Accessories such as right-angle and offset gearboxes for bolts where there is limited headroom, for example, will soon be available from RS.
The EBT series is available to purchase from RS from 1 October in the UK and Ireland.
-Ends-
About RS Components
RS Components is a trading brand of Electrocomponents plc. We offer more than 500,000 industrial and electronic products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.
We support customers across the product life cycle, whether via innovation and technical support at the design phase, improving time to market and productivity at the build phase, or reducing purchasing costs and optimising inventory in the maintenance phase. We offer our customers tailored product and service propositions that are essential for the successful operation of their businesses and help them save time and money.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2019 reported revenue of £1.88 billion. Electrocomponents has seven operating brands: RS Components, Allied Electronics & Automation, RS PRO, OKdo, DesignSpark, IESA and Monition.
For more information, please visit the website at https://uk.rs-online.com/web/.
Editorial Contact:
Aakriti Kaushik
PR Manager – Northern Europe
RS Components
aakriti.kaushik@rs-components.com
PR Agency Contact:
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0) 1225 470000
Further information is available via these links:
Twitter: @RSComponents; @designsparkRS
Linkedin: www.linkedin.com/company/rs-components
RS Components
www.rs-online.com
DesignSpark
www.rs-online.com/designspark
Electrocomponents plc
www.electrocomponents.com