Press Releases


RS Components launches low-cost, high-performance IR temperature sensor to fit in small spaces

Compact unit features integrated measurement display and parameter controls

London, UK, 24 September 2019:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel provider of industrial and electronic products and solutions, has introduced the RS PRO infrared temperature sensor, a low-cost non-contact voltage-output temperature sensor designed for factory maintenance, repair and operations (MRO) in smart manufacturing environments.

Maintenance engineers often ask RS for a small, low-cost temperature sensor that can fit into tight spaces, and that shows the measured temperature in situ, so they do not have to return to the control room to check it. The new RS PRO infrared temperature sensor is designed to meet these requirements. It is extremely small — just 30mm deep x 31mm in diameter — with a side-entry cable making it easy to mount in small spaces. It shows the temperature on a built-in backlit OLED display, without the need for contact with the target surface. The sensor is ideal for situations where contact probes cannot be used, such as when the target is moving or inaccessible; for example, it will fit between a wheel and the rim or hub of a disc brake.

The RS PRO infrared temperature sensor can measure surface temperatures from 0°C to 1000°C to an accuracy of ±1.5% of reading or ±1.5°C, whichever is greater, and repeatability of ±0.5% of reading or ±0.5°C. Its response time is just 250ms, allowing continuous monitoring by industrial process instrumentation via the DC voltage output.

The sensor provides simultaneous voltage and alarm outputs. The voltage output can be configured as 0–5VDC, 1–5VDC or 0–10VDC, with adjustable temperature range scaling, configured using built-in controls on the sensor. The open-collector alarm output offers adjustable temperature threshold and hysteresis.

As supplied, the sensor is set up to measure non-reflective surfaces such as paper, plastics, rubber, wood, tarmac, food, pharmaceuticals, organic materials and painted metal. To measure the temperature of reflective solid or liquid surfaces, the user can adjust emissivity settings between 0.20 and 1.00.

The RS PRO infrared temperature sensor is fitted as standard with a 1m long cable, which can be extended using terminal blocks or connectors. An optional air purge collar is available to help keep the lens clean in the presence of smoke, fumes, dust, steam or other potential contaminants.

Shipping now in the EMEA and Asia Pacific regions, the device is IP65 rated, offers highly competitive pricing and comes with the RS PRO Seal of Approval, which means it has been rigorously tested to meet demanding industry standards.

-Ends-

About RS Components

RS Components is a trading brand of Electrocomponents plc. We offer more than 500,000 industrial and electronic products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

We support customers across the product life cycle, whether via innovation and technical support at the design phase, improving time to market and productivity at the build phase, or reducing purchasing costs and optimising inventory in the maintenance phase. We offer our customers tailored product and service propositions that are essential for the successful operation of their businesses and help them save time and money.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2019 reported revenue of £1.88 billion. Electrocomponents has seven operating brands: RS Components, Allied Electronics & Automation, RS PRO, OKdo, DesignSpark, IESA and Monition.

For more information, please visit the website at https://uk.rs-online.com/web/

Editorial Contact:
Aakriti Kaushik
PR Manager – Northern Europe
RS Components
aakriti.kaushik@rs-components.com

PR Agency Contact:
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0) 1225 470000



Further information is available via these links:

Twitter: @RSComponents; @designsparkRS

Linkedin: www.linkedin.com/company/rs-components

RS Components

www.rs-online.com

DesignSpark

www.rs-online.com/designspark

Electrocomponents plc

www.electrocomponents.com