Press Releases


RS Components launches its first RS PRO digital multimeter with built-in thermal imaging

Compact yet versatile DMM identifies thermal overloads from a safe distance

London, UK, 8 August 2019:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel provider of industrial and electronic products and solutions, has introduced the first digital multimeter (DMM) in its RS PRO product range to feature a built-in thermal imager. The RS-9889 thermal imaging multimeter allows engineers to identify thermal overload issues in electrical equipment from a safe distance, without the need for any physical contact.

The RS-9889 thermal imaging DMM is an all-in-one handheld device designed, like other products in the RS PRO range, to combine durability and reliability with excellent value for money. It is suitable for a wide variety of applications, ranging from smart manufacturing in the industrial automation sector, to general electrical tasks such as testing sockets and lighting during business safety audits and home renovations.

The RS-9889 combines features of a digital multimeter — measuring circuit parameters such as voltages, currents and resistances — with an infrared thermal imaging camera to allow hot and cool points in electrical components to be identified on a viewable thermogram.

The thermal imager of the RS-9889 offers max, min and centre crosshair targeting to help the user identify and measure required temperature ranges easily. A Bluetooth Low Energy (BLE) connection allows thermal images to be shared quickly to other devices via the Thermview+ app. The thermal imager has a 2.8-inch colour TFT LCD screen with an infrared resolution of 80 x 80 pixels, a 21° x 21° field of view, thermal sensitivity (NETD or noise equivalent temperature difference) to less than 0.1°C/100mK, a fast 50 Hz thermal image frame rate, an object temperature range from 20° to 260°C, a spectral range of 8–14 μm, and accuracy to within ±2°C, or ±2% of the reading.

The versatile RS-9889 include also functions as a diode, resistance and continuity tester, equipped with a buzzer, and can measure temperatures all the way up to 1000°C using a K-type thermocouple probe. AC and AC+DC voltage and current are true RMS.

A lightweight portable device allowing users to work on the go, the RS-9889 measures just 80 x 58 x 195mm and weighs 540g. It is shipping now from RS in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components is a trading brand of Electrocomponents plc. We offer more than 500,000 industrial and electronic products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

We support customers across the product life cycle, whether via innovation and technical support at the design phase, improving time to market and productivity at the build phase, or reducing purchasing costs and optimising inventory in the maintenance phase. We offer our customers tailored product and service propositions that are essential for the successful operation of their businesses and help them save time and money.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2019 reported revenue of £1.88 billion. Electrocomponents has seven operating brands: RS Components, Allied Electronics & Automation, RS PRO, OKdo, DesignSpark, IESA and Monition.

For more information, please visit the website at https://uk.rs-online.com/web/

Editorial Contact:
Aakriti Kaushik
PR Manager – Northern Europe
RS Components
aakriti.kaushik@rs-components.com

PR Agency Contact:
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0) 1225 470000



Further information is available via these links:

Twitter: @RSComponents; @designsparkRS

Linkedin: www.linkedin.com/company/rs-components

RS Components

www.rs-online.com

DesignSpark

www.rs-online.com/designspark

Electrocomponents plc

www.electrocomponents.com