Press Releases


RS Components introduces professional-grade pocket-size thermal imager from Fluke

Ideal for maintenance teams, new PTi120 thermal camera delivers fast inspection capabilities to help maintain industrial equipment uptime

London, UK, 6 August 2019:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel provider of industrial and electronic products and solutions, has announced availability of the latest thermal imaging device from Fluke, a world leading maker of electronic test tools and software for professionals. The new and highly innovative PTi120 is the manufacturer’s first pocket-sized unit and targets troubleshooting and predictive maintenance applications for a wide range of industrial market sectors.

Targeting maintenance engineers especially, the pocket-sized thermal camera can be carried around easily. It enables maintenance teams to carry out enhanced infrared inspections and make quick temperature scans of electrical equipment, machinery, or specific pumps and motors, thereby helping in the effort to minimise equipment downtime.

A key feature of the fully radiometric unit is its 3.5-inch LCD touchscreen, together with its IR fusion ability, which enables the automatic and simultaneous capture of a digital visible-light image along with an infrared image. Users can blend the resulting image from full infrared to full visible light by simply sliding their finger across the screen, enabling the fast location of problem areas. Delivering measurement data right down to the pixel level, the unit offers a 120 x 90-pixel infrared resolution for a total of 10,800 pixels.

In addition, the PTi120 imager is a highly rugged device that comes in an IP54-rated enclosure, enabling it to resist dirt and water ingress, and withstand being dropped from a height of up to 1m. Other key specifications include: field of view of 50°(H) x 38°(V); a temperature measurement range from –20 to +150°C, with an accuracy of +/–2°C; and battery life of more than two hours.

When used in conjunction with Fluke’s Connect Desktop software and its ‘Asset Tagging’ capability, users can also scan an asset’s barcode or QR code, which enables the storing of a captured IR image along with date/time information to predefined folders. This data can be sent via WiFi or USB.

Shipping now from RS in the EMEA and Asia Pacific regions, the Fluke PTi120 comes with a two-year warranty as standard, as well as a USB cable for charging and data transfer, and a soft transport bag and an adjustable lanyard. The Fluke Connect Desktop software and user manual are available free via download.

-Ends-

About RS Components

RS Components is a trading brand of Electrocomponents plc, a global multi-channel provider of industrial and electronic products and solutions. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2019 had revenues of £1.88bn.

For more information, please visit the website at https://uk.rs-online.com/web/


Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000

Further information is available via these links:

Twitter: @RSComponents; @designsparkRS

Linkedin: www.linkedin.com/company/rs-components

RS Components

www.rs-online.com

DesignSpark

www.rs-online.com/designspark

Electrocomponents plc

www.electrocomponents.com