Press Releases


RS Components introduces new space-saving and high-speed industrial connector series from Hirose

Compact and rugged I/O connectors deliver potential to reduce space of installations by up to 75% compared to RJ45 based solutions

London, UK, 6 June 2019:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel provider of industrial and electronic products and solutions, has introduced a highly robust series of connectors for industrial applications. Manufactured by Hirose Electric, a global leader in high-quality connectors, the ix Industrial™ series meets all the requirements for space-constrained applications and can support I/O signal transmission speeds of up to 10 Gigabits per second.

The ix Industrial™ series is suitable for a range of industrial applications including factory automation controllers, industrial robotics, servo amplifiers, PLCs and many others such as security systems. In addition to delivering the potential to reduce installation space by up to 75% compared to RJ45 based solutions, the new Hirose series supports CAT5e (1-Gbps) and CAT6A (10-Gbps) cabling and features an optimised rugged and reliable EMI and ESD shielding design.

Other features of the series include availability with two keying codes for Ethernet and non-Ethernet applications and compliance with the IEC PAS 61076-3-124 standard. Electrical characteristics include: a current rating of 1.5A for all 10 contacts, with 3A capability on pins 1, 2, 6 and 7; voltage rating of 50V; 5000 mating cycles; and an operating temperature of from –40 up to +85°C.

The connector receptacle can be mounted in parallel with a pitch distance of only 10mm, which enables close side-by-side positioning of multiple connectors on a single PCB. The receptacle shell is PCB mounted via through-hole solder legs to enhance PCB retention, and the wire-termination unit and cable clamp are integrated into a single plug shell. Additionally, the snap-in I/O plug connector offers a positive metal lock, which provides a clear tactile click to ensure secure mating.

The Hirose ix Industrial connector series is now shipping from RS in the EMEA region.

-Ends-

About RS Components

RS Components is a trading brand of Electrocomponents plc, a global multi-channel provider of industrial and electronic products and solutions. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2019 had revenues of £1.88bn.

For more information, please visit the website at https://uk.rs-online.com/web/


Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000

Further information is available via these links:

Twitter: @RSComponents; @designsparkRS

Linkedin: www.linkedin.com/company/rs-components

RS Components

www.rs-online.com

DesignSpark

www.rs-online.com/designspark

Electrocomponents plc

www.electrocomponents.com