Press Releases


RS Components introduces new series of power supplies approved for use in medical markets

TRACO Power brand embedded switch-mode supplies deliver double insulation with wide selection of power ratings and package options

London, UK, 21 March 2019:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel provider of industrial and electronic products and solutions, has announced availability of of 11 new series of power supplies from TRACO Power that meet the demands of high-growth medical markets.

These embedded switch-mode power supplies feature a reinforced double I/O isolation system, according to the IEC/EN/ES 60601-1 third-edition medical safety standards, including 2 x MOPP (Means of Patient Protection) approval for operating altitudes up to 5000m. In addition, the units’ earth leakage current is less than 100μA, making them suitable for BF (body floating) class insulation applications. The units also operate in compliance with the medical EMC emission and immunity levels, according to latest standard IEC60601-1-2 fourth edition, and risk management for medical devices, according to ISO14971.

The TRACO Power units offer a very wide range of power ratings, including 13.2/15W (TPP15A-J, TPP15-J, TPP15A-D and TPP15-D series), 20/30W
(TPP30A-J, TTP30-J, TPP30A-D and TPP30-D), 40W (TPP40/A), 65W (TPP65/A), 100W (TPP100/A), 150W (TPP150/A) and 450W (TPP450/A).

Key electrical features of the supplies include: a wide range of voltage outputs – from 3.3V DC up to 48V DC for the 20W to 40W units, and from 12V DC up to 48V DC for the higher rated units; plus high power efficiencies ranging up to a maximum of 91.5% for the 30W TPP 30-J series, for example, which also delivers a high power density from a small-footprint package measuring only 1.5 x 3.95 inches.

Other features include: full load operating temperature range covering –40 to +60°C with the ability to handle temperatures up to +85°C with 50% load derating; universal AC input from 85 to 264V AC; enclosure options including open frame, encapsulated or metal enclosed packages, depending on the supply’s power rating; and a five-year warranty.

The TRACO Power supplies for medical applications are shipping from RS in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components, Allied Electronics & Automation, IESA and Monition are the trading brands of Electrocomponents plc, a global multi-channel provider of industrial and electronic products and solutions. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2018 had revenues of £1.71bn.

For more information, please visit the website at https://uk.rs-online.com/web/.


Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000

Further information is available via these links:

Twitter: @RSComponents; @designsparkRS

Linkedin: www.linkedin.com/company/rs-components

RS Components

www.rs-online.com

DesignSpark

www.rs-online.com/designspark

Electrocomponents plc

www.electrocomponents.com