Press Releases


RS Components introduces new version of robust interconnectivity series from HARTING for control panels and other demanding industrial applications

New Han-Eco® B series of hoods and housings delivers rear-side assembly and enables fast and easy assembly and significant reduction of system downtime

London, UK, 7 March 2019:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel provider of industrial and electronic products and solutions, has announced it is shipping a new interconnectivity series from HARTING suitable for use in a range of industries and applications, including rail and transportation, and automation and robotics in plant machinery.

The new Han-Eco® B series of connector hoods and housings is a major addition to the manufacturer’s Han-Eco® portfolio. The Eco B series available from RS has more than 100 robust devices that offer excellent resistance in demanding industrial environments, as well as integrating HARTING’s Han-Eco ‘click and mate’ snap-in functionality for fast and easy assembly.

The series offers sizes from 6B to 24B, and a range of designs including bulkhead-mount, surface-mount and cable-to-cable types, as well as versions suitable for outdoor use. Devices also feature a high-performance plastic construction that meets the EN 45545-2 and IEC 61948 standards, as well as offering IP65 protection and significant savings in weight compared to traditional metal housings.

A significant benefit offered by the series is rear-side assembly, which can lead to major time saving, especially in control panel applications. It provides companies with the ability to change the configuration of connections quickly and efficiently, significantly reducing downtime. Use of the series means that technicians do not have to install cables through the bulkhead-mounted housing before assembling the contact inserts. The series enables pre-assembled rear-mount inserts to be directly snapped into the housing, thereby greatly simplifying assembly of control cabinets. This approach also enables flexibility to separately pre-assemble cabinet units and cable harnesses.

The Han-Eco B series already offers 44 different versions of the bulkhead mounting housing, which allows insertion of monobloc or modular inserts. It also offers mating compatibility with metal hoods and housings, such as devices from HARTING’s Han B series.

The HARTING Han-Eco B series is now shipping in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components, Allied Electronics & Automation, IESA and Monition are the trading brands of Electrocomponents plc, a global multi-channel provider of industrial and electronic products and solutions. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2018 had revenues of £1.71bn.

For more information, please visit the website at https://uk.rs-online.com/web/.


Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000

Further information is available via these links:

Twitter: @RSComponents; @designsparkRS

Linkedin: www.linkedin.com/company/rs-components

RS Components

www.rs-online.com

DesignSpark

www.rs-online.com/designspark

Electrocomponents plc

www.electrocomponents.com