Press Releases
Low-cost IoT prototyping kits from Cypress now shipping from RS Components
Offering flexible platforms with Wi-Fi, Bluetooth and BLE connectivity and PSoC® 6 MCUs for IoT development
London, UK, 7 February 2019:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel provider of industrial and electronic products and solutions, has announced availability of two new PSoC® 6 prototyping kits from Cypress Semiconductor Corp.: the first for Wi-Fi and Bluetooth IoT development and the second for BLE (Bluetooth Low Energy) based IoT applications.
Along with advanced connectivity, the two kits offer a low-cost hardware development platform that enables designs based around the ultra-low-power dual-core-architecture Cypress PSoC 6 microcontroller. The PSoC 6 MCU integrates built-in security, up to 2MB of flash memory and 1MB of SRAM, together with an Arm® Cortex® M4 for high-performance tasks and a Cortex®-M0+ for low-power tasks, all on a single chip.
The PSoC 6 Wi-Fi-/BT prototyping kit combines the PSoC 6 MCU with industry-leading connectivity via an on-board module hosting the Cypress CYW4343W combo chipset, which provides 802.11b/g/n Wi-Fi and dual-mode Bluetooth 4.1 connectivity. The kit provides a snap-away form factor, giving developers flexibility to use different peripherals to design and prototype IoT applications. It also offers Cypress’ industry-leading CapSense® capacitive touch sensing technology, as well as a 512MB Quad-SPI NOR flash device, a MicroSD card slot, and a Digilent Pmod™ interface.
The second offering is the PSoC 6 BLE prototyping kit, which provides the CYBLE-416045-02 EZ-BLE™ Creator Module (based on the PSoC 63 MCU). This module is fully certified for Bluetooth 5.0 and provides a programmable turnkey solution for developers to add Bluetooth connectivity to IoT designs. It comes with a royalty-free BLE stack and provides 36 GPIOs in a 14 x 18.5 x 2.00mm package.
The kit is also designed with a snap-away form-factor, which allows the separation of the on-board programmer and debugger (KitProg2) from the target board. It also provides a mikroBUS™ interface allowing interfacing of the MCU with any of MikroElektronika’s 500+ click boards.
Both kits are shipping now from RS in the EMEA and Asia Pacific regions.
-Ends-
About RS Components
RS Components, Allied Electronics & Automation and IESA Ltd are the trading brands of Electrocomponents plc, a global multi-channel distributor. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2018 had revenues of £1.71bn.
For more information, please visit the website at https://uk.rs-online.com
Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com
PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000
Further information is available via these links:
Twitter: @RSComponents; @designsparkRS
Linkedin: www.linkedin.com/company/rs-components
RS Components
www.rs-online.com
DesignSpark
www.rs-online.com/designspark
Electrocomponents plc
www.electrocomponents.com