Press Releases


RS Components adds new high-voltage bidirectional buck-boost controller board from Renesas Electronics

Board enables engineers to evaluate capabilities of Renesas’ new buck-boost controller IC for range of power system applications

London, UK, 10 January 2019:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel distributor, is now shipping a new board that has been designed for the evaluation of Renesas Electronics’ recently launched ISL81601 bidirectional buck-boost controller IC.

The ISL81601EVAL1Z evaluation board integrates the ISL81601, which is a true bidirectional four-switch 60V high-voltage synchronous buck-boost controller. Employing the silicon vendor’s proprietary buck-boost algorithms, the chip offers peak and average current sensing and monitoring in either buck or boost mode. It can ensure high reliability for end equipment by providing cycle-by-cycle current limiting in fast transient conditions – in both directions and at either the line or load end.

Other capabilities of the ISL81601 include external soft-start, independent enable functions, and a wide series of protection features, including under-voltage, over-voltage/current and over-temperature. The IC also delivers peak efficiency of up to 99% for point-of-load (POL) and voltage rail conversion; a gate driver that delivers up to 20A for the buck-boost output; and programmable switching frequency ranging from 100 to 600kHz, which aids optimisation of inductor size.

The evaluation board offers a very wide input range – from 9V to 60V – and both the board and the IC are suitable for a wide selection of applications such as battery backup, USB Type-C power supplies and chargers, and redundant power supplies.

In addition, due to the chip’s wide input-voltage range, it is expected to be commonly used in telecommunications applications, battery-powered industrial equipment and in the automotive aftermarket, as well as other applications in medical equipment, robots and drones, and security surveillance markets.

The ISL81601EVAL1Z evaluation board from Renesas is shipping now in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components, Allied Electronics & Automation and IESA Ltd are the trading brands of Electrocomponents plc, a global multi-channel distributor. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2018 had revenues of £1.71bn.

For more information, please visit the website at https://uk.rs-online.com

Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000

Further information is available via these links:

Twitter: @RSComponents; @designsparkRS

Linkedin: www.linkedin.com/company/rs-components

RS Components

www.rs-online.com

DesignSpark

www.rs-online.com/designspark

Electrocomponents plc

www.electrocomponents.com