Press Releases


RS Components introduces high-end RS Pro dual-channel soldering station

Robust soldering tool offers simultaneous operation of iron and tweezer tools, delivering professional capabilities at a highly attactive price point

London, UK, 13 December 2018:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel distributor, has launched the RS Pro dual-channel smart soldering station for use by a wide range of engineering professionals. Now shipping at a highly competitive price of £599.95, it is the first product in the RS Pro range to offer a high-end, two-channel specification.

“This dual-channel soldering tool is a significant addition to the RS Pro range,” said Simon Brown, VP RS Pro. “Its combination of power, flexibility and functionality is simply not available elsewhere at this price level, thereby delivering access to professional soldering capability for a larger range of potential users.”

Offering a combined maximum power output of 200W, a key feature of the soldering station is that it enables the simultaneous use of a soldering iron and tweezers, which are both included in the package along with the main heating unit and two tool holders. The station is a heavy-duty and highly robust unit and the tool holders feature inserts made from metal for placement of the soldering iron and tweezers.

With fast heat-up and recovery, the supplied soldering iron has a power output of 130W and can reach maximum temperature within 10 seconds. The 100W output tweezers feature a soldering and desoldering function, suitable for use with a range of surface-mount devices. In addition, the maximum power output of 150W for a single-channel soldering iron means the product can handle the soldering of large bond pads.

Another key feature of the station is the automatic recognition of the connected soldering tools and the uploading of corresponding parameter data, which is displayed on the main unit’s large digital LCD screen. In addition, the station features a temperature range from 150 up to 480°C and comes with three pre-set temperature operations to support simplified operation, as well as offering energy-saving modes, including standby and auto-sleep.

In addition to the main heating unit, the two tool holders and iron and tweezers, the package includes cleaning sponges, UK and European plugs, and manuals. A range of replacement accessories will also soon be available from RS, including soldering irons in 50W, 130W and 150W variants, together with tweezers and tips.

Shipping now, the RS Pro soldering station has been rigorously tested to meet demanding industry standards and comes with a three-year warranty and the RS Pro Seal of Approval.

-Ends-

About RS Components

RS Components, Allied Electronics & Automation and IESA Ltd are the trading brands of Electrocomponents plc, a global multi-channel distributor. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2018 had revenues of £1.71bn.

For more information, please visit the website at https://uk.rs-online.com

Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000

Further information is available via these links:

Twitter: @RSComponents; @designsparkRS

Linkedin: www.linkedin.com/company/rs-components

RS Components

www.rs-online.com

DesignSpark

www.rs-online.com/designspark

Electrocomponents plc

www.electrocomponents.com