Press Releases


RS Components stocks graphic display controllers for development of HMI applications

Bridgetek’s EVE series of embedded video engine ICs delivers reduced system BOM cost for industrial touchscreens

London, UK, 22 November 2018:

RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), a global multi-channel distributor, has introduced two new graphic display controller ICs from Bridgetek that target the development of next-generation graphics displays for human machine interface (HMI) applications.

The BT815/816 controllers are the third generation of embedded video engine (EVE) devices. Delivering support for display, audio and touch capabilities, they enable engineers to quickly and efficiently design high-resolution displays and robust HMI solutions with a lower bill-of-material cost.

The innovative architecture used in the BT815/816 series can support adding display capabilities to a wide range of 8-, 16-, or 32-bit enabled MCU systems, over a simple SPI interface. Making use of an object-oriented approach to develop the final displayed image which is rendered line by line the EVE solution facilitates rapid development of static and animated displays with full touch control and no expensive frame-grabbing memory on the bill of materials.

New with the BT815/816 series is the addition of a dedicated Flash port, complementing the on-chip 1Mbyte RAM, for storing and accessing additional display assets without impacting system design bandwidth.

ASTC (Adaptive Scalable Texture Compression) decoding is also now supported, further extending the usability of available memory. The addition of this bitmap compression algorithm has enabled larger font tables, animations and other display objects to be applied more efficiently.

Both ICs have video playback capabilities and support graphics rendering for SVGA resolutions up to 800 × 600-pixel screens: the BT816 offers support for displays with four-wire resistive touchscreens; and the BT815 is designed for use with capacitive touchscreens offering multi-touch operation.

Other key features include: digital audio output pin, extended command set including the new Flash memory access, bitmap rotation around a user defined point, and Unicode string support.

Offering an operating temperature range from –40 to +85°C, series devices are packaged in 64-pin VQFNs.

The Bridgetek BT815/816 graphic display controller ICs are shipping now from RS in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components, Allied Electronics & Automation and IESA Ltd are the trading brands of Electrocomponents plc, a global multi-channel distributor. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2018 had revenues of £1.71bn.

For more information, please visit the website at https://uk.rs-online.com

Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000

Further information is available via these links:

Twitter: @RSComponents; @designsparkRS

Linkedin: www.linkedin.com/company/rs-components

RS Components

www.rs-online.com

DesignSpark

www.rs-online.com/designspark

Electrocomponents plc

www.electrocomponents.com