Press Releases


RS Components introduces Microchip microcontrollers and development kits for IoT and touch-control applications

MCUs and development kits are based around ArmÒ CortexÒ-M23 microprocessor and integrate Microchip’s picoPowerÒ technology

London, UK, 20 September 2018:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), a global multi-channel distributor, has announced availability of the SAM L10 and SAM L11 family of 32-bit microcontrollers (MCUs) from Microchip, along with supporting development kits that enable users to experience the high performance levels and integrated hardware-based security delivered by these new ArmÒ CortexÒ-powered MCUs.

This latest family of Microchip MCUs targets a broad spectrum of potential applications including the IoT and security-in-home automation or smart agriculture, and ultra-low-power applications such as energy harvesting and other low-power industrial use. The devices are also suitable for capacitive touch control applications such as remote controls, automotive door handles or industrial keypads.

The low-power SAM L10 and SAM L11 family comprises the industry’s first Arm Cortex-M23-based MCUs in a small footprint, delivering enhanced performance and smaller code size compared to Arm Cortex M0+-based devices. The family has achieved an EEMBC ULPMark certified benchmark score of 405, which is more than 200% higher than the nearest competitor devices.

The SAM L11 MCUs also provide robust security features including: ArmÒ TrustZoneÒ; chip-level tamper detect; crypto-acceleration with AES128 and SHA256 encryption; secure boot and bootloader; and secure key storage. Ideal for protecting network nodes from remote software attacks, the TrustZone technology can partition the main processor into secured and non-secure zones for a variety of IoT applications such as LoRA or SigFox low-power wireless nodes, or in access control, or in automated systems with connected thermostats, for example.

The SAM L10 and SAM L11 family also integrates industry-leading capacitive-touch technology and Microchip’s proprietary picoPower technology, which delivers both high performance and low-power consumption, thereby improving battery life and lowering overall system cost. Other key metrics of the MCUs include: an ultra-low active current of less than 25µA per MHz; standby RAM retention of less than 0.6µA; OFF-mode consumption of less than 100nA; and wakeup times of 1.5µs from idle mode and 2.6µs from sleep mode.

Both the SAM L10 and SAM L11 are configured with a 32MHz Cortex-M23 microprocessor core with up to 64K Flash memory and up to 16K SRAM. Key peripherals for both devices also include: enhanced PTC; 12-bit ADC; 10-bit DAC; op amps; and Sercom serial interfaces. Package options include TQFP, QFN, WLCSP and SSOP, and temperature options include –40 to +85°C and –40 to +125°C.

To enable engineers to get up and running quickly and evaluate the possibilities of the MCUs, RS is also stocking Microchip’s Xplained Pro development kits, based respectively around the SAM L10 and SAM L11.

The Microchip SAM L10 and SAM L11 MCUs and Xplained Pro kits are shipping now from RS in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components and Allied Electronics & Automation are the trading brands of Electrocomponents plc, a global multi-channel distributor. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2018 had revenues of £1.71bn.

For more information, please visit the website at www.rs-online.com.

Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com
+44 (0) 7795 400 651

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000



Further information is available via these links:

Twitter: 
@RSComponents     
@alliedelec   
@designsparkRS


RS Components on Linkedin:  
http://www.linkedin.com/company/rs-components


Other Relevant Links:

Electrocomponents plc: 
www.electrocomponents.com

RS Components: 
www.rs-online.com

DesignSpark
www.designspark.com