Press Releases


RS Components brings ambience and energy savings to enterprise market with simple, scalable SylSmart lighting

Focused family of LED lights, energy-harvesting switches, and occupancy/ambient sensors connects wirelessly with BLE and mobile app

London, UK, 10 July 2018:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), a global multi-channel distributor, has extended its portfolio of smart-building solutions with SylSmart lighting, a comprehensive and uncomplicated range from Sylvania designed to be easy to specify, install and commission.

Smart lighting gives end users greater control over the lit environment, as well as helping enterprises reduce energy costs. Venues can appear more welcoming, showrooms more enticing, and offices more productive. RS’ new SylSmart range simplifies implementation, comprising flat-panel and circular LED light modules, an ambient-light and occupation sensor, and a wall switch, all ready to connect using built-in Bluetooth® Low Energy (BLE) technology.

Installation is easy with minimal wiring required, commissioning is straightforward thanks to app-controlled pairing of the components, and the lighting system is quickly ready to use. The end user controls the lights via the intuitive SylSmart mobile app, or wall switches, and can create groups of lights, arrange lighting scenarios, and establish turn-on/turn-off and dimming presets based on time of day, ambient light, and occupancy. Adding new lights, switches or sensors to the network is also fast and easy, allowing cost-effective scalability.

The Syl-Lighter LED II SSC is a ceiling-mount recessed circular 21-Watt light unit in an aluminium housing designed for a 205mm-diameter cutout. The Start Flat Panel LED is a non-dimmable 595mm x 595mm square, 40-Watt unit, 10.5mm high, featuring a polycarbonate opal diffuser. Both lamps are cool white, 4000K CCT, with high colour fidelity at 80 CRI, and connect directly to the AC line. Both are featured for full wireless control via the wall switch or SylSmart app.

The SylSmart switch is a white, 2-gang wall switch. Built-in wireless and batteryless technologies simplify installation, giving freedom to position and re-position as required, without the need to add any new wiring. The switch is self-powered through built-in energy-harvesting technology, and is surface or back-box mountable.

The SylSmart Standalone wireless room sensor monitors ambient light and occupancy, and is designed for flush mounting with direct electrical connection to the AC line with no additional controls cabling required. It has occupancy detection range of up to seven metres, and adjustable time delay from 10 seconds to 99 minutes.

Architects or installers can easily configure a smart-lighting system for any building or space by combining lamps, switches and sensors as desired. The SylSmart app is free to download from app stores, to assist initial configuration as well as day-to-day lighting control by end users.

Sylvania’s SylSmart lighting solutions are available from RS in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components and Allied Electronics & Automation are the trading brands of Electrocomponents plc, a global multi-channel distributor. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2018 had revenues of £1.71bn.

For more information, please visit the website at www.rs-online.com.

Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com
+44 (0) 7795 400 651

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000



Further information is available via these links:

Twitter: 
@RSComponents     
@alliedelec   
@designsparkRS


RS Components on Linkedin:  
http://www.linkedin.com/company/rs-components


Other Relevant Links:

Electrocomponents plc: 
www.electrocomponents.com

RS Components: 
www.rs-online.com

DesignSpark
www.designspark.com