Press Releases


RS Components stocks 5-megapixel colour imaging module for FPGA development boards

Direct sensor-FPGA communication slashes latency

London, UK, 26 June 2018:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), a global multi-channel distributor, has announced availability of the Digilent Pcam 5C fixed-focus colour imaging module, designed for use with FPGA development boards. The Pcam 5C represents a reliable, keenly priced peripheral for electronics design engineers building devices with embedded camera applications.

The Pcam 5C is built around the 5-megapixel Omnivision OV5640 image sensor, which offers a number of internal processing functions to improve image quality. These include automatic white balance, automatic black level calibration, and controls to adjust saturation, hue, gamma and sharpness.

The Pcam 5C comes with a fixed-focus lens fitted to a standard M12 lens mount to allow interchanging. It is implemented on a small (4.0 x 2.5 cm) PCB with a 1x7 straight header to allow access to auxiliary camera signals. Output formats include RAW10, RGB565, CCIR656, YUV422/420 and YCbCr422.

Data transfer between the image sensor and its host development board is via a dual-lane MIPI CSI-2 interface, providing sufficient bandwidth to support frequently used streaming video formats including 1080p (full HD) at 30 frames per second and 720p (standard HD) at 60 frames per second. The physical connection is a 15-pin flat flexible cable (FFC) that is pin compatible with the familiar Raspberry Pi camera connector; a 10 cm FFC is supplied with the Pcam 5C.

Educational design tool specialist Digilent designed the Pcam 5C for use, in particular, with its Zybo Z7 ARM/FPGA development board, and both are to be made available as an ‘embedded vision bundle’. The Zybo Z7 features a dual-core ARM Cortex-9 processor integrated with Xilinx Zynq-7000 FPGA logic on a single SoC. The Z7’s onboard Pcam connector allows direct communication between the image sensor and the FPGA, delivering much lower latency than HDMI or USB alternatives.

Because it is expensive to license, or complex and time consuming to develop a MIPI CSI-2 controller implementation for FPGA, Digilent provides its own set of Vivado IP cores that work with the Pcam 5C on Xilinx FPGA and Zynq host boards. As no dedicated CSI-2 decoding hardware is involved, users can observe how decoding is accomplished using the FPGA.

The Digilent Pcam 5C is shipping now from RS in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components and Allied Electronics & Automation are the trading brands of Electrocomponents plc, a global multi-channel distributor. We offer more than 500,000 industrial and electronics products, sourced from over 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we ship more than 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2018 had revenues of £1.71bn.

For more information, please visit the website at www.rs-online.com.

Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com
+44 (0) 7795 400 651

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000



Further information is available via these links:

Twitter: 
@RSComponents     
@alliedelec   
@designsparkRS


RS Components on Linkedin:  
http://www.linkedin.com/company/rs-components


Other Relevant Links:

Electrocomponents plc: 
www.electrocomponents.com

RS Components: 
www.rs-online.com

DesignSpark
www.designspark.com