Press Releases


RS Components, MikroElektronika, Cypress Semiconductor co-create flexible platform for faster IoT-device development

Available exclusively through RS, new Clicker 2 for PSoC® 6 kit maximises ease of use and click board™ expandability for faster time to market

London, UK, 26 February 2018:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has worked with Cypress Semiconductor Corp. and MikroElektronika to create Clicker 2 for PSoC® 6, the development kit for faster prototyping with Cypress’ PSoC 6 ultra-low-power microcontrollers (MCUs).

Bridging the gap between expensive, power hungry application processors and low performance MCUs, PSoC 6 MCUs deliver advanced compute performance for energy-conscious devices like IoT endpoints or other small battery-powered objects. Its dual-core architecture combines an Arm® Cortex® M4 and an Arm® Cortex® M0+ on the same chip, delivering flexibility to assign tasks for optimum performance and power-efficiency. Its best-in-class flexible architecture enables interfacing with different types of sensors and creating custom interfaces. Lightweight, state-of-the-art security based on trusted execution environment (TEE) provides protection including secure boot, secure data storage, and advanced cryptographic algorithms without the overhead of external memory or a secure element.

Developers can now quickly bring their PSoC 6 projects to life using the new Clicker 2 development kit, to be marketed exclusively through RS. The board contains a PSoC 63 Connectivity Line device, which is Bluetooth® 5 compliant and simplifies interfacing with many different types of devices. Two separate mikroBUS™ interface headers ensure ample expandability using MikroElektronika click boards™. Literally hundreds of click boards are available, each with working example code, giving easy access to functions such as GSM, GPS/GNSS, motor control, sub-GHz or 2.4GHz radio, speech recognition, sensors, meters, LCD or OLED displays, and many more. The option to add two click boards simultaneously to Clicker 2 for PSoC 6 doubles expandability and saves users making either-or decisions.

Aleksandar Mitrovic, MikroElektronika Product Marketing Manager, commented, “Clicker 2 is the ideal platform to begin PSoC 6 projects, combining ease of use, flexibility and economy.”

“The Clicker 2 for PSoC 6 marks our introduction into the flourishing MikroElektronika click board community utilising our PSoC 6 MCU solution, which is purpose-built for the IoT,” said Jim Davis, Marketing Director of the MCU Business Unit at Cypress. “In line with Cypress’ focus on solving problems for our customers to enable their next-generation products, we are expanding our reach into strong partner ecosystems, and RS and MikroElektronika are a perfect fit.”

“Working together with MikroElektronika and Cypress, we have addressed important engineering challenges for developers to ensure Clicker 2 for PSoC 6 provides the best possible kick-start for our customers’ projects,” said Andy Keenan, Vice President Category Management for Semiconductors and Passives at RS.

PSoC 6 is an ideal microcontroller for performance-conscious, energy-constrained IoT devices. It combines perfectly with the out-of-the-box simplicity and huge range of custom expansion options provided by MikroElektronika’s Clicker 2 platform and click boards.

RS and its partners in the project will demonstrate Clicker 2 for PSoC 6 at the Cypress Semiconductor booth, Hall 4A Stand 148, at embedded world 2018 in Nuremberg from February 27 to March 1. The kit will be available exclusively from RS during March.

-Ends-

About RS Components

RS Components and Allied Electronics & Automation are the trading brands of Electrocomponents plc, the global distributor for engineers. We offer more than 500,000 industrial and electronic products, sourced from 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we trade through multiple channels and ship around 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2017 had revenues of £1.51bn.

For more information, please visit the website at www.rs-online.com.

Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com
+44 (0) 7795 400 651

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000



Further information is available via these links:

Twitter: 
@RSComponents     
@alliedelec   
@designsparkRS


RS Components on Linkedin:  
http://www.linkedin.com/company/rs-components


Other Relevant Links:

Electrocomponents plc: 
www.electrocomponents.com

RS Components: 
www.rs-online.com

DesignSpark
www.designspark.com