Press Releases


RS Components introduces class-leading function/arbitrary generators for test and design engineers

Launch of TGF3000 series marks 40th anniversary of business relationship between RS and Aim-TTi

London, UK, 23 February 2018:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has announced the launch of two new products from leading test and measurement company Aim-TTi (Thurlby Thandar Instruments). The TGF3000 series of function/arbitrary generators delivers class-leading performance and unrivalled value for money.

The launch also celebrates the working partnership between RS and Aim-TTi, which has been ongoing now for 40 years. During this time, Aim-TTi has built a reputation for innovation and enhancement and is one of the leading producers of general-purpose electronic test instruments and laboratory power supplies in Europe.

The TGF3000 series is the latest function/arbitrary waveform generator series and delivers a frequency capability of up to 160MHz, combined with two identical full-performance channels that can operate as independent generators or in coupled or tracking modes. The series also delivers precise channel-to-channel phase control with a resolution of 0.001°.

The series offers a wide range of built-in waveforms along with custom arbitrary waveforms that can be used at sample speeds up to 800-MS/s with replay rates up to 80MHz. The units also come with PC-based arbitrary waveform generation and editing software.

Other features include high resolution performance and the capability to generate low jitter pulses as well as wide-bandwidth white noise. In addition, an extensive array of modulations is available with gated, burst and sweep modes that are able to use either internal or external trigger sources.

On the launch of the new TGF3000 series, Mark Edwards, Managing Director at Aim-TTi, said: “Going back to 1978 when we first began working together with the launch of the PL series of digital power supplies, through the Thurlby Thandar merger in the late 1980s and beyond, our relationship with RS has always been a highly synergistic one. It has continued to evolve to deliver the benefits from our cooperation and the highest possible levels of service to engineers who are working in product design and development, and bench test environments.”

Two models are available in the TGF3000 series: the TGF3162, which is a 160MHz generator; and the TGF3082, which is an 80MHz generator. Both are now shipping from RS in the EMEA and Asia Pacific regions.

-Ends-

About RS Components

RS Components and Allied Electronics & Automation are the trading brands of Electrocomponents plc, the global distributor for engineers. We offer more than 500,000 industrial and electronic products, sourced from 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we trade through multiple channels and ship around 50,000 parcels a day.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2017 had revenues of £1.51bn.

For more information, please visit the website at www.rs-online.com.

Editorial Contacts
Aakriti Kaushik
PR Manager - Northern Europe
RS Components
aakriti.kaushik@rs-components.com
+44 (0) 7795 400 651

PR Agency Contact
Janice Fenton
Account Director
Publitek Technology PR
janice.fenton@publitek.com
+44 (0)1225 470000



Further information is available via these links:

Twitter: 
@RSComponents     
@alliedelec   
@designsparkRS


RS Components on Linkedin:  
http://www.linkedin.com/company/rs-components


Other Relevant Links:

Electrocomponents plc: 
www.electrocomponents.com

RS Components: 
www.rs-online.com

DesignSpark
www.designspark.com