Reducing Downtime with Predictive Sensors

If you want to move from reactive maintenance to a predictive maintenance regime, sensors can be retrofitted to machinery to detect problems before they become major issues.

An engineer calibrating a predictive sensor in a dimly lit factory.

If you are moving from reactive maintenance to a predictive maintenance regime, you will need to use predictive maintenance sensors to help reduce downtime. These are sensors that continuously monitor machinery condition in manufacturing facilities. They provide an early warning that there’s a problem that could lead to a machine breaking down. This enables engineers to intervene before the machine fails.

By carrying out predictive maintenance, manufacturers can save time and money and avoid the potentially catastrophic consequences of a machine breaking down unexpectedly. Read our guide to understand how to use predictive maintenance sensors.

How Vibration Analysis Predicts Bearing Failure

Vibration analysis is a commonly used condition monitoring technology. It works by analysing vibration patterns in gearboxes, motors, pumps, fans, compressors, turbines, and other types of mechanical components by using vibration sensors. When these components are working, they vibrate, but with a predictable pattern. However, if there is a mechanical problem, such as a worn-out bearing or misalignment, the pattern changes. This provides the engineer with a telltale sign that something is wrong, letting them know that an intervention is necessary to prevent the machine from failing altogether.

A vibration sensor is usually a type of accelerometer. It typically measures:

  • Amplitude (How strong is the vibration?)
  • Frequency (How fast is the vibration?)
  • Vibration patterns over time

When the engineer analyses this information, it can uncover a fault.

Vibration analysis has advantages over other common methods of detecting problems with machinery, such as measuring the temperature of components. While temperature measurements often indicate failure at a late stage, vibration analysis detects early-stage failure. Indeed, in the case of bearings, vibration analysis may detect faults months before breakdown takes place. This makes the technique an invaluable tool for engineers in sectors such as power generation, automotive manufacturing, the water industry, and in looking after common equipment such as motors and HVAC systems.

Shop Vibration Sensors

Browse From Our Hand Picked Selection of Vibration Sensors:

Each (In a Pack of 5)
£3.412
Each
£213.70
  • RS Stock No. 893-7177
  • Mfr. Part No. 11028414-00
Each
£10.35
Each
£297.13

Thermal Monitoring for Electrical Faults

Thermal monitoring of electrical systems can identify problems by detecting abnormal heat patterns. That’s because an electrical fault typically generates excess heat before failure. A temperature rise is another type of early warning that failure may be imminent. Thermal monitoring is used to detect problems in electrical switchboards, transformers, cables, circuit breakers, busbars, and many other electrical systems.

There are several thermal monitoring techniques on the market. Fixed thermal sensors may be used for continuous monitoring of electrical equipment. These types of sensors are often used in data centres, hospitals, and manufacturing facilities and provide real-time alerts by measuring factors such as busbar temperature, transformer winding temperature, or breaker contact temperature.

Infrared thermography is another common monitoring technology. This uses a thermal camera to detect heat differences without having to touch the component being analysed. The advantage of this technique is that it is quick and non-invasive. It is often used for periodic inspections of the health of electrical equipment.

An engineer holding a handheld thermal imaging camera, scanning an electrical panel to detect heat patterns and potential issues.

As with vibration analysis, infrared thermography and fixed thermal sensors help detect problems early on, enabling engineers to intervene. This avoids electrical fires, damage to equipment, and interruptions to production.

Let’s look at some of the FAQs when it comes to thermal monitoring:

Thermal Monitoring FAQs

Integrating Sensor Data with Your CMMS

A CMMS is a computerised maintenance management system. If you integrate sensor data with the CMMS, the alerts generated by the sensors can automatically generate a work order for maintenance to be carried out by an engineer. This helps speed up repairs.

Why integrate your sensors with the CMMS?

With integration
Without integration
Alerts trigger automatic work orderAlerts may be ignored
Real-time updates about assetsData has to be manually inputted
Predictive maintenanceReactive maintenance

Integrating sensor data with CMMSs can lead to a reduction in downtime of up to 50% and typically deliver a 10 – 25% reduction in maintenance costs. The integration of these systems also enables better forecasting of spare part requirements.

If you want to make a start on integrating your sensor data with your CMMS, it helps to bear in mind the following:

  • Identify critical assets first. Trying to do everything all at once is a recipe for a failed integration programme
  • Create automated workflows. By defining fault types, you can develop work order templates. The severity of the fault should help prioritise the work order
  • Define the level of your alarms and triggers. Is the alarm a warning that requires just an inspection, or is it critical, requiring immediate attention from a technician?

Retrofitting Sensors to Legacy Equipment

To set yourself up for IIOT condition monitoring in a smart factory, you may wish to retrofit sensors to older manufacturing equipment rather than buying new equipment with pre-installed sensor systems. Manufacturing assets may be very old, but work perfectly well mechanically. To move from reactive to predictive maintenance, it’s necessary to fit that older equipment with sensor technology.

Equipment where retrofitting is useful includes components such as motors, pumps, compressors, gearboxes, fans, conveyors, transformers, and switchgear. Sensors may be retrofitted at a much lower cost than replacing this equipment would entail, and with minimal disruption to production.

Sensors fitted may be vibration sensors, thermal sensors, current and power sensors, or acoustic or ultrasonic sensors. It’s important to consider the power supply for the sensor (if battery-powered, how long will the battery last?), sensor connectivity (what comms network will it send data over and will the connection be wired or wireless?), the mounting surface (is it flat and clean?), and environmental conditions (will the sensor operate in extremes of temperature, dust, moisture, or vibration?). Some common pitfalls to avoid include:

  • Poor sensor placement. Sensors are mounted on parts that come off or that aren’t rigid
  • Not looking at historical data. It’s important to know what constitutes normal functioning so you know when to set an alert
  • Lack of integration with the CMMS. If the sensors aren’t integrated with the CMMS, they may end up being ignored altogether

Calculating the ROI of a Sensor Network

The return on investment (ROI) of a sensor network is determined by the prevention of machinery downtime. To calculate ROI, you need to first factor in how much your new preventative maintenance system has cost, including installation of hardware (such as vibration monitoring systems), software expenditure (e.g., CMMS integration), and the costs of investing in IT and maintenance personnel.

Then factor in the savings: Calculate the cost of unplanned downtime per hour. If you multiply this by the number of hours of unplanned downtime prevented each year, you will have a good idea of the ROI. You could also consider maintenance that becomes unnecessary under the new predictive regime, or the financial benefits of extending the life of an asset. There may also be advantages in terms of improved manufacturing quality and performance (early detection of inefficiencies, for example).

If you analyse the impact of predictive maintenance across a portfolio of critical machinery, you will soon see how the benefits of a sensor network for predictive maintenance are stacking up in financial terms.

Why not explore our range of high-performance sensors and condition monitoring equipment?

Lorna Little

Lorna is an SEO Content Specialist at RS, where she creates search-led content focused on topics including industrial innovation, engineering, maintenance, and procurement. After studying Creative & Professional Writing at Canterbury Christ Church University, she built her career in SEO and content marketing across both agency and in-house environments, helping readers navigate technical subjects through informative, user-focused content. Outside of work, Lorna enjoys reading, travelling, and making memories with her family.

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy