- Justyna Matuszak
- Published 8 Sept 2026
- Last Modified 29 Oct 2026
- 5 min
IO-Link and its Importance in Industry 4.0
In today's factories, the demand for automation, flexibility and advanced technologies is growing. Efficient production relies on intelligent devices that allow for real-time connectivity, transforming traditional sensors and actuators into intelligent components.

In this article, we'll explore IO-Link technology and its wide-ranging industrial applications. We'll highlight innovative solutions from some of the industry's leading suppliers, demonstrating how IO-Link is transforming communication between sensors, actuators, and control systems. By improving data accessibility, diagnostics, and process transparency, IO-Link is playing a vital role in helping manufacturers advance their digitalisation strategies and successfully transition towards Industry 4.0.
Meaning of IO-Link in Industry 4.0
Manufacturing is getting more digitalised and mechanised as big data, robotics, and virtual reality become more integrated. Traditional production is changing into smart factories where everything is connected. Thus traditional sensors become 'smart' with IO-Link, allowing them to connect with several parameters.
Instead of reporting merely a low or high signal, a sensor using the IO-Link protocol may convey the actual temperature measurement in real-time. Before, the only information that could be extracted from sensors was an on/off status. IO-Link provides a data structure that is both clear and machine-readable.
IO-Link is not just gaining increasing acceptance in an ever greater number of applications ‒ the manufacturer-independent communication technology is also an enabler for innovative sensor solutions and supports the global availability of data and information required by Industry 4.0.
IO-Link communication standard
IO-link is the first standardised, powerful two-way point-to-point communication system. In other words, IO-Link is a field data acquisition interface with a lot of flexibility. The open communication standard enables a continuous data flow from the sensor or actuator to the control level. Thanks to its compatibility with common industrial architectures, such as Fieldbus and industrial Ethernet, it can be easily connected to existing PLCs or HMIs using standard connectors without additional cabling.
It is especially important that open information technology between the sensor/actuator and I/O terminal complies with the international IO-Link standard, IEC 61131-9. IO-Link, minimises factory downtime, maximises throughput and enables efficient transparency in both the control cabinet and the field.
A simple, consistent and inexpensive point-to-point connection that links sensors and actuators to the control level, systematic diagnostic concepts and efficient handling of parameter data on all levels of the automation system are just a few of the main benefits of IO-Link.

Main benefits of IO-Link communication
Depending on the industry, IO-Link has many advantages, such as:
- Easy integration of complex sensors
- Economical and efficient installation
- Secure and efficient
- Reduced control cabinet size
- Increased availability
- Less wiring and assembly effort
- Detection of disturbance
- Optimised plant operation
- Efficient engineering and diagnosis
- Rapid diagnosis and monitoring of relays and drives
IO-Link Applications
IO-Link devices can be used in many applications in different industrial sectors, including agriculture, food production, machine production, manufacturing, and advanced technologies like switchgear. Below we showcase the vision of industry leaders on IO-Link technology, supported by recommended products like the ones below.
Recommended Products
OMRON
In addition to collecting total runtime data and even temperature information, users can use IO-Link to identify the vendor, product name, and hardware revision. Users may know the condition of many sensors in real-time with the E2E proximity sensors from Omron, allowing them to determine the location and cause of failures ahead of time.
Siemens SIMATIC
Siemens SIMATIC S7-1200 controllers are compact CPUs with integrated I/Os and industrial communication modules that provide an intuitive alternative for compact automation solutions with enhanced communication options and numerous networking functionalities.
Siemens Expansion Module, ET 200 AL
Siemens ET 200 AL Distributed I/O systems have IO-Link modules enabling easy connection of standard sensors to any PLCs or controllers modules, or automation networks, making it the ideal data gathering, monitoring, and control system for totally integrated automation applications.
IO-Link is more than just a communication protocol; it is a key enabler of digital transformation in modern industry. As the demand for greater visibility, automation, and operational intelligence continues to grow, IO-Link provides manufacturers with the foundation needed to build scalable, future-ready production systems. From sensors and actuators to RFID systems, condition monitoring devices, and IO-Link masters, a wide range of compatible products is available to help businesses unlock the full potential of connected manufacturing.

Justyna is a Digital Content Writer at RS, responsible for writing and managing content. She studied Journalism and Social Communication with a specialisation in social media and e-PR. In that time, she participated in journalist internships in Wroclaw (PL) and London. She is passionate about tech innovations, the shift to a digital world and the impact technology has on our lives. Her interests are sport, music and film photography.