Safe Isolation Procedures for Commercial Electrical Panels

Protect your contracting team by using safe isolation procedures. A step-by-step guide to locking out and proving dead for commercial electrical panels before maintenance.

A lockout/tagout system placed on an electrical panel

Commercial electrical equipment requires ongoing maintenance and service, but this must be done safely to prevent contact with live wires. Electrical incidents still produce far too many workplace injuries in the UK. Safe isolation procedures guarantee that the wires you’re working around are and will stay dead.

Electrical lockout tagout and proving dead are essential steps for achieving this. Read on to learn about how they’re quite straightforward and thus have no reason to be neglected.

The Importance of Electrical Lockout Tagout

Safety is of utmost importance when performing electrical troubleshooting and maintenance. Workplace electrical hazards are ever-present, silent, and out-of-sight, but should not be out-of-mind. The HSE reports an annual average of 1,000 workplace incidents related to electricity, 30 of which are fatal. Electricity is also the most common cause of workplace fires, at 18% of all incidents.

Electrical injuries include electric shock, electrical burns, arc flash injuries (such as eye damage from arc blasts of ultraviolet light), electrocution (shock causing death, usually by cardiac arrest), and secondary injuries such as muscle spasms post-shock leading to falls from heights. Electricians and engineers working on electrical equipment need guarantees that they can do their work safely without contacting energised circuits.

Electrical lockout tagout procedures ensure that circuits are dead and safe to work on before work begins. These processes prevent ‘off’ circuits from turning back ‘on', give clear warnings that they’re meant to be locked out, and prove that off circuits are truly dead. They also visibly demonstrate compliance with electrical safety regulations to show that technicians are taking proper precautions.

Lockout tagout locks placed on an electrical panel

Step 1: Planning and Identification

Before locking out a circuit, you should plan proper access to the right one. The first step is to obtain permission to do electrical work on the equipment that needs attention. A work permit is helpful for documenting this permission in case of inspections or audits - or if, despite your best efforts, a safety incident still happens. The permit should specify that isolating the equipment’s circuit is granted.

You’ll also want to determine which specific circuit breaker(s) you need to isolate for this work. The electrical panel’s breakers should hopefully be well-labelled, but this isn’t always the case. Labels can even be incorrect or out of date if circuits have been modified.

Circuit breaker finders are great tools for resolving this since they conclusively determine the circuit breaker for a given electrical device. These tools feature a transmitter and a receiver. To use one to find a breaker, follow these steps:

  1. Verify battery power on the receiver.
  2. Plug the transmitter into an outlet for a device to be serviced and verify that the transmitter lights up, indicating power.
  3. Test that touching the receiver to the transmitter produces a light or a beep, indicating that it’s picked up the transmitter’s signal.
  4. Touch and hold the receiver directly onto the panel’s breakers one at a time. Don’t rush. The receiver will light up or beep at the breaker for the circuit the transmitter is plugged into.

With the circuit breaker identified, you can now proceed with locking it out.

Step 2: Isolation and Proving Dead

Circuit breaker lockout devices hold breakers in the off position and prevent unauthorised personnel from turning them on, which could re-energise circuits technicians are working on. A lockout should fit the size and shape of the breaker, provide a way to be locked, and allow tagout tags to be affixed.

Circuit breaker lockouts come in different shapes, sizes, and fastening methods. They can be snap-on, clamp-on, or use a push button in the case of pin-in and pin-out lockouts. Ensure the lockout is sized properly to your breaker. Lockout sizes are often grouped by the voltage of the breakers they’re suited for, so your breaker voltage is a good place to start when selecting a lockout. Your site’s environmental conditions and activity level can also factor into your lockout choice.

Once the lockout is fastened and holding the breaker off, attach a lock to prevent removing the lockout. This can be a regular padlock, but specialty lockout ones with lockout warnings are ideal. Hasps go a step further by allowing multiple locks on the same lockout. Each one requires a different technician’s key, so they all need to be unlocked before the lockout can be removed from the breaker. Also, it’s good practice to have a unique key for each lock; a key repeated for multiple locks reduces security.

When attaching the locks you should also feed them through tagout tags to warn that the lockout is not to be removed, and the equipment is thus not to be operated until service is complete. Fill in your name, your department, the date, and any other information required so it’s clear who is permitted to remove the lockout and re-energise the circuit.

However, just because a circuit is forced off doesn’t mean it’s dead (i.e., not live). You must also conclusively prove that the circuit is dead before beginning service work on it. If an energised load connects to the neutral of the circuit you’ve locked out, it can become live, meaning serious electrical safety hazards are still present.

Proving dead is an essential step in safe isolation procedures for electrical maintenance, and it should always be done using a combination of a voltage indicator and a proving unit. A common mistake is to use a multimeter or a non-contact voltage detector for proving dead. Multimeters have a chance for human error, and dead batteries can produce false dead readings. Meanwhile, non-contact voltage detectors just detect voltage, not the absence of it, and static can interfere with them.

Using Voltage Indicators

Proper, safe proving dead of circuits should involve both a voltage indicator and a proving unit.

A voltage indicator (VI) indicates the presence of voltage going through a circuit or component. Its probes are connected to a suspected live wire and a grounding point, and the indicator assesses any resultant flowing current by feeding it through a fixed, known resistance. Based on Ohm’s Law (which relates current and resistance to voltage), the indicator displays that calculated voltage.

A proving unit verifies that the VI is working, which you don’t want to take chances on. Proving units are battery-powered and send a set, known voltage through the VI to check that it reads that voltage value. These units work with both AC and DC.

After locking out the circuit, follow these steps for proving dead with these instruments:

  1. Verify your proving unit has battery charge available.
  2. Connect its testing probes to the VI: the black probe to the negative terminal and the red to the positive.
  3. Set the proving unit to AC or DC, based on the application, and set its test voltage.
  4. Verify that the VI reads that voltage value.
  5. Connect the voltage indicator’s probes to the circuit to be tested and to ground, and verify that no voltage is detected.
  6. Re-check the VI with the proving unit in case it malfunctioned due to a surge from the circuit.

If this second proof on the VI is accurate, you’ve proved this circuit is dead and safe to work on.

Step 3: Securing the Panel

One further step in safe isolation procedures for electrical work is to lock out the entire electrical panel. This gives a further layer of security against accidental re-activation of the circuits under service.

You might be able to simply lock the panel’s door with a padlock, but a proper electrical lockout tagout device for the panel provides greater security and clearly demonstrates that the panel’s been intentionally locked out for safety.

A panel lockout typically snags hooks onto both ends of a (closed) panel’s width and then tightens them taut to block opening the door. A lock and tag are then affixed to complete the lockout.

Once the panel is locked out, and provided you followed all the other above steps in the correct order, you can now perform maintenance on the circuit, safe in the knowledge that it is deactivated and dead and will stay that way.

Electrical lockout tagout kits feature lockouts, locks, hasps, and tags, so they’re great for getting you started on electrically safe isolation procedures. We also stock lockouts for various types of industrial valves. Browse our lockout offerings today.

FAQs

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy