The Shift from Reactive to Predictive Facility Maintenance

Building assets such as AHUs, lifts, and pumps exhibit warning signs before their performance suffers or they break down. Predictive maintenance allows facilities teams to spot these issues early.

Technician using a handheld thermal imaging camera to inspect industrial machinery

Reactive maintenance can look efficient at first glance. It means you only invest in parts and labour when something fails, freeing up budget and engineer time. 

The problems arise when an asset fails without warning. That’s when repairs take longer, and the costs can be harder to control. Likewise, it can be exceedingly difficult to plan last-minute repairs that minimise disruption to building operations. 

Predictive facilities maintenance approaches the problem of unexpected asset failure differently. It works from the idea that an asset should not have to fail before you take action. To do this, it analyses data from your assets to spot problems before they affect your site's operations. The result is less downtime, lower maintenance costs, and extended asset lifecycles.

This article will explain why and how facilities teams are moving from reactive to predictive maintenance.

The Limitations of Reactive Maintenance

Many teams already get signals about the state of their assets from their building energy management system. However, those signals can often occur at or too close to the point of actual failure.

Another issue is that the signal itself may not give engineers enough context. That means engineers have to locate and check the asset's service history. Those details may not be accurate or complete. There simply may not be enough detail for them to connect the current fault to an earlier issue.

With only a late warning and limited context, engineers then have two choices. They can complete a temporary repair to keep the asset running safely until the next planned maintenance window, or they can do a full repair, which can take building services offline.

Whatever they decide, they have to make sure the repair:

  • Minimises disruption to tenants, staff, and visitors
  • Takes place when suitable contractors are available for the work
  • Does not impact on the safe running of other building services
  • Complies with all service, statutory, and warranty requirements

Reactive maintenance is last-minute, expensive, and harder to manage. Plus, running assets close to or at the point of breaking can shorten their useful lifespan. This also increases the risk of damage to other connected assets.

With predictive maintenance, there’s no waiting for a fixed service date or a complete failure. Asset condition data can be used to decide when to inspect, service, or repair an asset. Studies have shown that taking this approach can save 12% to 18% compared with reactive maintenance alone.

Predictive maintenance won’t rid a building of faults. It will, however, provide earlier warnings, more time to plan, and greater control over the repair budget.

Female maintenance technician wearing safety glasses, ear protection, and gloves while inspecting industrial machinery in a manufacturing facility.

Building a Proactive FM Strategy

Any proactive facility maintenance (FM) strategy must start with prioritising the assets. These can include:

  • HVAC plant
  • Lifts
  • Pumps
  • Electrical panels
  • Access systems
  • Fire safety equipment

These are the systems that have the greatest effect on safety, comfort, and day-to-day building use.

The next step is investigating how each asset on the list behaves before it fails. That might be pumps vibrating more, motors drawing more current, and changes in pressure or flow in water systems. These may all indicate a danger of more serious service problems appearing later down the line.

To monitor these assets, FM teams need sensors and building data that show early signs of wear, load changes, and repeat faults. The people on the team need to know how to read the data and what to do if a reading changes or goes over the agreed threshold.

The most effective predictive maintenance strategies connect data to action. Depending on the issue the data highlights, that might trigger one or more of the following actions from you or a member of the FM team:

  • Inspecting the asset
  • Ordering a replacement part
  • Scheduling in a qualified contractor
  • Checking part availability

The key to a successful, proactive FM strategy is a plan for each asset, where the most important risks take precedence. While unexpected failures are still possible, they will occur far less frequently and cause far less disruption.

Implementing Digital Twin Smart Buildings

A digital twin smart building is a live digital model of a physical building and its assets. Digital twins help facilities teams see a fuller picture of a potential fault before sending an engineer. 

For example, a temperature sensor may show that one area is getting too warm. The reason for this could be:

  • A sensor feeding back incorrect readings
  • Heating or cooling equipment not responding as expected
  • Restrictions to the airflow in that part of the building
  • The control setting on a piece of equipment telling the system to hold the wrong setpoint
  • Recent work, like a filter change or sensor replacement

Without a central source of information, piecing together the actual reasons a fault occurred is hard.

In a digital twin smart building, this information is centralised. Each reading and record is linked to the same asset, room, or building system. 

In the example above, the team can check the temperature reading against airflow data, sensor records, and more. This gives the engineer a clearer starting point before they start work. 

In this case, they could model a setpoint change to see whether the temperature in the area would go back to the right range. If it doesn't fix the issue in the model, then it might be better to send in the engineer to check the sensor, equipment, and airflow.

Digital twin models need accurate and up-to-date records to work effectively. The reliability of any results lessens when data like asset tags are wrong, service history is missing, and sensor names are unclear.

In older buildings and mixed estates, teams often need to check and clean their asset records before using a twin in decision-making.

The Role of IoT and Data

Implementing a digital twin smart building requires the installation of reporting sensors. These sensors reduce the reliance on walk-round checks where inspections often miss details like small changes in:

  • Carbon dioxide
  • Current draw
  • Energy use
  • Flow
  • Humidity
  • Occupancy
  • Pressure
  • Run time
  • Temperature
  • Vibration

CIBSE has found that many buildings already collect some of this data through their existing BMS, BEMS, or BACS systems.

As such, some buildings don't need to invest in a brand new set of sensors. It may be enough for an organisation to check which readings already exist from established assets. They still may need to replace a sensor, however, if it doesn't provide all the necessary data, for example. 

When building a predictive facility maintenance programme, each sensor or system reading must be paired with an asset. The team will then know which piece of equipment the alert relates to and where it is.

Each asset must have its own response rules. A small vibration charge on a non-critical pump might need logging but no more. But with a pump serving a busy area, a vibration may necessitate an inspection, part check, or immediate repair.

The data created by condition monitoring needs owners. There should be an agreement on who checks individual critical assets, systems, or areas in the building energy management system.

Setting the right roles and rules now means engineers focus on the assets that need action before they disrupt operations.

The Future of Predictive Facility Maintenance

Data is the vital component in predictive facility maintenance. However, more data on increasingly complex dashboards is not likely to be the future. Artificial intelligence (AI) will influence this shift more.

AI is capable of handling and evaluating data at far greater speed and in far greater volumes than humans. It can constantly compare readings across building zones, zeroing in on individual assets like lifts, panels, and AHUs. AI-powered digital twins can spot patterns that are too complex for people to recognise while on the move.

In the long term, this will have spin-off effects in procurement as well. Distributed AI-powered systems will learn which parts in individual assets are the most likely to fail. Facilities teams can then hold critical spares for high-risk assets. This can help prevent emergency orders and longer repair delays.

Together, this technology is building toward smarter, more proactive facilities. If you’re ready to shift from reactive repairs to a proactive maintenance strategy, you can explore our range of condition monitoring solutions and vibration sensors to start capturing real-time asset data. You can also browse our complete building automation range to equip your facility for data-driven downtime prevention.

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy