Regenerative Braking on Conveyors

Regenerative braking system conveyors recover energy instead of wasting it as heat. Read our guide to find out how, and whether regenerative braking is suitable for your conveyor.

A conveyor system in operation in a warehouse

A regenerative braking system on a conveyor recovers energy instead of wasting it as heat. On some conveyors – especially conveyors that run downhill – the load pulls the belt faster than the motor that is driving it. In a conventional conveyor set-up, braking resistors or mechanical brakes are used to dissipate that excess energy in the form of heat.

By contrast, if regenerative braking is used, the motor acts as a generator and energy from the load is converted into electrical energy. That energy is then directed back into the system. This guide explains how regenerative braking on conveyors works, how to calculate energy recovery, and the impact on power quality.

Read on to learn more about harvesting energy from conveyors.

A conveyor system in operation in a warehouse

The Physics: Motoring Vs. Generating Quadrants

If your conveyor can be driven by gravity or load, it’s a candidate for regenerative braking. That’s because regenerative braking is most beneficial in applications where the conveyor declines, features heavy loads moving downhill, or where there is frequent deceleration of large masses.

Most modern regenerative drive conveyors use a variable frequency drive (VFD) with regenerative capability – or ‘VFD regen unit.’ The conveyor runs downhill and the load drives the motor, which enters generating mode. The VFD captures this energy and feeds it back into the grid or shares it with other drives.

In electric drive systems, motoring and generating quadrants show how torque and speed interact to define whether a motor is consuming or producing energy. This relationship can be set out as four quadrants. The central concept is that power = torque x speed. The positivity or negativity of torque and rotational speed determines the direction of the flow of power.

Let’s break those quadrants down step-by-step.

Quadrant 1: Forward motoring

  • Speed – positive
  • Torque – positive
  • Power – positive

Quadrant 1 is the normal operating mode. The motor drives the load forward.

Quadrant 2: Forward generating (regenerative braking)

  • Speed – positive
  • Torque – negative
  • Power – negative

In Quadrant 2, the load drives the motor while it is rotating forward and the motor resists motion (negative torque) and acts as a generator. The power generated can be used elsewhere.

Quadrant 3: Reverse motoring

  • Speed – negative
  • Torque – negative
  • Power – positive

In Quadrant 3, the motor actively drives the system in reverse. Torque and speed are aligned and energy flows from the electrical supply to the load, just in a reversed direction.

Quadrant 4: Reverse generating

  • Speed – negative
  • Torque – positive
  • Power – negative

In Quadrant 4, the system generates in reverse, but the motor applies opposing torque. The load drives the system, and energy is regenerated.

Braking Resistors vs Regenerative Units

Braking resistors and regenerative units slow down or control overhauling loads on conveyor systems by dealing with excess energy. Braking resistors are the traditional solution to the problem.

When the motor enters generating mode, the excess electrical energy is routed into a resistor via the drive. That energy then dissipates as heat. Braking resistors are good solutions where there is short or intermittent deceleration or light overhauling loads.

Regenerative units instead reuse the excess energy. When the motor generates the power, the drive converts it into usable electrical energy and feeds it back into the power supply.

Let’s compare some of the key differences between these two technologies:

Characteristic
Regenerative Braking
Braking Resistor
PrincipleConverts excess energy into usable powerDissipates excess energy as heat
Energy efficiencyHighLow
Power flowMotor to driveMotor to resistor
Capital costHigher upfront costLow
Operating costLower thanks to energy savingsHigh
Heat generationLowHigh
ComplexityMore complexLow
MaintenanceLess mechanical stress, but more power electronics to maintainModerate maintenance required
ApplicationsDownhill conveyors, mining, portsLight conveyors, cranes
Impact on electrical networkMust meet grid standardsNone
Return on investmentHigher initial cost, payback from energy suppliedLow initial cost, no payback

Calculating Potential Energy Recovery

Calculating potential energy recovery from regenerative braking systems means quantifying how much gravitational energy is available and how much of it can be converted into electrical energy.

The fundamental recoverable energy is based on gravitation energy. It can be expressed as:

E = m x g x h

Where E is potential energy, m is material mass, g is gravitational acceleration, and h is vertical drop. Since conveyors move continuously, their energy requirements can’t be treated as a one-off calculation. Instead, engineers calculate power, the rate of energy transfer over time.

To convert to power, replace mass with mass flow rate (kg/s). This results in: 

P = m x g x h

Where m is the mass flow rate. Running this calculation will tell you how much gravitational power is available when material is moving downhill.

It’s important to also consider the specific details of the conveyor system. For example, what is its throughput? This needs to be converted from the typical metric of tonnes per hour into kg/sec. You must also consider the vertical drop (this is not the length of the conveyor, but the change in elevation experienced by the load), and the energy efficiency of the system. Losses may occur due to belt friction or gearbox and motor inefficiencies.

Don’t forget that only conveyors operating in a generating quadrant (drive by gravity) can recover energy. As a rule, the steeper, heavier, and more continuous the conveyor flow is, the greater potential for energy recovery.

Impact on Power Quality (Harmonics)

Harmonics and power quality are also important considerations. Harmonics are distortions in the electrical waveform caused by non-linear loads. Instead of smooth (sinusoidal) current, devices such as VFDs draw current in pulses, creating additional frequency components. These are known as harmonic frequencies. Power quality problems can arise when distortions affect the wider electrical system. Typical issues include overheating of cables, transformers, and motors, tripping of protection devices, reduced efficiency and equipment lifespan, and interference with electronics.

This issue is vital in a regenerative braking system for a conveyor because power is sent back to the supply, not just taken from it. This means that engineers must specify a drive that can control waveform quality. A VFD regen unit will employ passive or active harmonic filters, multi-pulse rectifiers, or active front-end drives designed to produce near-sinusoidal currents.

ROI for Downhill Applications

Calculating potential energy recovery provides a solid foundation for evaluating whether regenerative braking is worth investing in a downhill conveyor application. The financial benefit is in recovered energy, which must balance the higher upfront cost of investment in such a system.

By calculating recoverable power, an engineer can estimate annual energy savings by multiplying by operating hours and electricity costs (£/kWh). These savings can be substantial for a frequently used, high throughput conveyor. It’s important to remember, however, that the capital costs of VFDs are higher than braking resistors.

The return on your investment in regenerative braking may not just be in the form of recovered energy. The system also reduces heat, and therefore potentially the need for cooling. It may even mean lower maintenance costs because there is less stress on braking systems.

The longer a downhill conveyor spends generating energy, the stronger the business case for adopting a regenerative braking system. It’s important to weigh up all factors when determining the ROI, including recoverable energy, how the system is used and its efficiency, and what adoption will mean for your maintenance regime.

Did you know we stock an array of electric motors and inverter accessories? Explore our extensive range today.

FAQs

Lorna Little

Lorna is an SEO Content Specialist at RS, where she creates search-led content focused on topics including industrial innovation, engineering, maintenance, and procurement. After studying Creative & Professional Writing at Canterbury Christ Church University, she built her career in SEO and content marketing across both agency and in-house environments, helping readers navigate technical subjects through informative, user-focused content. Outside of work, Lorna enjoys reading, travelling, and making memories with her family.

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy