Surface Roughness (Ra) Conversion Chart

Surface roughness (Ra) is crucial for interlocked, sealed, or sliding surfaces. The ideal roughness depends on the application. Ra is the average of all surface peaks and valleys (overall texture), while Rz (Mean Depth) focuses on isolated, critical defects. Manufacturing processes like machining, grinding, and casting directly influence the final finish. A surface roughness conversion chart is vital for translating requirements across different standards (N-Grades, Ra in µm, and Ra in µin).

A red banner with a lighter red gradient.

For two surfaces to work well together, such as those that need to interlock, seal, slide, or bond, for example, each surface must have a specific level of roughness.

In certain applications, a rougher surface is best. This is true of the flat machined surfaces of gasket mating faces. These need greater surface roughness so that when they clamp the gasket, causing it to deform, the gasket surface fills any microgaps in the gasket mating faces. This prevents fluid or gas leaking across the joint.

The lowest levels of surface roughness are needed for the bore of a hydraulic cylinder. The dynamic O-ring, which travels continuously within the inner surface of the cylinder, can only do so effectively at a certain level of roughness. Each time it passes the lip of a seal along the cylinder, it needs to do so with as little abrasion as possible to ensure the seal doesn’t become damaged and potentially, over time, losing its ability to maintain pressure.

Understanding Ra vs Rz

Average Roughness (Ra) and Mean Depth (Rz) are two complementary ways of assessing a surface’s finish.

Ra is the average of all a surface’s peaks and valleys, while Rz is the average of five peak-to-valley distances, from five areas of sampling across the surface.

The implication of high Ra in a manufacturing surface is that the surface has a consistently rough texture, which could create a higher level of friction. A surface with greater levels of friction may need more lubrication to function or may fail to meet the standard required for a specific function, such as creating an effective seal.

The implication of a high Rz measurement in a manufactured surface is that it contains significant peaks or valleys, which are isolated across the surface. This metric is critical for sealing applications, where one deep valley can form a leak path or a high peak can cause a rupture.

A way to think about Ra vs Rz is that Ra provides a picture of the overall texture of a surface, 

Rz is an essential safeguard for the Ra measurement, providing a view of localised surface defects.

Diagram showing Ra average surface roughness and Rz maximum peak-to-valley depth, highlighting how deep defects can cause sealing leaks.

How Manufacturing Processes Define Surface Finish

Different machining methods and manufacturing processes, such as injection moulding, forging, or metal powder 3D printing directly impact the resulting surface finish. For example:

  • Machining leaves a pattern of tool marks. Depending on the cutting machine that moves across the surface, the resulting finish can be approximately 0.4 µm (16 µin) Ra to 3.2 µm (125 µin) Ra
  • Grinding or honing uses abrasion to smooth surfaces to tight tolerances. This can be 0.3 µm (12 µin) Ra or better
  • Polishing also uses abrasion or electrochemistry to reach mirror-like surface finishes. This can achieve a Ra of 0.025 - 0.1 µm (1-4 µin)
  • Casting / forging results in a less refined surface finish, due to the nature of the process (molten material solidifying against a mould or compressive force) which introduces surface irregularities such as grain flow lines, oxide layers, porosity, or an imprint of the mould texture. Casting or forging usually needs a secondary method such as grinding or hot blasting to achieve the appropriate level of finish.

These processes have environmental implications, and may need to be evaluated against green manufacturing certifications if sustainability is a focus for your business.

Chart showing typical Ra surface roughness ranges for polishing, grinding, machining, and raw casting, measured in µm and µin.

An array of factors affect surface finish, in addition to the machining or manufacturing method. For example, 

  • Higher speed cutting tools, with lower feed rates, naturally produce a smoother surface finish due to reduced tool pressure, vibration, and the formation of Built-Up Edge (BUE), where a piece of worked material welds to a cutting tip when operated at low speed
  • Tools that have experienced wear and tear will be less precise than sharp, rigid tools (which reduce vibration-imparted defects), and produce a less finely tuned surface finish
  • The way different materials react to different machining or manufacturing processes can vastly affect the resulting surface roughness. Even though aluminium is easy to machine to a fine level of detail due to its soft, ductile properties, its tendency to warp and tear under pressure from machining and finishing can result in a higher level of roughness. Harder materials, such as steel, are more resistant to finishing and therefore can result in a rougher surface finish

To learn more about how your choice of material and its properties affect manufacturing results, see our advanced manufacturing materials guide.

Conversion Table: Ra to N-Grades

Engineers and manufacturers may find their finishing requirement specifications expressed in different units. To understand how surface roughness values relate to one another across different measurements and standards, a surface roughness conversion chart is essential. 

N-Grade
Ra (µm)
Ra (µin)
Typical Process
N10.0251Superfinishing / lapping
N20.052Superfinishing / lapping
N30.14Polishing
N40.28Polishing / grinding
N50.416Grinding / fine machining
N60.832Grinding / honing
N71.663Fine machining
N83.2125Machining
N96.3250Rough machining
N1012.5500Casting / forging
N11251000Casting / forging
N12502000Raw material / sand casting

An engineer will also encounter surface finish symbols in technical drawings, standards and specifications, and in quality control reports. These indicate the specific finish required to the faces and features of different parts. 

They’ll include the Ra and Rz value, as well as the direction of measurement (important for surfaces where the direction of tool marks relative to the intended sliding or sealing contact direction can affect how much friction, wear and tear or leakage could be caused), the machining method and whether it’s permitted or required to remove material.

Measuring Roughness: Stylus vs Optical Methods

In manufacturing, there are two instruments which are used to measure surface roughness: 

  1. A high precision diamond-tipped probe (or stylus) which measures the topography of a surface point by point. The tip drags across the surface and degrees of vertical displacement are recorded
  2. Focused light (optical method), of which there are three techniques:
    1. Wave patterns (interferometry), which measure surface height variations down to nanometres. This is a precision method, often used to verify a surface finish is compliant
    2. A laser beam (profilometry), which scans a surface to detect and measure height variations. This is a fast, accurate method and it’s particularly useful for measuring Ra across a range of surface types, as well as curved surfaces and surfaces with complex geometries
    3. Light through a pinhole aperture (microscopy), which sections a surface and creates a visual 3D map of surface measurements, perfect for capturing intricate surface features
Comparison table of contact stylus and optical surface roughness measurement methods, showing operation, best uses, advantages and trade-offs.

Both stylus and optical methods are used to verify standards defined by ISO 1302 or ASME B46.1. The stylus approach is the established industry method, it’s slower, but generally cheaper than the optical methods and it’s best for flatter, simpler surfaces.

The optical method is more expensive, but faster and better for complex geometries, fine surfaces, and ultra-delicate surfaces, where the risk of surface damage from the stylus can’t be tolerated.

Why Surface Finish Matters for Seal Performance

Seals need to be manufactured to compliant surface finish standards for two reasons: to ensure high efficacy of the seal itself and to guard against wear and tear, which, over time, undermines the effectiveness of the seal.

Static seals must meet standards such as ISO 1302 and ASME B46.1 to ensure proper functioning of the seal interface, preventing the leakage of fluids or gases under pressure.

While dynamic seals need to be manufactured to tighter Ra tolerances, to ensure they maintain consistent contact and lubrication across moving surfaces.

Friction created by the contact of the surfaces of a seal, such as an airtight O-ring or mechanical face seal, can cause damage over time. That damage can undermine the effectiveness of the seal.

This would be disastrous in life-critical applications, such as aerospace hydraulic systems, medical device fluid circuits or nuclear isolation valves, where seal failure could result in a loss of pressure, the contamination of fluid (an essential consideration in making single-use devices more sustainable), or compromise the containment of radioactive material. 

We stock a range of surface roughness testers, as well as surface roughness comparator sets. Kit out your workshop, lab, or facility with the right engineering test and measurement tools for a perfect finish.

If you’re looking for the right sealant to match your surface finish, you’ll also find adhesive and sealant dispensers in our range, including dispensing guns, adhesive material dispensers and dispensing tips for controlled application.

Lorna Little

Lorna is an SEO Content Specialist at RS, where she creates search-led content focused on topics including industrial innovation, engineering, maintenance, and procurement. After studying Creative & Professional Writing at Canterbury Christ Church University, she built her career in SEO and content marketing across both agency and in-house environments, helping readers navigate technical subjects through informative, user-focused content. Outside of work, Lorna enjoys reading, travelling, and making memories with her family.

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy