Electropolishing vs Mechanical Polishing

Understanding the differences between electropolishing vs mechanical polishing is essential for industries where cleanliness and precision are critical. Used extensively in food and beverage manufacturing and the pharmaceuticals industry, these finishing techniques offer distinct benefits. This guide breaks down the key differences.

A woman in a blue jumpsuit and yellow headphones, in a workshop electropolishing metal materials

Electropolishing and mechanical polishing are used to finish stainless steel equipment in pharmaceuticals and the food industry. Both techniques are used to improve surface finish, enhance visual appearance, and make stainless steel suitable for environments where hygiene is paramount.

Both processes are subtractive, that is, they remove material. They are commonly used on stainless steels, such as 304 and 316L, in welded fabrications, tanks, pipework, fittings, and vessels.

However, there are some key differences when it comes to electropolishing vs mechanical polishing. Want to learn more? Read on.

Key Points:

  • Mechanical polishing and electropolishing help finish stainless steel surfaces but have different end results
  • Both are useful in the food manufacturing and pharmaceutical industries, but electropolishing should be used for surfaces that come into contact with the product
  • Electropolishing offers superior corrosion resistance and helps prevent the development of biofilms on equipment

Mechanical Polishing: Abrasives and Compounds

Mechanical polishing can be defined as a surface finishing process in which metal is smoothed using physical abrasion. This physical abrasion may be carried out with belts, wheels, abrasives, or buffing compounds. The technique is widely used on stainless steel materials and equipment as an initial or intermediary finishing stage.

During mechanical polishing, mechanical energy is used to physically remove surface material. For example, grinding removes welds, defects, or scratches. Finer abrasives may be used to reduce surface roughness, while buffing compounds help to create a reflective finish.

Benefits of mechanical polishing include:

  • Reduction in visible surface defects
  • Visually clean, even, mirror-like appearance
  • Reduction in macroscopic roughness
  • Surfaces that are ready for further treatment

In food and pharmaceutical industry equipment, this technology is used on external tank surfaces, structural elements such as steel frames, pipework, and non-critical process surfaces.

While mechanical polishing improves the look and feel of stainless steel, it doesn’t necessarily achieve the sanitary finish stainless steel can produce, and which may be needed in these two sectors. That’s where electropolishing comes in.

Electropolishing: Anodic Dissolution Explained

Electropolishing is an electrochemical process where a stainless steel part functions as the anode in a bath of electrolyte. When current is applied, metal atoms on the surface are converted into ions. The ions dissolve into the electrolyte, and the surface is levelled at a microscopic scale. This means the surface is effectively being chemically dissolved in a controlled manner, rather than grinding the surface using a mechanical technique.

The reason electropolishing works is that higher peaks on the surface of the material are exposed to more current and dissolve quicker than at lower points (valleys). This evens out the surface of the stainless steel part or structure. The surface effectively flattens as electropolishing takes place.

This is an effect that exceeds the visual impression of smoothness created by mechanical polishing. The ultra-smooth surface at a microscopic level reduces areas where bacteria can attach to the metal. It also means the stainless steel offers improved corrosion resistance and better cleanability.

Microscopy Comparison: Peaks and Valleys

What’s the surface finish comparison that’s most appropriate for electropolishing vs mechanical polishing? Again, it helps to go back to that analogy of peaks and valleys. Electropolishing can be thought of as dissolving the top of a peak faster than the valley at the bottom. By contrast, mechanical polishing can be thought of as sanding the peak down. 

Despite appearances, stainless steel is not flat. Mechanical polishing and electropolishing make it flatter.

At a microscopic level, mechanical polishing flattens peaks as abrasives physically grind the surface. The stainless steel is plastically deformed. Peaks are reduced, but material tends to be pushed sideways. This results in what is known as smearing and the valleys remain relatively deep. Although the surface looks smooth, it’s still rough at a microscopic level.

Electropolishing, on the other hand, selectively removes peaks and creates shallower valleys. Unlike mechanical polishing, it doesn’t create directional scratches or smears. That’s because the surface is being dissolved chemically, with high points dissolving faster, and low points dissolving slower because they carry less current. At a microscopic level, this creates a level surface - peaks are reduced and valleys are relatively less pronounced. Abrasive particles may remain embedded in the material.

Let’s do a quick comparison of the features of these two techniques:

Feature
Electropolishing
Mechanical polishing
Peak removalSelective dissolutionMechanical cutting
Material behaviourUniform removal of metalSmearing and deformation
Microbial sitesReducedAvailable
Embedded particlesNonePossible
Surface patternSmoothDirectional scratches
Valley depthSignificantly reducedRelatively deep

Why Electropolishing Offers Better Corrosion Resistance

Electropolishing improves corrosion resistance. It makes stainless steel chemically stable and less reactive. Following mechanical polishing, stainless steel will be stressed, smeared, plastically deformed, and more chemically reactive.

Electropolishing dissolves this outer layer away and exposes a cleaner and more uniform stainless steel structure underneath, removing the corrosion-prone part of the surface.

Stainless steel resists corrosion because of a chromium oxide passive film. Electropolishing helps to enrich this layer by removing iron from the surface of the steel, leaving a surface that is relatively richer in chromium and nickel. Corrosion often starts at microscopic features on the metal surface such as peaks, valleys, grooves, or scratches. Electropolishing helps to remove these elements, enhancing the corrosion resistance of the metal.

Choosing for Food & Pharma Applications

To choose between mechanical polishing and electropolishing, you need to consider hygiene risk, cleanability, appearance, and regulatory expectations.

A useful rule of thumb is to use electropolishing for surfaces that come into contact with the product, and mechanical polishing for non-product-contact surfaces. In food manufacturing, mechanical polishing is suitable for equipment frames and supports, external surfaces of machines, components that don’t get wet, and low-risk, dry handling areas.

Electropolishing comes into its own for:

  • Milk, dairy, and cream processing
  • Beer, beverage, and brewery pipework
  • Liquid food systems (such as for sauces or syrups)
  • Tanks and mixers leading to wet processing

It’s particularly important to electropolish where there are concerns that fats, proteins, or sugars can adhere to surfaces, or where clean-in-place systems are used.

In pharmaceutical manufacturing, mechanical polishing may be used initially for structural stainless steel supports and non-critical equipment surfaces. Electropolishing is used in bioreactors, water for injection systems, piping for products, sterile processing equipment, and filling lines, such as for liquid injectables or biologics.

Electropolishing is widely used in pharma manufacturing because of cleanability concerns, the need for low bio burden risk, and the consistent control of the surface the technique enables.

In short, electropolishing and mechanical polishing both have similar but quite distinct use cases. Your choice of technique will depend on requirements in terms of quality of surface finish, cleanability, and whether the equipment is coming into contact with the product. Explore our lab equipmentrange today to support your needs.

Glossary

Lorna Little

Lorna is an SEO Content Specialist at RS, where she creates search-led content focused on topics including industrial innovation, engineering, maintenance, and procurement. After studying Creative & Professional Writing at Canterbury Christ Church University, she built her career in SEO and content marketing across both agency and in-house environments, helping readers navigate technical subjects through informative, user-focused content. Outside of work, Lorna enjoys reading, travelling, and making memories with her family.

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy