Cryogenic Treatment for Tool Life

Cooling steel to −196°C transforms retained austenite into martensite. We explain how cryogenic treatment of tools extends the life of drill bits, milling cutters, and dies.

A red banner with light grey gradient

The cutting tools used in manufacturing processes like metal machining and woodworking are subjected to tremendous abrasion, temperatures, and stresses. Tool steels can better withstand this if cryogenic hardening tools and techniques are worked into the steel production. Cryogenic treatment of tools used for cutting involves gradually cooling them to extreme sub-zero temperatures after their initial heat treating so that their retained austenite can be transformed into martensite, improving hardness.

Cryogenic treatment also unlocks further advanced materials properties like enhanced wear resistance, fatigue resistance, and durability. Read on to understand the concepts and techniques involved in this.

Key Takeaways:

  • The alloying compositions of tool steels makes them retain austenite after heat treating, leaving them soft inside
  • Promptly cooling these steels to cryogenic temperatures (below −150°C) lets their retained austenite form martensite, improving hardness
  • Cryogenic treatment can also encourage eta-carbides to form within the martensite, further improving hardness
  • Cooling to cryogenic temperatures must be done gradually to prevent cracks. Tempering before and after this cooling helps improve results too

Definitions:

  • Austenite: A state that steel microstructure can achieve at elevated temperatures if conditions were controlled properly. It’s critical for preventing the steel’s carbon from leaching out and then diminishing the steel’s strength, but if the austenite remains after cooling, this makes the steel soft
  • Martensite: A hardened state that steel microstructure can achieve if it’s cooled just right
  • Ferrite: A form of iron that’s stable and magnetic at room temperature
  • Precipitate: A solid formed due to a chemical reaction from material that had been in liquid form in a solution
  • Carbide: A hard precipitate formed of carbon and iron (or other elements) during steel metallurgy
  • Cementite: Also known as iron carbide, it’s hard and brittle and can precipitate out of austenite as it cools and forms ferrite, or out of martensite during tempering
  • Tempering: Reheating steel to a moderate temperature after the initial heat treatment to achieve greater toughness
  • Quenching: Rapidly cooling steel from its heat treating temperature

The Metallurgy: Austenite to Martensite Conversion

Heat treating steel involves bringing it to elevated temperatures (approaching 1,100°C) so it can form austenite, which in turn is intended to transform into the better hardened state of martensite once it cools. For tool steels, it’s ideal for all the austenite to convert to martensite, but simply cooling to room temperature can leave considerable austenite retained alongside the martensite that forms.

As you increase the heat treatment temperature, you can dissolve more of the carbides in the steel and bring more carbon into solution to improve hardness. Eventually, though, increasing the temperature will make the resultant hardness come back down, while the amount of austenite retained increases.

The formation of martensite is driven by the temperature the steel reaches (the martensite start temperature, Ms). Martensite starts forming once the temperature starts to decrease and stops forming when the temperature stops decreasing (or when it reaches the martensite finish temperature, Mf). Ms decreases as the amounts of carbon and other alloying elements increase. As the Ms decreases, so does Mf, to the point that the lowest temperature where the martensite will transform into austenite is significantly below room temperature.

Cold treatments subject the steel post-heat-treating to low temperatures such as those of household freezers, dry ice, or liquid nitrogen. Liquid nitrogen achieves cryogenic temperatures - below −150°C, and even going down to −196°C. With cryogenic treatment of steels that experience a very low Mf, you can transform much more (and ideally all) of the retained austenite into martensite. This improves hardness, wear resistance, durability, and fatigue resistance. For cutting tool steels, this helps the material better withstand deformation and abrasion, while retaining its cutting edge better at high temperatures.

You should consider the stabilisation of austenite, though. Stabilised austenite is unlikely to successfully convert to martensite during cold treatment, and this stabilisation happens when the steel is left at room temperature. For best results, quench the steel rapidly from Ms down to room temperature and then continuously keep cooling it down to cryogenic temperatures until it reaches Mf.

Precipitating Eta-Carbides for Wear Resistance

Carbides are compounds of carbon and iron (or alloying elements) that precipitate into distinct solids in steel microstructure during steel production. Strategic formation of carbides is a major part of tool steel production since they help improve wear resistance and yield strength.

A study found that cryogenic treatment of tools can increase their wear resistance due to the precipitation of transition carbides called eta-carbides (η-carbides). Transition carbides are extremely small (in the range of 2-4 nm) and are named for their role as an early stage of the formation of cementite (iron carbide). When eta-carbides fill the microscopic voids in steel microstructure, this greatly increases the material’s hardness and wear resistance, which are essential properties for cutting tool steels.

During the cryogenic hardening process, eta-carbides form due to expansion and contraction of the atoms of iron and alloying elements. This lattice deformation allows carbon atoms to shift accordingly and form eta-carbides. The result is that they enhance the hardness of the martensite they’re embedded in.

Which Steels Benefit Most? High Speed Steel vs Carbide

High speed steel is a carbon steel alloyed with elements such as molybdenum, vanadium, tungsten, and chromium. Those give it good wear resistance and help it maintain hardness at high temperatures (dropping to 48.5 HRC at 600°C from 62 to 65 HRC nominal). High speed steel also has good toughness.

Carbide steel generally refers to tungsten carbide steel, which is a composite of tungsten carbide and a metallic binder such as cobalt. It has very high hardness (69 to 81 HRC), and can hold 60 HRC at high temperatures such as 900 to 1,000°C. It resists wear and corrosion well and holds its strength in extreme conditions.

Deep cold treatment steel work can impart benefits on each of these types of steel in different ways.

Exposing high speed steel tools to cryogenic treatment hardens and toughens them, and improves their service life by letting them maintain their hardness longer at higher speeds. It also helps improve the surface finish of parts cut with high speed steels.

Applying cryogenic treatment to tungsten carbide steels similarly improves their hardness and service life. Specifically, it helps refine the cobalt binder matrix by alleviating its tensile stress into compressive stress, preventing microcracks. The cryogenic treatment also precipitates some atoms out of the cobalt as compounds, further hardening it.

Cryogenic treatment of tools made from either of these materials can help them both achieve better performance and last longer.

A range of circular steel frames

The Treatment Cycle: Slow Cool and Temper

Here’s an example set of steps for performing cryogenic treatment on tool steels to increase their hardness. This assumes that two phases of tempering will be done, although this can vary based on the steel to be made.

  1. Assess the percentages of carbon and other alloying elements in the starting steel
  2. Based on that composition, consult charts to determine the temperatures required for the heat treatment, tempering, and cryogenic treatment to achieve the desired finishing properties
  3. Place the steel in the conventional heat treatment oven and bring it to its desired maximum temperature
  4. Quench the steel rapidly in water, air, or oil, based on what’s best for the application
  5. Reheat the steel for its initial tempering, heating it just enough so that the martensite created so far isn’t lost
  6. Quench the steel again, and then promptly start slowly further cooling with gaseous nitrogen. This initial sub-zero cooling phase helps avoid thermal stress
  7. Gradually expose the steel to liquid nitrogen until it reaches cryogenic temperatures. Be patient, as slower cooling equals better resultant steel properties
  8. Hold the steel at the target lowest temperature for up to 24 hours
  9. Temper the steel again, bringing it to the same tempering temperature as before to remove any brittleness that may have formed during the cryogenic martensite formation, preventing cracking

However, keep in mind these common mistakes to avoid:

  • Leaving the initially cooled steel at room temperature for too long, which stabilises the austenite, preventing it from forming martensite
  • Cryogenically cooling the steel too rapidly, which adds thermal stresses and can crack it
  • Cooling the steel colder than is required, which increases brittleness and the likelihood of cracks
  • Failing to consider that thin sections will cool more quickly than thick ones, thus becoming brittle sooner. The initial tempering phase helps alleviate this

By following the right heating and cooling procedures for your steel application, you can achieve the enhanced hardness available through cryogenic treatment.

Expected Life Increase Statistics

Let’s compare how cryogenically hardening tools and parts in different applications can increase their service life:

Type of Part or Cutting Tool
Service Life % Increase
Bandsaw blades (for wood)280
Bandsaw blades (for metal)300
Stamping dies310
Punch presses320 to 425
Chipper knives (soft woods)380
Chipper knives (hard woods)270
Plasma torch tips360
Roller chains275 to 325
Abrasive slurry pumps200
Moulder knives400

Across a wide range of applications, cryogenic treatment helps steel last significantly longer, increasing its usable life and making it a more sustainable choice.

Make sure to always use safe practices and PPE around liquid nitrogen. To help seal heating ovens and containers for liquid nitrogen, we stock dispensing tips for silicones, adhesives, and gels. We can also help you with material dispensers like sealant guns and tape dispensers. Explore our full range online today.

FAQs

Lorna Little

Lorna is an SEO Content Specialist at RS, where she creates search-led content focused on topics including industrial innovation, engineering, maintenance, and procurement. After studying Creative & Professional Writing at Canterbury Christ Church University, she built her career in SEO and content marketing across both agency and in-house environments, helping readers navigate technical subjects through informative, user-focused content. Outside of work, Lorna enjoys reading, travelling, and making memories with her family.

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy