Phoenix Contact Label Printers| RS
Please look at our Phoenix Contact Label Printer range, available for next day delivery!
Label Printers are used to create high quality labels, these types of printers can be used at home or in professional environments such as offices, construction sites, hospitality, retail, health care and many more. Most Label Printers offer the user an option to be able to amend the font, font size and frames to create a custom label.
These devices can be standalone or desktop. If your device is standalone it will come with a keyboard and a display screen. Portable Label Makers work from battery power, they can either have batteries in the device or need to be battery charged, If your label printer needs to be battery charged this can be charged wirelessly through a USB port or with a plug depending on the type of device you have. Desktop devices work alongside a computer and are connected together via Bluetooth, USB or Wi-Fi. This type of label printer prints larger labels.
Most Label Printers use Thermal Labels which create high quality images and are commonly used to print barcodes. Thermal print-heads use chemically treated labels which darken the text or image required which lowers the cost of use as no ink, toner or ribbon is required.
Depending on the use of your Label Printer the labels can endure ultraviolet exposures, chemicals and extreme temperatures. The direct thermal printing method is more sensitive to light and heat whereas the Thermal transfer method creates more durable and long-lasting labels.