StarTech.com USB Network Adapters
StarTech.com ensure that all their products have tested and certified compatibility, to meet the technical performance needs of all IT pros. Centring their focus on fixing their customers' problems, StarTech.com work passionately to fulfil each customer requirement by working with RS Components to put hard-to-find technology solutions at your fingertips through an extensive range of modern USB network adapters. Features such as thermoplastic elastomer (TPE) construction and enhanced strain relief, for example, in many of their adapters ensure reliability, enhanced performance, and innovation to meet your needs.
What is a USB network adapter?
A USB network adapter is also commonly referred to as a USB ethernet adapter. The USB network adapter has an ethernet port on one end, which connects to a wired network, and the other end is a USB plug, which is to be plugged into your computer. If your wireless network does not offer you a stable enough connection, then a USB network adapter may be beneficial for you. The StarTech.com USB network adapters result in an increase in internet speed, as well as making the internet connection more stable than a wireless connection.How do I use a USB network adapter?
The USB network adapter has a USB-C connector. Simply insert the USB-C connector into your device's USB-C port. If you're connecting your wi-fi router, for example, take the router's ethernet cable and insert the end into the adapter's ethernet jack. It will take a few minutes for the driver to automatically install.Can you run internet through USB?
In short, yes you can. By using a StarTech.com USB network adapter, you can access the internet quickly and successfully. For instance, the StarTech.com range of USB network adapters offer top-quality features. This includes fast file transfers (where it uses true Gigabit bandwidth support for fast ethernet networks or Gigabit ethernet), portable designs so that you can take it anywhere, if necessary, and simple and efficient access for your USB-C devices using our USB Type-C connector.Popular Searches
Related links
- USB Network Adapters
- Startech USB Ethernet Adapter USB 3.0 USB A to RJ45...
- StarTech.com USB Network Adapter USB 3.0 USB A to RJ45
- Startech USB Ethernet Adapter USB 2.0 USB A to SFP Fibre Optic...
- StarTech.com USB Network Adapter
- StarTech.com USB Network Adapter USB 2.0 A to RJ45
- StarTech.com USB Ethernet Adapter USB 2.0 RJ45 to USB 2.0 A...
- StarTech.com 4 Port USB Network Adapter 10/100/1000Mbit/s Network Speed